<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ball Diameter for i.MX 6ULL LFBGA289 Package in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Ball-Diameter-for-i-MX-6ULL-LFBGA289-Package/m-p/2313085#M243873</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;The drawing show 0.45mm over 0.35mm, is this the possible range or two different nominal values?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;These values are a possible range of ball diameter.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Is this accurate and the drawing is not up to date?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;All of the dimensions (documentation, footprint, design files) can be “correct” according to the different land‑pattern for your design such as NSMD or SMD, I suggest you use the footprint provided in NXP website. As you mention, the reference design can use a smaller pad diameter but at the end, this can vary depending on the specific manufacturing process.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Thu, 05 Feb 2026 16:40:09 GMT</pubDate>
    <dc:creator>JorgeCas</dc:creator>
    <dc:date>2026-02-05T16:40:09Z</dc:date>
    <item>
      <title>Ball Diameter for i.MX 6ULL LFBGA289 Package</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ball-Diameter-for-i-MX-6ULL-LFBGA289-Package/m-p/2308547#M243840</link>
      <description>&lt;P&gt;Can anyone confirm the ball diameter or a recommended pad diameter for the LFBGA289 package found here?&lt;BR /&gt;&lt;A href="https://www.nxp.com/packages/SOT1534-2" target="_blank"&gt;SOT1534-2: LFBGA289 | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The drawing show 0.45mm over 0.35mm, is this the possible range or two different nominal values?&lt;BR /&gt;&lt;BR /&gt;The nominal footprint I downloaded from NXP uses 0.37mm pad diameters, while the reference design&amp;nbsp;MCIMX6ULL-CM uses 0.30mm pad diameters.&lt;/P&gt;&lt;P&gt;I am designing with MCIMX6Y2DVM09AB specifically.&lt;BR /&gt;&lt;BR /&gt;I started a chat on the website and attached the transcript. I received confirmation that the ball diameter is actually in the range of 0.38 to 0.48mm. Is this accurate and the drawing is not up to date? They also mentioned a document with recommended land patterns that could potentially be shared, and recommended a pad diameter of 0.4mm. That seems high to me, given the reference SODIMM module uses about 0.3mm&lt;/P&gt;</description>
      <pubDate>Wed, 04 Feb 2026 14:04:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ball-Diameter-for-i-MX-6ULL-LFBGA289-Package/m-p/2308547#M243840</guid>
      <dc:creator>a1wolfe</dc:creator>
      <dc:date>2026-02-04T14:04:18Z</dc:date>
    </item>
    <item>
      <title>Re: Ball Diameter for i.MX 6ULL LFBGA289 Package</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ball-Diameter-for-i-MX-6ULL-LFBGA289-Package/m-p/2313085#M243873</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;The drawing show 0.45mm over 0.35mm, is this the possible range or two different nominal values?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;These values are a possible range of ball diameter.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Is this accurate and the drawing is not up to date?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;All of the dimensions (documentation, footprint, design files) can be “correct” according to the different land‑pattern for your design such as NSMD or SMD, I suggest you use the footprint provided in NXP website. As you mention, the reference design can use a smaller pad diameter but at the end, this can vary depending on the specific manufacturing process.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 05 Feb 2026 16:40:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ball-Diameter-for-i-MX-6ULL-LFBGA289-Package/m-p/2313085#M243873</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2026-02-05T16:40:09Z</dc:date>
    </item>
  </channel>
</rss>