<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to make Ramdisk.img and boot.img in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-Ramdisk-img-and-boot-img/m-p/255718#M24384</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all:&lt;/P&gt;&lt;P&gt;I can buil the linux kernel and u-boot by using the modified environment and source code. I use the recent myandroid to build the ramdisk.img.&lt;BR /&gt;I can run the uboot and linux kernel. however,it will stop on the init which is on the ramdisk. I trace the procedure and find that it will stop on the mount function.&lt;BR /&gt;Do you have any idea about it?&lt;/P&gt;&lt;P&gt;The attached file is the log.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Justin Wu&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336914"&gt;log_zuni_data_0703_d_log.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Jul 2013 06:22:24 GMT</pubDate>
    <dc:creator>JustinWu2</dc:creator>
    <dc:date>2013-07-05T06:22:24Z</dc:date>
    <item>
      <title>How to make Ramdisk.img and boot.img</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-Ramdisk-img-and-boot-img/m-p/255718#M24384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all:&lt;/P&gt;&lt;P&gt;I can buil the linux kernel and u-boot by using the modified environment and source code. I use the recent myandroid to build the ramdisk.img.&lt;BR /&gt;I can run the uboot and linux kernel. however,it will stop on the init which is on the ramdisk. I trace the procedure and find that it will stop on the mount function.&lt;BR /&gt;Do you have any idea about it?&lt;/P&gt;&lt;P&gt;The attached file is the log.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Justin Wu&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336914"&gt;log_zuni_data_0703_d_log.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2013 06:22:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-make-Ramdisk-img-and-boot-img/m-p/255718#M24384</guid>
      <dc:creator>JustinWu2</dc:creator>
      <dc:date>2013-07-05T06:22:24Z</dc:date>
    </item>
    <item>
      <title>Re: How to make Ramdisk.im​g and boot.img</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-Ramdisk-img-and-boot-img/m-p/255719#M24385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,justin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please see android user's guide for R13.4.1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;5.4 Build boot.img&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;As outlined in Run Android with Prebuilt Image, we use boot.img and booti as default commands to boot, not the uramdisk&lt;/P&gt;&lt;P&gt;and uImage we used before.&lt;/P&gt;&lt;P&gt;You can use this command to generate boot.img under Android environment:&lt;/P&gt;&lt;P&gt;$ cd ~/myandroid&lt;/P&gt;&lt;P&gt;$ source build/envsetup.sh&lt;/P&gt;&lt;P&gt;$ lunch sabresd_6dq-user&lt;/P&gt;&lt;P&gt;$ make bootimage&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Weidong&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2013 08:48:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-make-Ramdisk-img-and-boot-img/m-p/255719#M24385</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-07-05T08:48:21Z</dc:date>
    </item>
  </channel>
</rss>