<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic OV5640 autofocus with IMX8MP in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/OV5640-autofocus-with-IMX8MP/m-p/2305397#M243796</link>
    <description>&lt;P&gt;We are currently developing a project using an i.MX8MP processor running Android 11 (NXP BSP). Our hardware setup includes an OV5640 camera module with autofocus support, connected via the MIPI-CSI interface.&amp;nbsp;&lt;BR /&gt;While the camera imaging and preview are working, we have encountered an issue regarding autofocus functionality. It appears that the standard Android 11 BSP for i.MX8MP does not natively support or expose AF controls for the OV5640. We are using kernel 5.10.72 and OV5640 MIPI Camera Subdev Driver (drivers/media/i2c/ov5640.c).&lt;/P&gt;&lt;P&gt;Is there an updated OV5640 kernel driver for the i.MX8MP that includes autofocus support?&lt;BR /&gt;Any guidance, patches, or reference documentation would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 15:07:18 GMT</pubDate>
    <dc:creator>zb2020</dc:creator>
    <dc:date>2026-02-03T15:07:18Z</dc:date>
    <item>
      <title>OV5640 autofocus with IMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OV5640-autofocus-with-IMX8MP/m-p/2305397#M243796</link>
      <description>&lt;P&gt;We are currently developing a project using an i.MX8MP processor running Android 11 (NXP BSP). Our hardware setup includes an OV5640 camera module with autofocus support, connected via the MIPI-CSI interface.&amp;nbsp;&lt;BR /&gt;While the camera imaging and preview are working, we have encountered an issue regarding autofocus functionality. It appears that the standard Android 11 BSP for i.MX8MP does not natively support or expose AF controls for the OV5640. We are using kernel 5.10.72 and OV5640 MIPI Camera Subdev Driver (drivers/media/i2c/ov5640.c).&lt;/P&gt;&lt;P&gt;Is there an updated OV5640 kernel driver for the i.MX8MP that includes autofocus support?&lt;BR /&gt;Any guidance, patches, or reference documentation would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 15:07:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OV5640-autofocus-with-IMX8MP/m-p/2305397#M243796</guid>
      <dc:creator>zb2020</dc:creator>
      <dc:date>2026-02-03T15:07:18Z</dc:date>
    </item>
    <item>
      <title>Re: OV5640 autofocus with IMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OV5640-autofocus-with-IMX8MP/m-p/2310808#M243850</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Unfortunately, in Android BSP, there is no support for Auto Focus Ccontrol. You may need to contact OmniVision, there is an application note "Auto FocusCamera Module Application Notes". It mentions a firmware and AF Sequence but, you need to add the AFC function in the driver by yourself.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Feb 2026 17:07:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OV5640-autofocus-with-IMX8MP/m-p/2310808#M243850</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2026-02-04T17:07:31Z</dc:date>
    </item>
  </channel>
</rss>