<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX93 RMII 50MHz Reference Clock Disappears After Linux Boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-RMII-50MHz-Reference-Clock-Disappears-After-Linux-Boot/m-p/2304075#M243746</link>
    <description>&lt;P&gt;firstly I suggest that you can refer to the attached AN which has very detailed settings and configuration for imx93 RMII mode&lt;/P&gt;</description>
    <pubDate>Sat, 31 Jan 2026 06:01:18 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2026-01-31T06:01:18Z</dc:date>
    <item>
      <title>i.MX93 RMII 50MHz Reference Clock Disappears After Linux Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-RMII-50MHz-Reference-Clock-Disappears-After-Linux-Boot/m-p/2303486#M243729</link>
      <description>&lt;P&gt;I am using i.MX93 with two Ethernet ports configured in RMII mode, where the SoC provides the 50 MHz RMII reference clock.&lt;BR /&gt;With the attached DTS, the 50 MHz RMII clock is correctly output during U-Boot, but disappears after Linux boots.&lt;BR /&gt;Please analyze the attached DTS and advise:&lt;BR /&gt;- The root cause of the RMII clock being disabled in Linux&lt;BR /&gt;- Required Linux device-tree changes or driver/clock configuration&lt;BR /&gt;- Any known limitations or mandatory settings for SoC-generated RMII clock on i.MX93&lt;BR /&gt;I would appreciate guidance on the correct configuration or recommended solution.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;David&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jan 2026 08:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-RMII-50MHz-Reference-Clock-Disappears-After-Linux-Boot/m-p/2303486#M243729</guid>
      <dc:creator>seongkeunjin</dc:creator>
      <dc:date>2026-01-30T08:50:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 RMII 50MHz Reference Clock Disappears After Linux Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-RMII-50MHz-Reference-Clock-Disappears-After-Linux-Boot/m-p/2303487#M243730</link>
      <description>&lt;P&gt;The DTS file is here.&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jan 2026 08:51:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-RMII-50MHz-Reference-Clock-Disappears-After-Linux-Boot/m-p/2303487#M243730</guid>
      <dc:creator>seongkeunjin</dc:creator>
      <dc:date>2026-01-30T08:51:30Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 RMII 50MHz Reference Clock Disappears After Linux Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-RMII-50MHz-Reference-Clock-Disappears-After-Linux-Boot/m-p/2304075#M243746</link>
      <description>&lt;P&gt;firstly I suggest that you can refer to the attached AN which has very detailed settings and configuration for imx93 RMII mode&lt;/P&gt;</description>
      <pubDate>Sat, 31 Jan 2026 06:01:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-RMII-50MHz-Reference-Clock-Disappears-After-Linux-Boot/m-p/2304075#M243746</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2026-01-31T06:01:18Z</dc:date>
    </item>
  </channel>
</rss>