<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CDC VNIC FreeRTOS example in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CDC-VNIC-FreeRTOS-example/m-p/2292834#M243381</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250887"&gt;@alaanasef96&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;It is likely that Linux works because the example enumerates as&amp;nbsp;a standards‑based CDC Ethernet device (CDC‑ECM), which Windows 11 does not support.&lt;/P&gt;
&lt;P&gt;Did you follow the steps shown on the readme.md of the example project to install the&amp;nbsp;RNDIS driver? Does following these steps change anything on your windows computer?&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jan 2026 22:26:50 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2026-01-13T22:26:50Z</dc:date>
    <item>
      <title>CDC VNIC FreeRTOS example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CDC-VNIC-FreeRTOS-example/m-p/2292689#M243371</link>
      <description>&lt;P&gt;I am trying to use the USB interface of the i.MX RT1050 evaluation kit as a network interface using the&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;CDC VNIC FreeRTOS&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;example.&lt;BR /&gt;On&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;Linux&lt;/STRONG&gt;, the example works perfectly: it creates a bridge between the on-board Ethernet interface and the USB interface.&lt;/P&gt;&lt;P&gt;However, on&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;Windows 11&lt;/STRONG&gt;, the USB device is detected as a&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;COM port&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;instead of a network interface.&lt;BR /&gt;I tried installing the&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;RNDIS driver&lt;/STRONG&gt;, but Windows already includes a built-in RNDIS driver as far as I saw online.&lt;/P&gt;&lt;P&gt;Can someone explain why this happens and what needs to be changed to make Windows recognize the USB interface as a network adapter?&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jan 2026 15:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CDC-VNIC-FreeRTOS-example/m-p/2292689#M243371</guid>
      <dc:creator>alaanasef96</dc:creator>
      <dc:date>2026-01-13T15:28:24Z</dc:date>
    </item>
    <item>
      <title>Re: CDC VNIC FreeRTOS example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CDC-VNIC-FreeRTOS-example/m-p/2292834#M243381</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250887"&gt;@alaanasef96&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;It is likely that Linux works because the example enumerates as&amp;nbsp;a standards‑based CDC Ethernet device (CDC‑ECM), which Windows 11 does not support.&lt;/P&gt;
&lt;P&gt;Did you follow the steps shown on the readme.md of the example project to install the&amp;nbsp;RNDIS driver? Does following these steps change anything on your windows computer?&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jan 2026 22:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CDC-VNIC-FreeRTOS-example/m-p/2292834#M243381</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2026-01-13T22:26:50Z</dc:date>
    </item>
    <item>
      <title>Re: CDC VNIC FreeRTOS example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CDC-VNIC-FreeRTOS-example/m-p/2293037#M243396</link>
      <description>It seems that I was trying to install the incorrect RNDIS drivers, when I used the one in the example folder "which I didnot know they exist" it works now, thank you.&lt;BR /&gt;now I need to change this example to use usbX and threadX</description>
      <pubDate>Wed, 14 Jan 2026 08:12:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CDC-VNIC-FreeRTOS-example/m-p/2293037#M243396</guid>
      <dc:creator>alaanasef96</dc:creator>
      <dc:date>2026-01-14T08:12:26Z</dc:date>
    </item>
  </channel>
</rss>