<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Simultan access  GPIO13 from core m7 and GPIO9 from core m4</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Simultan-access-GPIO13-from-core-m7-and-GPIO9-from-core-m4/m-p/2291136#M243305</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189442"&gt;@AndreasL&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for the information.&lt;/P&gt;
&lt;P&gt;During the period when GPIO13 registers are being accessed, the LPSR domain bus will be on hold.&lt;/P&gt;
&lt;P&gt;In this case, GPIO9 is part of the LPSR domain, which means that communication from the M4 core to GPIO9 must wait until the M7 core finishes accessing the GPIO13 registers.&lt;/P&gt;
&lt;P&gt;See Table 3: i.MX RT1170 Modules List in the i.MX RT1170 Crossover Processors Data Sheet.&lt;/P&gt;
&lt;P&gt;If the motor control cycle implementation is being affected by this behavior, you could try using a GPIO other than GPIO13.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Pablo&lt;/P&gt;</description>
    <pubDate>Fri, 09 Jan 2026 18:57:43 GMT</pubDate>
    <dc:creator>Pablo_Ramos</dc:creator>
    <dc:date>2026-01-09T18:57:43Z</dc:date>
    <item>
      <title>Simultan access  GPIO13 from core m7 and GPIO9 from core m4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Simultan-access-GPIO13-from-core-m7-and-GPIO9-from-core-m4/m-p/2290123#M243245</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear NXP team,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CPU i.mxrt1176CVM8A.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In my application I have on core m4 motor control application and on core m7 real time application.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If I access simultaneously from core m7 GPIO13 and from core m4 GPIO9, the access to GPIO9 will be delayed more than 31µs.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In the datasheet I can found chapter 13.1 And in chapter 2.1.2 System Bus Diagram following information&lt;BR /&gt;&lt;BR /&gt;When LPSRMIX master is accessing GPIO13, XB will hold WAKEUPMIX master requests to any AIPS4 peripheral until current LPSRMIX master access is completed. Because GPIO13 access is based on 32 K clock as it’s in SNVS domain to save power, these WAKEUPMIX master requests could be held for over 31µs.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I understand the delay from core m7 between AIPS4 to GPIO13(LPSRMIX-Domin) but not the delay from more than 31µs to the GPIO9(WAKEUPMIX) pin GPIO_AD_31 over the direct way from core m4 to GPIO-SOC. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please find in the attachment the bus diagram, I have marked with green and blue communications:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Please can you help me. I have with this delay a problem with the motor control cycle!&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jan 2026 09:54:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Simultan-access-GPIO13-from-core-m7-and-GPIO9-from-core-m4/m-p/2290123#M243245</guid>
      <dc:creator>AndreasL</dc:creator>
      <dc:date>2026-01-08T09:54:21Z</dc:date>
    </item>
    <item>
      <title>Re: Simultan access  GPIO13 from core m7 and GPIO9 from core m4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Simultan-access-GPIO13-from-core-m7-and-GPIO9-from-core-m4/m-p/2290406#M243254</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189442"&gt;@AndreasL&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I am not able to see the attachment of the bus diagram. Could you please send it again?&lt;/P&gt;
&lt;P&gt;What are the configurations of the Cortex?&lt;/P&gt;
&lt;P&gt;What are the speeds of both Cortex?&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jan 2026 18:09:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Simultan-access-GPIO13-from-core-m7-and-GPIO9-from-core-m4/m-p/2290406#M243254</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2026-01-08T18:09:18Z</dc:date>
    </item>
    <item>
      <title>Re: Simultan access  GPIO13 from core m7 and GPIO9 from core m4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Simultan-access-GPIO13-from-core-m7-and-GPIO9-from-core-m4/m-p/2290657#M243272</link>
      <description>&lt;P&gt;Hi Pablo,&lt;/P&gt;&lt;P&gt;Many thanks for your quick response.&lt;/P&gt;&lt;P&gt;The cortex m7 is the master the main clock is: 792.000.000 Hz&lt;BR /&gt;The main clock of the cortex m4 is: 392.727.258 Hz&lt;BR /&gt;Bus clock root is: 240 MHz&lt;BR /&gt;Bus LPSR clock root is: 160 MHz&lt;BR /&gt;&lt;BR /&gt;Please find also attached the configuration files.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="BusDiagram.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/372258iB65BDE40D00DC153/image-size/medium?v=v2&amp;amp;px=400" role="button" title="BusDiagram.png" alt="BusDiagram.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Andreas&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Fri, 09 Jan 2026 07:10:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Simultan-access-GPIO13-from-core-m7-and-GPIO9-from-core-m4/m-p/2290657#M243272</guid>
      <dc:creator>AndreasL</dc:creator>
      <dc:date>2026-01-09T07:10:12Z</dc:date>
    </item>
    <item>
      <title>Re: Simultan access  GPIO13 from core m7 and GPIO9 from core m4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Simultan-access-GPIO13-from-core-m7-and-GPIO9-from-core-m4/m-p/2291136#M243305</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189442"&gt;@AndreasL&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for the information.&lt;/P&gt;
&lt;P&gt;During the period when GPIO13 registers are being accessed, the LPSR domain bus will be on hold.&lt;/P&gt;
&lt;P&gt;In this case, GPIO9 is part of the LPSR domain, which means that communication from the M4 core to GPIO9 must wait until the M7 core finishes accessing the GPIO13 registers.&lt;/P&gt;
&lt;P&gt;See Table 3: i.MX RT1170 Modules List in the i.MX RT1170 Crossover Processors Data Sheet.&lt;/P&gt;
&lt;P&gt;If the motor control cycle implementation is being affected by this behavior, you could try using a GPIO other than GPIO13.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jan 2026 18:57:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Simultan-access-GPIO13-from-core-m7-and-GPIO9-from-core-m4/m-p/2291136#M243305</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2026-01-09T18:57:43Z</dc:date>
    </item>
  </channel>
</rss>