<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Adding Support for the IMX412 Camera Sensor on a VC MIPI Module for IMX95 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Adding-Support-for-the-IMX412-Camera-Sensor-on-a-VC-MIPI-Module/m-p/2277790#M243157</link>
    <description>&lt;P&gt;&lt;STRONG&gt;Overview&lt;/STRONG&gt;&lt;BR /&gt;As part of adding support for the IMX412 camera sensor mounted on a VC MIPI module to Compulab’s EVK (UCM-IMX95) running an i.MX95 SoM, the following changes were made:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Added the required device tree nodes to describe the video capture pipeline:&lt;BR /&gt;&lt;STRONG&gt;VC camera → MIPI CSI controller → CSI pixel formatter → ISI&lt;/STRONG&gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Integrated the official VC driver from their GitHub repository (&lt;A href="https://github.com/VC-MIPI-modules" target="_blank" rel="noopener"&gt;https://github.com/VC-MIPI-modules&lt;/A&gt;), with minor modifications, as the driver primarily targets the i.MX8 family.&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;STRONG&gt;Current Status&lt;/STRONG&gt;&lt;BR /&gt;The driver successfully communicates with the sensor over the I²C bus, reports the supported video formats, and creates&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;/dev/video*&amp;nbsp;&lt;/STRONG&gt;device nodes. However, it does not create&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;/dev/media*&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;or&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;/dev/v4l-subdev*&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;devices.&lt;BR /&gt;At this stage, I am unsure of the root cause, but I suspect the issue is related to the device tree configuration.&lt;/P&gt;&lt;P&gt;I have attached the relevant DTS files, as well as the vc driver. I would appreciate any insights or suggestions on what might be missing or misconfigured.&lt;/P&gt;&lt;P&gt;*Note: The file imx95.dts is really imx95.dtsi. I changed it so that the upload would be accepted.&lt;/P&gt;</description>
    <pubDate>Mon, 05 Jan 2026 14:57:33 GMT</pubDate>
    <dc:creator>Arliden</dc:creator>
    <dc:date>2026-01-05T14:57:33Z</dc:date>
    <item>
      <title>Adding Support for the IMX412 Camera Sensor on a VC MIPI Module for IMX95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-Support-for-the-IMX412-Camera-Sensor-on-a-VC-MIPI-Module/m-p/2277790#M243157</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Overview&lt;/STRONG&gt;&lt;BR /&gt;As part of adding support for the IMX412 camera sensor mounted on a VC MIPI module to Compulab’s EVK (UCM-IMX95) running an i.MX95 SoM, the following changes were made:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Added the required device tree nodes to describe the video capture pipeline:&lt;BR /&gt;&lt;STRONG&gt;VC camera → MIPI CSI controller → CSI pixel formatter → ISI&lt;/STRONG&gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Integrated the official VC driver from their GitHub repository (&lt;A href="https://github.com/VC-MIPI-modules" target="_blank" rel="noopener"&gt;https://github.com/VC-MIPI-modules&lt;/A&gt;), with minor modifications, as the driver primarily targets the i.MX8 family.&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;STRONG&gt;Current Status&lt;/STRONG&gt;&lt;BR /&gt;The driver successfully communicates with the sensor over the I²C bus, reports the supported video formats, and creates&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;/dev/video*&amp;nbsp;&lt;/STRONG&gt;device nodes. However, it does not create&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;/dev/media*&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;or&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;/dev/v4l-subdev*&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;devices.&lt;BR /&gt;At this stage, I am unsure of the root cause, but I suspect the issue is related to the device tree configuration.&lt;/P&gt;&lt;P&gt;I have attached the relevant DTS files, as well as the vc driver. I would appreciate any insights or suggestions on what might be missing or misconfigured.&lt;/P&gt;&lt;P&gt;*Note: The file imx95.dts is really imx95.dtsi. I changed it so that the upload would be accepted.&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jan 2026 14:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-Support-for-the-IMX412-Camera-Sensor-on-a-VC-MIPI-Module/m-p/2277790#M243157</guid>
      <dc:creator>Arliden</dc:creator>
      <dc:date>2026-01-05T14:57:33Z</dc:date>
    </item>
    <item>
      <title>Re: Adding Support for the IMX412 Camera Sensor on a VC MIPI Module for IMX95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-Support-for-the-IMX412-Camera-Sensor-on-a-VC-MIPI-Module/m-p/2281619#M243172</link>
      <description>&lt;P&gt;why do you need add&amp;nbsp; IMX412 camera sensor mounted on a VC MIPI module? what's the purpose of this module? do you have further information about this?&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jan 2026 03:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-Support-for-the-IMX412-Camera-Sensor-on-a-VC-MIPI-Module/m-p/2281619#M243172</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2026-01-06T03:16:36Z</dc:date>
    </item>
    <item>
      <title>Re: Adding Support for the IMX412 Camera Sensor on a VC MIPI Module for IMX95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-Support-for-the-IMX412-Camera-Sensor-on-a-VC-MIPI-Module/m-p/2281805#M243176</link>
      <description>&lt;P&gt;Thank you for the prompt reply!&lt;BR /&gt;The VC mipi module is just the board shipped from vision components onto which the imx412 is mounted. I am attaching the hardware operation manual they provided.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jan 2026 06:28:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-Support-for-the-IMX412-Camera-Sensor-on-a-VC-MIPI-Module/m-p/2281805#M243176</guid>
      <dc:creator>Arliden</dc:creator>
      <dc:date>2026-01-06T06:28:50Z</dc:date>
    </item>
    <item>
      <title>Re: Adding Support for the IMX412 Camera Sensor on a VC MIPI Module for IMX95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-Support-for-the-IMX412-Camera-Sensor-on-a-VC-MIPI-Module/m-p/2289944#M243238</link>
      <description>&lt;P&gt;I checked that these VC drivers are for the third party company board, currently we haven't supported these boards yet since imx95 is under preproduction, I suggest that you can consult from the third party company&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jan 2026 07:31:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-Support-for-the-IMX412-Camera-Sensor-on-a-VC-MIPI-Module/m-p/2289944#M243238</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2026-01-08T07:31:55Z</dc:date>
    </item>
  </channel>
</rss>