<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: linux sja1105 bridge mode causes PTP L2 layer data to lose timestamps in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/linux-sja1105-bridge-mode-causes-PTP-L2-layer-data-to-lose/m-p/2270975#M243133</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/257340"&gt;@hjk003&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;你使用的内核版本是什么？这里的MAC1 和MAC2分别是哪个网口？&lt;/P&gt;
&lt;P&gt;请使用ethtool -T swp1来查看它已经启用的功能。然后确保/dev/ptp0是你真正需要的接口。&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
    <pubDate>Mon, 05 Jan 2026 01:21:58 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2026-01-05T01:21:58Z</dc:date>
    <item>
      <title>linux sja1105 bridge mode causes PTP L2 layer data to lose timestamps</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-sja1105-bridge-mode-causes-PTP-L2-layer-data-to-lose/m-p/2269161#M243064</link>
      <description>&lt;P&gt;Hi, NXP team. When using a SoC (imx8mp-evk) + Switch (SJA1105) architecture, setting the network bridge mode causes PTP L2 layer data to lose timestamps.&lt;BR /&gt;This is our architecture:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;        ┌──────────────────────────────┐
        │                              │
        │                              │
        │                              │
        │                              │
        │                              │
        │                  ┌───────────┴───────────────┐
        │                  │         SPI               │
  ┌─────▼─────────┐        │                           │
  │   SPI         │        │                           │
  │ port0         │        │M                          │
  │ port1    port2◄────────┤A                          │
  │    SJA1105    │        │C                          │
  │               │        │1       CPU                │
  │ port3         │        │   MIMX8ML8DVNLZAB         │
  │ port4         │        │                           │
  │               │        │                           │
  └─────── ───────┘        │                           │
                           │        MAC2               │
                           └──────────┬────────────────┘
                                      │
                                      │
                                      │
┌───────── ────────┐                  │
│       RGMII      │                  │
│                  │                  │
│   PHY            │                  │
│   88E1512       M│                  │
│                 D◄──────────────────┘
│                 I│
│                 O│
│                  │
└───────┬──────────┘
        │
        │
        │
        │
        │
        │
        │
        │
        │
        └► OUT&lt;/LI-CODE&gt;&lt;P&gt;Ports 1 through 4 are each connected to a SoC device.&lt;/P&gt;&lt;P&gt;Linux system configuration&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;br0: flags=4163&amp;lt;UP,BROADCAST,RUNNING,MULTICAST&amp;gt;  mtu 1500
        inet 172.16.2.100  netmask 255.255.255.0  broadcast 172.16.2.255
        inet6 fe80::d053:57ff:feb1:df50  prefixlen 64  scopeid 0x20&amp;lt;link&amp;gt;
        ether d2:53:57:b1:df:50  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 12  bytes 984 (984.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

end0: flags=4163&amp;lt;UP,BROADCAST,RUNNING,MULTICAST&amp;gt;  mtu 1500
        inet 192.168.2.100  netmask 255.255.255.0  broadcast 192.168.2.255
        inet6 fe80::3065:76ff:feed:96cb  prefixlen 64  scopeid 0x20&amp;lt;link&amp;gt;
        ether 32:65:76:ed:96:cb  txqueuelen 1000  (Ethernet)
        RX packets 2  bytes 132 (132.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 49  bytes 2434 (2.4 KB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

end1: flags=4163&amp;lt;UP,BROADCAST,RUNNING,MULTICAST&amp;gt;  mtu 1504
        inet6 fe80::7c32:f0ff:fefb:c940  prefixlen 64  scopeid 0x20&amp;lt;link&amp;gt;
        ether 7e:32:f0:fb:c9:40  txqueuelen 1000  (Ethernet)
        RX packets 58  bytes 7130 (7.1 KB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 22  bytes 1828 (1.8 KB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
        device interrupt 210

lo: flags=73&amp;lt;UP,LOOPBACK,RUNNING&amp;gt;  mtu 65536
        inet 127.0.0.1  netmask 255.0.0.0
        inet6 ::1  prefixlen 128  scopeid 0x10&amp;lt;host&amp;gt;
        loop  txqueuelen 1000  (Local Loopback)
        RX packets 130  bytes 9914 (9.9 KB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 130  bytes 9914 (9.9 KB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

swp1: flags=4163&amp;lt;UP,BROADCAST,RUNNING,MULTICAST&amp;gt;  mtu 1500
        ether 7e:32:f0:fb:c9:40  txqueuelen 1000  (Ethernet)
        RX packets 58  bytes 6898 (6.8 KB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 0  bytes 0 (0.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

swp2: flags=4163&amp;lt;UP,BROADCAST,RUNNING,MULTICAST&amp;gt;  mtu 1500
        ether 7e:32:f0:fb:c9:40  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 0  bytes 0 (0.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

swp3: flags=4163&amp;lt;UP,BROADCAST,RUNNING,MULTICAST&amp;gt;  mtu 1500
        ether 7e:32:f0:fb:c9:40  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 0  bytes 0 (0.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

swp4: flags=4163&amp;lt;UP,BROADCAST,RUNNING,MULTICAST&amp;gt;  mtu 1500
        ether 7e:32:f0:fb:c9:40  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 12  bytes 984 (984.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
&lt;/LI-CODE&gt;&lt;LI-CODE lang="markup"&gt;root@hawaii-gen2:~# ptp4l -f linux_ptp_bc.conf -m &amp;amp;&amp;amp; phc2sys -a -r -m
ptp4l[149.643]: selected /dev/ptp0 as PTP clock
ptp4l[149.645]: port 2 (swp1): just a bunch of devices
ptp4l[149.645]: port 3 (swp2): just a bunch of devices
ptp4l[149.645]: port 4 (swp3): just a bunch of devices
ptp4l[149.645]: port 5 (swp4): just a bunch of devices
ptp4l[149.680]: port 1 (end0): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[149.717]: port 2 (swp1): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[149.753]: port 3 (swp2): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[149.785]: port 4 (swp3): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[149.817]: port 5 (swp4): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[149.817]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[149.817]: port 0 (/var/run/ptp4lro): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[150.545]: port 1 (end0): new foreign master 0080ee.fffe.60f9b8-1
ptp4l[154.561]: selected best master clock 0080ee.fffe.60f9b8
ptp4l[154.561]: port 1 (end0): LISTENING to UNCALIBRATED on RS_SLAVE
ptp4l[154.561]: Switched to /dev/ptp0 as PTP clock
ptp4l[155.360]: port 1 (end0): minimum delay request interval 2^-3
ptp4l[156.258]: port 3 (swp2): LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
ptp4l[156.292]: port 4 (swp3): LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
ptp4l[156.452]: port 5 (swp4): LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
ptp4l[156.569]: master offset -1766736492136248875 s0 freq      -0 path delay      1150
ptp4l[156.612]: port 2 (swp1): LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
ptp4l[157.261]: port 2 (swp1): received DELAY_REQ without timestamp
ptp4l[157.262]: port 4 (swp3): received DELAY_REQ without timestamp
ptp4l[157.262]: port 5 (swp4): received DELAY_REQ without timestamp
ptp4l[157.295]: port 2 (swp1): received DELAY_REQ without timestamp
ptp4l[157.295]: port 3 (swp2): received DELAY_REQ without timestamp
ptp4l[157.295]: port 5 (swp4): received DELAY_REQ without timestamp
ptp4l[157.455]: port 2 (swp1): received DELAY_REQ without timestamp
ptp4l[157.455]: port 3 (swp2): received DELAY_REQ without timestamp
ptp4l[157.455]: port 4 (swp3): received DELAY_REQ without timestamp
ptp4l[157.573]: master offset -1766736492136230812 s1 freq  +17991 path delay      -718
ptp4l[157.614]: port 3 (swp2): received DELAY_REQ without timestamp
ptp4l[157.615]: port 4 (swp3): received DELAY_REQ without timestamp
ptp4l[157.615]: port 5 (swp4): received DELAY_REQ without timestamp
ptp4l[158.262]: port 2 (swp1): received DELAY_REQ without timestamp
ptp4l[158.262]: port 4 (swp3): received DELAY_REQ without timestamp
ptp4l[158.262]: port 5 (swp4): received DELAY_REQ without timestamp
ptp4l[158.295]: port 2 (swp1): received DELAY_REQ without timestamp
ptp4l[158.296]: port 3 (swp2): received DELAY_REQ without timestamp
ptp4l[158.296]: port 5 (swp4): received DELAY_REQ without timestamp
ptp4l[158.455]: port 2 (swp1): received DELAY_REQ without timestamp
ptp4l[158.455]: port 3 (swp2): received DELAY_REQ without timestamp
ptp4l[158.455]: port 4 (swp3): received DELAY_REQ without timestamp
ptp4l[158.577]: master offset      -1848 s2 freq  +16143 path delay      -718
ptp4l[158.577]: port 1 (end0): UNCALIBRATED to SLAVE on MASTER_CLOCK_SELECTED&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Dec 2025 08:12:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-sja1105-bridge-mode-causes-PTP-L2-layer-data-to-lose/m-p/2269161#M243064</guid>
      <dc:creator>hjk003</dc:creator>
      <dc:date>2025-12-26T08:12:31Z</dc:date>
    </item>
    <item>
      <title>Re: linux sja1105 bridge mode causes PTP L2 layer data to lose timestamps</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-sja1105-bridge-mode-causes-PTP-L2-layer-data-to-lose/m-p/2270975#M243133</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/257340"&gt;@hjk003&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;你使用的内核版本是什么？这里的MAC1 和MAC2分别是哪个网口？&lt;/P&gt;
&lt;P&gt;请使用ethtool -T swp1来查看它已经启用的功能。然后确保/dev/ptp0是你真正需要的接口。&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jan 2026 01:21:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-sja1105-bridge-mode-causes-PTP-L2-layer-data-to-lose/m-p/2270975#M243133</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2026-01-05T01:21:58Z</dc:date>
    </item>
  </channel>
</rss>