<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: No response when reading Status and Command Register in PCIE of i.MX7D</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2267927#M243025</link>
    <description>&lt;P&gt;Hello Zhiming_Liu.&lt;BR /&gt;Regarding the support I received from you, I am having trouble with the i.MX8 processing, which is a preliminary step.&lt;BR /&gt;I referred to "5.5.9.5 Example Code 4" in the Reference Manual.&lt;BR /&gt;reg32_write (GPC_IPS_BASE_ADDR + 0xF8 , *** | 0x2 );&lt;BR /&gt;After running this code, the MPU becomes unresponsive.&lt;BR /&gt;However, there is no problem with values ​​other than PCIE_PHY.&lt;/P&gt;&lt;P&gt;Could you please tell me what to set and how to set it before running u-boot/drivers/pci/pcie_imx.c@probe(struct udevice *dev)?&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;</description>
    <pubDate>Tue, 23 Dec 2025 04:31:34 GMT</pubDate>
    <dc:creator>tamotsu</dc:creator>
    <dc:date>2025-12-23T04:31:34Z</dc:date>
    <item>
      <title>No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2262242#M242881</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;There is no response when reading the Status and Command Register in the PCIE of i.MX7D.&lt;/P&gt;&lt;P&gt;I have the following settings:&lt;/P&gt;&lt;P&gt;RDC_MRCn : (RDC_PDAO45) 0x000000FF&lt;/P&gt;&lt;P&gt;PMU_REG_1P0Dn : 0x00021073&lt;/P&gt;&lt;P&gt;CCM_TARGET_ROOTn : PCIE_CTRL_CLK_ROOT : 0x12000000&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; PCIEPHY_CLK_ROOT : 0x11000000&lt;/P&gt;&lt;P&gt;CCM_CCGR96 : pcie : 0x00000003&lt;/P&gt;&lt;P&gt;SRC_PCIEPHY_RCR : 0x00000000&lt;/P&gt;&lt;P&gt;Are there any other settings I need to make?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Dec 2025 05:39:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2262242#M242881</guid>
      <dc:creator>tamotsu</dc:creator>
      <dc:date>2025-12-15T05:39:04Z</dc:date>
    </item>
    <item>
      <title>Re: No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2262659#M242887</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Please ensure the clock is not gated and has been generated. If the clock is confirmed to be correct, then check the permission settings in RDC.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Mon, 15 Dec 2025 09:43:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2262659#M242887</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-12-15T09:43:21Z</dc:date>
    </item>
    <item>
      <title>Re: No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2263453#M242909</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;Zhiming.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I tried changing the CCM and RCD settings but nothing changed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So I checked the voltage with an oscilloscope.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The FUSE_FSOURCE voltage is 1.8v.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I set PMU_REG_1P0D to 0x210F3, but the PCIE_VPH terminal and others remained at 0V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What could be the cause?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Dec 2025 08:35:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2263453#M242909</guid>
      <dc:creator>tamotsu</dc:creator>
      <dc:date>2025-12-16T08:35:44Z</dc:date>
    </item>
    <item>
      <title>Re: No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2265556#M242955</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Zhiming.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There was a mistake in what I wrote yesterday.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When 0x00031077 was written to "PMU_REG_1P0Dn", the "VDD_1P0_CAP" pin output 1.0V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I cannot find any instructions on how to set the "VDDA_PHY_1P8" switch in Figure 5-23 of the reference manual and on Sheet 5 of the SABRE board schematic. Therefore, "VDDA_PHY_1P8" remains at 0V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please give me some advice.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regarding your advice, "the clock is not gated and has been generated," I have no way to confirm this with an oscilloscope.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please give me some advice.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Dec 2025 00:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2265556#M242955</guid>
      <dc:creator>tamotsu</dc:creator>
      <dc:date>2025-12-18T00:45:20Z</dc:date>
    </item>
    <item>
      <title>Re: No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2265777#M242964</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203270"&gt;@tamotsu&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I know you might be bringing up a baremetal system, but I'd like to discuss what PCIe requires from Linux.&lt;/P&gt;
&lt;P&gt;For PCIe itself, needs correct three key resources: clock, power, reset timing.&lt;/P&gt;
&lt;P&gt;1.&amp;nbsp; You need to make sure that these three clocks are generated and ungate.&lt;/P&gt;
&lt;P&gt;2. Make sure pcie power domain is opened in GPC.&lt;/P&gt;
&lt;P&gt;After doing these two steps, at least the register can be read.&lt;/P&gt;
&lt;P&gt;3. Perfom correct reset timing referring the pcie driver: drivers/pci/controller/dwc/pci-imx6.c.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;			clocks = &amp;lt;&amp;amp;clks IMX7D_PCIE_CTRL_ROOT_CLK&amp;gt;,
				 &amp;lt;&amp;amp;clks IMX7D_PLL_ENET_MAIN_100M_CLK&amp;gt;,
				 &amp;lt;&amp;amp;clks IMX7D_PCIE_PHY_ROOT_CLK&amp;gt;;
			clock-names = "pcie", "pcie_bus", "pcie_phy";
			assigned-clocks = &amp;lt;&amp;amp;clks IMX7D_PCIE_CTRL_ROOT_SRC&amp;gt;,
					  &amp;lt;&amp;amp;clks IMX7D_PCIE_PHY_ROOT_SRC&amp;gt;;
			assigned-clock-parents = &amp;lt;&amp;amp;clks IMX7D_PLL_ENET_MAIN_250M_CLK&amp;gt;,
						 &amp;lt;&amp;amp;clks IMX7D_PLL_ENET_MAIN_100M_CLK&amp;gt;;

			fsl,max-link-speed = &amp;lt;2&amp;gt;;
			power-domains = &amp;lt;&amp;amp;pgc_pcie_phy&amp;gt;;
			resets = &amp;lt;&amp;amp;src IMX7_RESET_PCIEPHY&amp;gt;,
				 &amp;lt;&amp;amp;src IMX7_RESET_PCIE_CTRL_APPS_EN&amp;gt;,
				 &amp;lt;&amp;amp;src IMX7_RESET_PCIE_CTRL_APPS_TURNOFF&amp;gt;;
			reset-names = "pciephy", "apps", "turnoff";









gpc: gpc@303a0000 {
				compatible = "fsl,imx7d-gpc";
				reg = &amp;lt;0x303a0000 0x10000&amp;gt;;
				interrupt-controller;
				interrupts = &amp;lt;GIC_SPI 87 IRQ_TYPE_LEVEL_HIGH&amp;gt;;
				#interrupt-cells = &amp;lt;3&amp;gt;;
				interrupt-parent = &amp;lt;&amp;amp;intc&amp;gt;;
				fsl,mf-mix-wakeup-irq = &amp;lt;0x54410000 0xc00 0x0 0x1040640&amp;gt;;

				pgc {
					#address-cells = &amp;lt;1&amp;gt;;
					#size-cells = &amp;lt;0&amp;gt;;

					pgc_mipi_phy: power-domain@0 {
						#power-domain-cells = &amp;lt;0&amp;gt;;
						reg = &amp;lt;0&amp;gt;;
						power-supply = &amp;lt;&amp;amp;reg_1p0d&amp;gt;;
					};

					pgc_pcie_phy: power-domain@1 {
						#power-domain-cells = &amp;lt;0&amp;gt;;
						reg = &amp;lt;1&amp;gt;;
						power-supply = &amp;lt;&amp;amp;reg_1p0d&amp;gt;;
					};

					pgc_hsic_phy: power-domain@2 {
						#power-domain-cells = &amp;lt;0&amp;gt;;
						reg = &amp;lt;2&amp;gt;;
						power-supply = &amp;lt;&amp;amp;reg_1p2&amp;gt;;
					};
				};
			};&lt;/LI-CODE&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Thu, 18 Dec 2025 07:24:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2265777#M242964</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-12-18T07:24:58Z</dc:date>
    </item>
    <item>
      <title>Re: No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2266563#M242985</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788" target="_self"&gt;&lt;SPAN class=""&gt;Zhiming_Liu&lt;/SPAN&gt;&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;I'm debugging PCIE in u-boot.&lt;BR /&gt;u-boot reads the contents of the device tree (fsl, imx6q-pcie) and executes imx_pciw_dm_probe().&lt;BR /&gt;The function imx_pciw_dm_probe() jumps to the function imx_pcie_link_up().&lt;BR /&gt;At the beginning of this function, there is a process to read the PCIE "Status and Command Register (0x33800004)".&lt;BR /&gt;This process results in no response.&lt;BR /&gt;The result was the same even with the Device tree information you provided.&lt;BR /&gt;The registers did not reflect the contents of the Device tree.&lt;/P&gt;&lt;P&gt;So I set the following registers:&lt;BR /&gt;　　PMU_REG_1P0D 0x00021079&lt;BR /&gt;　　SRC_PCIEPHY_RCR 0x00000000&lt;BR /&gt;　　CCM_TARGET_ROOT PCIE 0x12000000&lt;BR /&gt;　　CCM_TARGET_ROOT PHY 0x11000000&lt;BR /&gt;　　CCM_CCGR96 0x00000003&lt;/P&gt;&lt;P&gt;I did not change the following registers.&lt;BR /&gt;PDC_PDAP45 0x000000FF&lt;BR /&gt;PDC_MDA2 0x00000000&lt;/P&gt;&lt;P&gt;Even with this setting, when I load 0x33800000 in the debugger, there is no response.&lt;/P&gt;&lt;P&gt;Next I thought that the reason why "VDDA_PHY_1P8" remained at 0V was related to the GPC.&lt;BR /&gt;I set "PGA CPU mapping(0x303a00ec) to 0x09.&lt;BR /&gt;I wrote 0x01 to "CPU GPC software power up trigger (0x303a00f0)" but it remained 0x00.&lt;BR /&gt;Also, when I wrote 0x02 to "PU GPC software power up trigger (0x303a00f8)", the contents of DRAM changed.&lt;/P&gt;&lt;P&gt;What other registers should I set?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Fri, 19 Dec 2025 06:54:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2266563#M242985</guid>
      <dc:creator>tamotsu</dc:creator>
      <dc:date>2025-12-19T06:54:44Z</dc:date>
    </item>
    <item>
      <title>Re: No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2267475#M243000</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203270"&gt;@tamotsu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You might want to take a look at the patch below for some additional ideas. The overall porting should be based on the software framework rather than directly modifying registers.&amp;nbsp; It looks like uboot has i.MX7D SRC driver.&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Add-i-MX8MPlus-pci-driver-in-uboot/ta-p/1753246" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Add-i-MX8MPlus-pci-driver-in-uboot/ta-p/1753246&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Mon, 22 Dec 2025 07:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2267475#M243000</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-12-22T07:09:04Z</dc:date>
    </item>
    <item>
      <title>Re: No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2267927#M243025</link>
      <description>&lt;P&gt;Hello Zhiming_Liu.&lt;BR /&gt;Regarding the support I received from you, I am having trouble with the i.MX8 processing, which is a preliminary step.&lt;BR /&gt;I referred to "5.5.9.5 Example Code 4" in the Reference Manual.&lt;BR /&gt;reg32_write (GPC_IPS_BASE_ADDR + 0xF8 , *** | 0x2 );&lt;BR /&gt;After running this code, the MPU becomes unresponsive.&lt;BR /&gt;However, there is no problem with values ​​other than PCIE_PHY.&lt;/P&gt;&lt;P&gt;Could you please tell me what to set and how to set it before running u-boot/drivers/pci/pcie_imx.c@probe(struct udevice *dev)?&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Dec 2025 04:31:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2267927#M243025</guid>
      <dc:creator>tamotsu</dc:creator>
      <dc:date>2025-12-23T04:31:34Z</dc:date>
    </item>
    <item>
      <title>Re: No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2268017#M243029</link>
      <description>&lt;P&gt;Hello Zhiming_Liu.&lt;/P&gt;&lt;P&gt;The IMX7DSABRE has a Mini PCIE port.&lt;BR /&gt;I am wondering why u-boot does not have the source code to set the PCIE clock, power, etc. of the IMX7DSABRE.&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Dec 2025 07:32:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2268017#M243029</guid>
      <dc:creator>tamotsu</dc:creator>
      <dc:date>2025-12-23T07:32:17Z</dc:date>
    </item>
    <item>
      <title>Re: No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2268022#M243031</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203270"&gt;@tamotsu&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;The PCIe driver is maintained by mainline, not NXP, so missing some code is normal. You can refer the i.MX7D Linux PCIe driver to port it in uboot. The pci_imx.c also refers the Linux kernel driver.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Tue, 23 Dec 2025 07:44:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2268022#M243031</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-12-23T07:44:55Z</dc:date>
    </item>
    <item>
      <title>Re: No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2268368#M243047</link>
      <description>&lt;P&gt;Hello Zhiming_Liu.&lt;/P&gt;&lt;P&gt;I understand the advice.&lt;BR /&gt;I will read the reference manual again and try again.&lt;/P&gt;&lt;P&gt;BEst Regards.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Dec 2025 00:07:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2268368#M243047</guid>
      <dc:creator>tamotsu</dc:creator>
      <dc:date>2025-12-24T00:07:22Z</dc:date>
    </item>
    <item>
      <title>Re: No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2268766#M243059</link>
      <description>&lt;P&gt;Hello Zhiming_Liu.&lt;/P&gt;&lt;P&gt;I finally found out why it wasn't responding.&lt;BR /&gt;I made the SABRE circuit's "SW2_1V8" to "VDDA_1P8_01(pin-V6)" the same, but I found that the inductance resistance value was too large.&lt;BR /&gt;The moment I set GPC_PU_PGC_SW_PUP_REG, the voltage of "VDDA_1P8_01(V6)" dropped by 0.2V in 2uSec.&lt;BR /&gt;As a result, VDDA_PHY_1P8 only rose to 0.35V.&lt;BR /&gt;When I shorted this inductance, VDDA_PHY_1P8 became 1.8V.&lt;/P&gt;&lt;P&gt;I thought that VDDA_PHY_1P8 would be fine even if the input voltage dropped a little, but I found that this was not the case.&lt;/P&gt;&lt;P&gt;Thank you very much for all your advice.&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;</description>
      <pubDate>Thu, 25 Dec 2025 01:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2268766#M243059</guid>
      <dc:creator>tamotsu</dc:creator>
      <dc:date>2025-12-25T01:55:34Z</dc:date>
    </item>
    <item>
      <title>Re: No response when reading Status and Command Register in PCIE of i.MX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2268771#M243060</link>
      <description>&lt;P&gt;Hello Zhiming_Liu.&lt;/P&gt;&lt;P&gt;I finally found out why it wasn't responding.&lt;/P&gt;&lt;P&gt;I made the SABRE circuit's "SW2_1V8" to "VDDA_1P8_01(pin-V6)" the same.&lt;/P&gt;&lt;P&gt;But I found that the inductance resistance value was too large.&lt;/P&gt;&lt;P&gt;The moment I set GPC_PU_PGC_SW_PUP_REG, the voltage of "VDDA_1P8_01(V6)" dropped by 0.2V in 2uSec.&lt;/P&gt;&lt;P&gt;As a result, VDDA_PHY_1P8 only rose to 0.35V.&lt;/P&gt;&lt;P&gt;When I shorted this inductance, VDDA_PHY_1P8 became 1.8V.&lt;/P&gt;&lt;P&gt;I thought that VDDA_PHY_1P8 would be fine even if the input voltage dropped a little, but I found that this was not the case.&lt;/P&gt;&lt;P&gt;Thank you very much for all your advice.&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;</description>
      <pubDate>Thu, 25 Dec 2025 02:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-response-when-reading-Status-and-Command-Register-in-PCIE-of/m-p/2268771#M243060</guid>
      <dc:creator>tamotsu</dc:creator>
      <dc:date>2025-12-25T02:00:47Z</dc:date>
    </item>
  </channel>
</rss>