<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Can RTC_XTALI connect to RTC SQW</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-RTC-XTALI-connect-to-RTC-SQW/m-p/2264574#M242942</link>
    <description>&lt;P&gt;Here you can not connect the RTC SQW to the&amp;nbsp;RTC_XTALI , for the RTC_XTALI is the&amp;nbsp;analog clock input.&lt;/P&gt;
&lt;P&gt;CKIL (Clock Input Low) is a dedicated pin used to receive external 32.768 kHz digital clock signals, so you need to connect the RTC SQW to the&amp;nbsp;CKIL on the i.MX6Q side.&amp;nbsp; You need to follow the circuilt recommend.&lt;/P&gt;
&lt;P&gt;Any questions contact us freely.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 17 Dec 2025 08:42:05 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2025-12-17T08:42:05Z</dc:date>
    <item>
      <title>Can RTC_XTALI connect to RTC SQW</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-RTC-XTALI-connect-to-RTC-SQW/m-p/2252653#M242549</link>
      <description>&lt;P&gt;The BLOCK diagram is as follows:&lt;BR /&gt;&lt;BR /&gt;&lt;U&gt;&lt;STRONG&gt;Phenomenon:&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;After powering on, the 3.3V voltage drops to 3.0V. When the connection between RTC_XTALI and SQW is disconnected, the voltage returns to 3.3V.&lt;BR /&gt;&lt;U&gt;&lt;STRONG&gt;Issue: &lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;Can the SQW of the RTC chip be connected directly to the CPU's RTC_XTALI interface?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;U&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="BLOCK.png" style="width: 678px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/368100iCC6B52BB8F4D4079/image-dimensions/678x524?v=v2" width="678" height="524" role="button" title="BLOCK.png" alt="BLOCK.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;BLOCK.png&lt;/span&gt;&lt;/span&gt;&lt;/U&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Dec 2025 02:24:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-RTC-XTALI-connect-to-RTC-SQW/m-p/2252653#M242549</guid>
      <dc:creator>WSLJ</dc:creator>
      <dc:date>2025-12-02T02:24:20Z</dc:date>
    </item>
    <item>
      <title>Re: Can RTC_XTALI connect to RTC SQW</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-RTC-XTALI-connect-to-RTC-SQW/m-p/2264574#M242942</link>
      <description>&lt;P&gt;Here you can not connect the RTC SQW to the&amp;nbsp;RTC_XTALI , for the RTC_XTALI is the&amp;nbsp;analog clock input.&lt;/P&gt;
&lt;P&gt;CKIL (Clock Input Low) is a dedicated pin used to receive external 32.768 kHz digital clock signals, so you need to connect the RTC SQW to the&amp;nbsp;CKIL on the i.MX6Q side.&amp;nbsp; You need to follow the circuilt recommend.&lt;/P&gt;
&lt;P&gt;Any questions contact us freely.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Dec 2025 08:42:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-RTC-XTALI-connect-to-RTC-SQW/m-p/2264574#M242942</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-12-17T08:42:05Z</dc:date>
    </item>
  </channel>
</rss>