<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Inquiry Regarding Simultaneous Use of Parallel CSI, MIPI CSI, and USB3 OTG on i.MX 8X Family</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Inquiry-Regarding-Simultaneous-Use-of-Parallel-CSI-MIPI-CSI-and/m-p/2256909#M242719</link>
    <description>&lt;P&gt;for your case, I suggest that you can refer to the imx8mp, which has dual mipi csi camera, and imx8mp is cheaper than imx8x&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/i.MX8MPLUS" target="_blank"&gt;https://www.nxp.com/products/i.MX8MPLUS&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 08 Dec 2025 08:10:21 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2025-12-08T08:10:21Z</dc:date>
    <item>
      <title>Inquiry Regarding Simultaneous Use of Parallel CSI, MIPI CSI, and USB3 OTG on i.MX 8X Family</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inquiry-Regarding-Simultaneous-Use-of-Parallel-CSI-MIPI-CSI-and/m-p/2256641#M242713</link>
      <description>&lt;P&gt;I am currently planning to use a parallel camera and a MIPI CSI camera simultaneously, and I need to transmit the data from both cameras through USB 3.0.&lt;/P&gt;&lt;P&gt;Based on the i.MX 8X Family Block Diagram, I understand that the device provides one Parallel CSI, one MIPI CSI, and one USB3 OTG with PHY.&lt;BR /&gt;Could you please confirm whether these three interfaces can be used concurrently from a hardware perspective?&lt;/P&gt;&lt;P&gt;Additionally, I would appreciate your recommendation on which product family within the i.MX series would be the most suitable for this type of camera-streaming and USB transmission application.&lt;/P&gt;&lt;P&gt;Thank you for your assistance. I appreciate your support and look forward to your response.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;seobi&lt;/P&gt;</description>
      <pubDate>Mon, 08 Dec 2025 04:07:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inquiry-Regarding-Simultaneous-Use-of-Parallel-CSI-MIPI-CSI-and/m-p/2256641#M242713</guid>
      <dc:creator>seobi</dc:creator>
      <dc:date>2025-12-08T04:07:17Z</dc:date>
    </item>
    <item>
      <title>Re: Inquiry Regarding Simultaneous Use of Parallel CSI, MIPI CSI, and USB3 OTG on i.MX 8X Family</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inquiry-Regarding-Simultaneous-Use-of-Parallel-CSI-MIPI-CSI-and/m-p/2256909#M242719</link>
      <description>&lt;P&gt;for your case, I suggest that you can refer to the imx8mp, which has dual mipi csi camera, and imx8mp is cheaper than imx8x&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/i.MX8MPLUS" target="_blank"&gt;https://www.nxp.com/products/i.MX8MPLUS&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Dec 2025 08:10:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inquiry-Regarding-Simultaneous-Use-of-Parallel-CSI-MIPI-CSI-and/m-p/2256909#M242719</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-12-08T08:10:21Z</dc:date>
    </item>
    <item>
      <title>Re: Inquiry Regarding Simultaneous Use of Parallel CSI, MIPI CSI, and USB3 OTG on i.MX 8X Family</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inquiry-Regarding-Simultaneous-Use-of-Parallel-CSI-MIPI-CSI-and/m-p/2257497#M242738</link>
      <description>We have confirmed that the i.MX 8M Plus provides two MIPI-CSI interfaces, but we were not able to find any information regarding a parallel CSI interface.&lt;BR /&gt;Could you please clarify whether a parallel camera port is also supported?</description>
      <pubDate>Tue, 09 Dec 2025 00:28:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inquiry-Regarding-Simultaneous-Use-of-Parallel-CSI-MIPI-CSI-and/m-p/2257497#M242738</guid>
      <dc:creator>seobi</dc:creator>
      <dc:date>2025-12-09T00:28:46Z</dc:date>
    </item>
    <item>
      <title>Re: Inquiry Regarding Simultaneous Use of Parallel CSI, MIPI CSI, and USB3 OTG on i.MX 8X Family</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inquiry-Regarding-Simultaneous-Use-of-Parallel-CSI-MIPI-CSI-and/m-p/2257667#M242751</link>
      <description>&lt;P&gt;must you use parallel csi? if yes, imx8mp doesn't have this, for imx8 series, only imx8qxp has parallel csi interface, and can meet your request&lt;/P&gt;</description>
      <pubDate>Tue, 09 Dec 2025 06:21:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inquiry-Regarding-Simultaneous-Use-of-Parallel-CSI-MIPI-CSI-and/m-p/2257667#M242751</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-12-09T06:21:28Z</dc:date>
    </item>
  </channel>
</rss>