<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8mp HDMI EDDC I2C configuration in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8mp-HDMI-EDDC-I2C-configuration/m-p/2256202#M242685</link>
    <description>&lt;P&gt;I'm facing the same problem, but the pinout on my HDMI is correct. I was able to read EDID information from one display, but when I connect a different model, the I2C communication stops right after the first 8 clocks, since no acknowledge is send back from the display. Trying to read out the EDID information with an external Microcontroller over the same HDMI cable works fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Were you able to fix the issue with the tight SDA hold timing? Could you please share the solution.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;BR Gabriel&lt;/P&gt;</description>
    <pubDate>Fri, 05 Dec 2025 15:06:32 GMT</pubDate>
    <dc:creator>stollg</dc:creator>
    <dc:date>2025-12-05T15:06:32Z</dc:date>
    <item>
      <title>IMX8mp HDMI EDDC I2C configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8mp-HDMI-EDDC-I2C-configuration/m-p/1823537#M220932</link>
      <description>&lt;P&gt;We are bringing up a new imx8mp board that we have designed. All is functional except the HDMI interface. It almost works with some monitors.&lt;/P&gt;&lt;P&gt;Basically the issue is that the system can't read the DDC data across the HDMI's I2C bus. The design we have is identical to one we have used on another imx8mp board, but we are using the latest NXP 6.1.55_2.2.0 Yocto Linux system.&lt;/P&gt;&lt;P&gt;Looking at the HDMI I2C signals to the monitor it looks like the SCL to SDA timings are a bit off. SDA is changing very close to the SCL -ve transition and we wonder if this could be the cause.&lt;/P&gt;&lt;P&gt;This I2C bus appears to be driven by a special I2C EDID E-DDC interface in the imx8mp. I can't see any particular settings for this in the DTS.&lt;/P&gt;&lt;P&gt;1. Where is the configuration for this I2C type of device ?&lt;/P&gt;&lt;P&gt;2. Has anyone seen this issue before ?&lt;/P&gt;&lt;P&gt;3. Any ideas ?&lt;/P&gt;</description>
      <pubDate>Thu, 07 Mar 2024 17:00:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8mp-HDMI-EDDC-I2C-configuration/m-p/1823537#M220932</guid>
      <dc:creator>TerryBarnaby1</dc:creator>
      <dc:date>2024-03-07T17:00:29Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8mp HDMI EDDC I2C configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8mp-HDMI-EDDC-I2C-configuration/m-p/1823550#M220933</link>
      <description>&lt;P&gt;This is what the HDMI I2C lines when trying to read I2C device 0x50 address 0. There is no ack from the monitor.&lt;/P&gt;</description>
      <pubDate>Thu, 07 Mar 2024 17:19:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8mp-HDMI-EDDC-I2C-configuration/m-p/1823550#M220933</guid>
      <dc:creator>TerryBarnaby1</dc:creator>
      <dc:date>2024-03-07T17:19:42Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8mp HDMI EDDC I2C configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8mp-HDMI-EDDC-I2C-configuration/m-p/1823849#M220952</link>
      <description>&lt;P&gt;I have found the issue. We are using a micro HDMI connector on this board. We used a Wurth 685119248123 part and went with the pinout defined on that datasheet. This was wrong. They have updated the datasheet to a 0002.000 version.&lt;/P&gt;&lt;P&gt;However the DDC I2C timings do look a little tight to me. I tried increasing the value in the EDDC I2C DDC SDA Hold Register and timings look better to me.&lt;/P&gt;&lt;P&gt;Sorry for the noise.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Mar 2024 05:56:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8mp-HDMI-EDDC-I2C-configuration/m-p/1823849#M220952</guid>
      <dc:creator>TerryBarnaby1</dc:creator>
      <dc:date>2024-03-08T05:56:38Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8mp HDMI EDDC I2C configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8mp-HDMI-EDDC-I2C-configuration/m-p/2256202#M242685</link>
      <description>&lt;P&gt;I'm facing the same problem, but the pinout on my HDMI is correct. I was able to read EDID information from one display, but when I connect a different model, the I2C communication stops right after the first 8 clocks, since no acknowledge is send back from the display. Trying to read out the EDID information with an external Microcontroller over the same HDMI cable works fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Were you able to fix the issue with the tight SDA hold timing? Could you please share the solution.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;BR Gabriel&lt;/P&gt;</description>
      <pubDate>Fri, 05 Dec 2025 15:06:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8mp-HDMI-EDDC-I2C-configuration/m-p/2256202#M242685</guid>
      <dc:creator>stollg</dc:creator>
      <dc:date>2025-12-05T15:06:32Z</dc:date>
    </item>
  </channel>
</rss>