<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Camera Compatible with i.MX 93 FRDM Development Board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Camera-Compatible-with-i-MX-93-FRDM-Development-Board/m-p/2255169#M242633</link>
    <description>&lt;P&gt;did you add the new camera in the dts files? could you share the logfile and your develop code?&lt;/P&gt;</description>
    <pubDate>Thu, 04 Dec 2025 09:38:38 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2025-12-04T09:38:38Z</dc:date>
    <item>
      <title>Camera Compatible with i.MX 93 FRDM Development Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-Compatible-with-i-MX-93-FRDM-Development-Board/m-p/2254873#M242624</link>
      <description>&lt;P&gt;Hi, im facing a problem with the camera csi2 of the FRDM i.MX 93 Board.&lt;BR /&gt;When i read the hardware reference of that board on the CSI port P6. i see that, theoretically, if i using a camera like Raspberry Pi camera module V2 (with 15P 1mm FPC) then convert using 15P to 22P 0.5mm FPC, it can plug into the camera connector of that FRDM board.&amp;nbsp;&lt;BR /&gt;By the way, when i plug it on the board and boot it. The logs show that, no module is load via 'lsmod' command.&amp;nbsp;&lt;BR /&gt;As expected, im using this imx219 driver, and my kernel has prebuilt kernel module imx219=m. But it's not showing anything at all.&amp;nbsp;&lt;BR /&gt;&lt;LI-PRODUCT title="IMX93QSB" id="IMX93QSB"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp; &lt;LI-PRODUCT title="FRDM-i.MX93" id="FRDM-iMX93"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Dec 2025 06:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-Compatible-with-i-MX-93-FRDM-Development-Board/m-p/2254873#M242624</guid>
      <dc:creator>Kyuubi0323</dc:creator>
      <dc:date>2025-12-04T06:32:20Z</dc:date>
    </item>
    <item>
      <title>Re: Camera Compatible with i.MX 93 FRDM Development Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-Compatible-with-i-MX-93-FRDM-Development-Board/m-p/2255169#M242633</link>
      <description>&lt;P&gt;did you add the new camera in the dts files? could you share the logfile and your develop code?&lt;/P&gt;</description>
      <pubDate>Thu, 04 Dec 2025 09:38:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-Compatible-with-i-MX-93-FRDM-Development-Board/m-p/2255169#M242633</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-12-04T09:38:38Z</dc:date>
    </item>
  </channel>
</rss>