<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX 95 EVK boot process log in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-95-EVK-boot-process-log/m-p/2254640#M242617</link>
    <description>&lt;P&gt;Hi NXP Experts,&lt;/P&gt;&lt;P&gt;We are studying the boot process of the i.MX 95 with Yocto Linux image and would like to understand the boot flow more deeply.&lt;BR /&gt;Is there any detailed documentation on the boot process sequence?&lt;BR /&gt;Also, could you provide a hardware boot log from an i.MX 95 EVK board would be very helpful for our reference.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 03 Dec 2025 23:20:26 GMT</pubDate>
    <dc:creator>chienhau</dc:creator>
    <dc:date>2025-12-03T23:20:26Z</dc:date>
    <item>
      <title>i.MX 95 EVK boot process log</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-95-EVK-boot-process-log/m-p/2254640#M242617</link>
      <description>&lt;P&gt;Hi NXP Experts,&lt;/P&gt;&lt;P&gt;We are studying the boot process of the i.MX 95 with Yocto Linux image and would like to understand the boot flow more deeply.&lt;BR /&gt;Is there any detailed documentation on the boot process sequence?&lt;BR /&gt;Also, could you provide a hardware boot log from an i.MX 95 EVK board would be very helpful for our reference.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 03 Dec 2025 23:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-95-EVK-boot-process-log/m-p/2254640#M242617</guid>
      <dc:creator>chienhau</dc:creator>
      <dc:date>2025-12-03T23:20:26Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 95 EVK boot process log</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-95-EVK-boot-process-log/m-p/2255598#M242659</link>
      <description>&lt;P&gt;the i.mx95 is still under preproduction, all of materials are available on the official website&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/i.MX95" target="_blank"&gt;https://www.nxp.com/products/i.MX95&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;for the boot log, pls refer to the enclosed file, I used&amp;nbsp;imx95-19x19-evk-it6263-lvds0.dtb and connect with HDMI&lt;/P&gt;</description>
      <pubDate>Fri, 05 Dec 2025 00:45:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-95-EVK-boot-process-log/m-p/2255598#M242659</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-12-05T00:45:28Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 95 EVK boot process log</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-95-EVK-boot-process-log/m-p/2348792#M244839</link>
      <description>HI Joanxie:&lt;BR /&gt;Thanks for your previous imx95 boot log, it's very helpful.&lt;BR /&gt;&lt;BR /&gt;We are currently studying i.MX 952 (&lt;A href="https://www.nxp.com/products/i.MX-952" target="_blank"&gt;https://www.nxp.com/products/i.MX-952&lt;/A&gt;) and would like to kindly ask if the corresponding boot log is available for reference and debugging.&lt;BR /&gt;Thank you</description>
      <pubDate>Fri, 10 Apr 2026 02:36:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-95-EVK-boot-process-log/m-p/2348792#M244839</guid>
      <dc:creator>chienhau</dc:creator>
      <dc:date>2026-04-10T02:36:58Z</dc:date>
    </item>
  </channel>
</rss>