<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Core Allocation CPU Affinity Support for Applications &amp;amp; systemd Services on i.MX8QXP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Core-Allocation-CPU-Affinity-Support-for-Applications-amp/m-p/2250442#M242464</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;# CPU Affinity Support for i.MX8QXP&lt;BR /&gt;&lt;BR /&gt;The i.MX8QXP platform with its 4 Cortex-A35 cores supports multiple CPU affinity mechanisms to optimize utilization for specific applications and systemd services.&lt;BR /&gt;&lt;BR /&gt;## Supported CPU Affinity Mechanisms&lt;BR /&gt;&lt;BR /&gt;1. **taskset Command**&lt;BR /&gt;- Assign specific applications to run on designated cores&lt;BR /&gt;- Example: `taskset -c 0,1 your_application`&lt;BR /&gt;- For systemd services: Use `CPUAffinity=` directive in service unit files&lt;BR /&gt;&lt;BR /&gt;2. **Kernel Boot Parameters**&lt;BR /&gt;- `isolcpus=` - Isolates CPUs from the kernel scheduler&lt;BR /&gt;- `nohz_full=` - Reduces timer interrupts on specified cores&lt;BR /&gt;- `rcu_nocbs=` - Moves RCU callback processing off specified cores&lt;BR /&gt;- `irqaffinity=` - Directs hardware interrupts to specific cores&lt;BR /&gt;&lt;BR /&gt;3. **Systemd Service Configuration**&lt;BR /&gt;- Add to your service unit files:&lt;BR /&gt;```&lt;BR /&gt;[Service]&lt;BR /&gt;CPUAffinity=0-1 # Restrict to cores 0 and 1&lt;BR /&gt;```&lt;BR /&gt;&lt;BR /&gt;4. **Runtime CPU Management**&lt;BR /&gt;- Enable/disable cores dynamically:&lt;BR /&gt;```&lt;BR /&gt;echo 0 &amp;gt; /sys/devices/system/cpu/cpu3/online&lt;BR /&gt;```&lt;BR /&gt;&lt;BR /&gt;5. **Process/Thread Specific Affinity**&lt;BR /&gt;- In C/C++ applications: `pthread_setaffinity_np()`&lt;BR /&gt;- For running processes: `taskset -p -c 2,3 [PID]`&lt;BR /&gt;&lt;BR /&gt;For optimal deterministic performance, use a combination of `isolcpus`, `nohz_full`, and `irqaffinity` boot parameters to dedicate specific cores to your critical applications while keeping system services on separate cores.&lt;BR /&gt;&lt;BR /&gt;Note that complete isolation isn't entirely possible as certain kernel threads (migration, ksoftirqd, kworker) will remain present on all cores, but their impact on performance is minimal.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 27 Nov 2025 13:57:34 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2025-11-27T13:57:34Z</dc:date>
    <item>
      <title>Core Allocation CPU Affinity Support for Applications &amp; systemd Services on i.MX8QXP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Core-Allocation-CPU-Affinity-Support-for-Applications-amp/m-p/2249354#M242436</link>
      <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;We are working on the i.MX8QXP platform running Yocto Linux Nanbield (custom HMI build).&lt;BR /&gt;Our setup uses &lt;STRONG&gt;4 Cortex-A35 cores&lt;/STRONG&gt;, and we want to optimize CPU utilization for specific applications and systemd services.&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;Assign a systemd service to run only on a particular CPU core&lt;/STRONG&gt;?&lt;BR /&gt;We are exploring CPU load balancing and deterministic performance for certain tasks within our custom HMI application stack.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Please advise on:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Supported CPU affinity mechanisms on i.MX8QXP&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Any NXP documentation references or examples for CPU isolation/assignment&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Wed, 26 Nov 2025 11:44:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Core-Allocation-CPU-Affinity-Support-for-Applications-amp/m-p/2249354#M242436</guid>
      <dc:creator>Ram2</dc:creator>
      <dc:date>2025-11-26T11:44:40Z</dc:date>
    </item>
    <item>
      <title>Re: Core Allocation CPU Affinity Support for Applications &amp; systemd Services on i.MX8QXP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Core-Allocation-CPU-Affinity-Support-for-Applications-amp/m-p/2250442#M242464</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;# CPU Affinity Support for i.MX8QXP&lt;BR /&gt;&lt;BR /&gt;The i.MX8QXP platform with its 4 Cortex-A35 cores supports multiple CPU affinity mechanisms to optimize utilization for specific applications and systemd services.&lt;BR /&gt;&lt;BR /&gt;## Supported CPU Affinity Mechanisms&lt;BR /&gt;&lt;BR /&gt;1. **taskset Command**&lt;BR /&gt;- Assign specific applications to run on designated cores&lt;BR /&gt;- Example: `taskset -c 0,1 your_application`&lt;BR /&gt;- For systemd services: Use `CPUAffinity=` directive in service unit files&lt;BR /&gt;&lt;BR /&gt;2. **Kernel Boot Parameters**&lt;BR /&gt;- `isolcpus=` - Isolates CPUs from the kernel scheduler&lt;BR /&gt;- `nohz_full=` - Reduces timer interrupts on specified cores&lt;BR /&gt;- `rcu_nocbs=` - Moves RCU callback processing off specified cores&lt;BR /&gt;- `irqaffinity=` - Directs hardware interrupts to specific cores&lt;BR /&gt;&lt;BR /&gt;3. **Systemd Service Configuration**&lt;BR /&gt;- Add to your service unit files:&lt;BR /&gt;```&lt;BR /&gt;[Service]&lt;BR /&gt;CPUAffinity=0-1 # Restrict to cores 0 and 1&lt;BR /&gt;```&lt;BR /&gt;&lt;BR /&gt;4. **Runtime CPU Management**&lt;BR /&gt;- Enable/disable cores dynamically:&lt;BR /&gt;```&lt;BR /&gt;echo 0 &amp;gt; /sys/devices/system/cpu/cpu3/online&lt;BR /&gt;```&lt;BR /&gt;&lt;BR /&gt;5. **Process/Thread Specific Affinity**&lt;BR /&gt;- In C/C++ applications: `pthread_setaffinity_np()`&lt;BR /&gt;- For running processes: `taskset -p -c 2,3 [PID]`&lt;BR /&gt;&lt;BR /&gt;For optimal deterministic performance, use a combination of `isolcpus`, `nohz_full`, and `irqaffinity` boot parameters to dedicate specific cores to your critical applications while keeping system services on separate cores.&lt;BR /&gt;&lt;BR /&gt;Note that complete isolation isn't entirely possible as certain kernel threads (migration, ksoftirqd, kworker) will remain present on all cores, but their impact on performance is minimal.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Nov 2025 13:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Core-Allocation-CPU-Affinity-Support-for-Applications-amp/m-p/2250442#M242464</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-11-27T13:57:34Z</dc:date>
    </item>
  </channel>
</rss>