<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Unusual question of the electricity on imx258 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unusual-question-of-the-electricity-on-imx258/m-p/156718#M2421</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The first picture, Vout is the voltage of CPU pin 3.3V, Iout is the current of CPU pin 3.3V. &lt;BR /&gt;Before power-on, 3.3V remained on circuit board about 200mV, after power-on, the oscillograph captured current 2.7A consumed. Power system detects abnormal current to enter the protected status while closing output.&lt;/P&gt;&lt;P&gt;Question:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;why the residual voltage can cause CPU's NVCC_XXX (digital terminal) current consumption so much&lt;BR /&gt;2.What is the residual voltage, the system will not consume high current?&lt;BR /&gt;3.What better way to avoid this anomaly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Jun 2011 07:37:11 GMT</pubDate>
    <dc:creator>abelguan</dc:creator>
    <dc:date>2011-06-03T07:37:11Z</dc:date>
    <item>
      <title>Unusual question of the electricity on imx258</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unusual-question-of-the-electricity-on-imx258/m-p/156718#M2421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The first picture, Vout is the voltage of CPU pin 3.3V, Iout is the current of CPU pin 3.3V. &lt;BR /&gt;Before power-on, 3.3V remained on circuit board about 200mV, after power-on, the oscillograph captured current 2.7A consumed. Power system detects abnormal current to enter the protected status while closing output.&lt;/P&gt;&lt;P&gt;Question:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;why the residual voltage can cause CPU's NVCC_XXX (digital terminal) current consumption so much&lt;BR /&gt;2.What is the residual voltage, the system will not consume high current?&lt;BR /&gt;3.What better way to avoid this anomaly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2011 07:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unusual-question-of-the-electricity-on-imx258/m-p/156718#M2421</guid>
      <dc:creator>abelguan</dc:creator>
      <dc:date>2011-06-03T07:37:11Z</dc:date>
    </item>
  </channel>
</rss>