<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can KVM run on the i.MX93? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-KVM-run-on-the-i-MX93/m-p/2202786#M242099</link>
    <description>Thank you for the response, Salas.</description>
    <pubDate>Tue, 11 Nov 2025 14:16:54 GMT</pubDate>
    <dc:creator>FRDM-User</dc:creator>
    <dc:date>2025-11-11T14:16:54Z</dc:date>
    <item>
      <title>Can KVM run on the i.MX93?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-KVM-run-on-the-i-MX93/m-p/2202157#M242063</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Can KVM run on the i.MX93, technically? WRT virtualization, the i.MX93 only really seems to explicitly support Jailhouse... Would there be any potential challenges/risks associated with using an "unsupported" hypervisor such as KVM?&lt;BR /&gt;&lt;BR /&gt;My understanding is that there shouldn't be any issue with using KVM due to the i.MX93's A55 cores being of the Armv8-A variety, i.e. they support virtualization.&lt;BR /&gt;&lt;BR /&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Mon, 10 Nov 2025 22:11:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-KVM-run-on-the-i-MX93/m-p/2202157#M242063</guid>
      <dc:creator>FRDM-User</dc:creator>
      <dc:date>2025-11-10T22:11:39Z</dc:date>
    </item>
    <item>
      <title>Re: Can KVM run on the i.MX93?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-KVM-run-on-the-i-MX93/m-p/2202180#M242064</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256739"&gt;@FRDM-User&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;I hope you are doing very well.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;The i.MX93 family includes Arm Cortex-A55 cores, which implement the Armv8-A architecture and support hardware virtualization extensions. From a purely technical perspective, this means hypervisors such as KVM can run on the CPU.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;&lt;BR /&gt;However, NXP only validates and officially supports Jailhouse as the virtualization solution for i.MX93.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;The possible considerations to keep in mind are:&lt;/P&gt;
&lt;UL&gt;
&lt;LI class="lia-align-justify"&gt;NXP does not provide BSP integration, testing, or patches for KVM on i.MX93.&amp;nbsp;&lt;/LI&gt;
&lt;LI class="lia-align-justify"&gt;The i.MX93 does not include an IOMMU (SMMU)&lt;/LI&gt;
&lt;LI class="lia-align-justify"&gt;Jailhouse offers strong isolation and minimal overhead, while KVM introduces more complexity and may impact real-time performance&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Mon, 10 Nov 2025 23:48:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-KVM-run-on-the-i-MX93/m-p/2202180#M242064</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2025-11-10T23:48:13Z</dc:date>
    </item>
    <item>
      <title>Re: Can KVM run on the i.MX93?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-KVM-run-on-the-i-MX93/m-p/2202786#M242099</link>
      <description>Thank you for the response, Salas.</description>
      <pubDate>Tue, 11 Nov 2025 14:16:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-KVM-run-on-the-i-MX93/m-p/2202786#M242099</guid>
      <dc:creator>FRDM-User</dc:creator>
      <dc:date>2025-11-11T14:16:54Z</dc:date>
    </item>
  </channel>
</rss>