<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8mp SAI bit counter not working</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-SAI-bit-counter-not-working/m-p/2201219#M242012</link>
    <description>&lt;P&gt;I am working with the imx8mp processor, receiving serial data over SAI2.&amp;nbsp; The SAI's VERID register indicates version 3.1 with timestamp registers.&amp;nbsp; I have the SAI2 receive working and dumping the incoming data into a DMA buffer.&amp;nbsp; The master clock, bit clock, and frame clock are all generated externally.&amp;nbsp; I expected to get values in the timestamp counter (RTSR), bit counter (RBCR), and bit timestamp (RBCTR), but they stay at zero even as I am receiving valid data.&amp;nbsp; I have verified via readback that the receive timestamp control (RTCR) is 0x000003, which should allow the timestamp counter to increment even without the bit counter incrementing.&amp;nbsp; Is there anything else I need to configure to get the bit counter and timestamp working?&lt;/P&gt;</description>
    <pubDate>Sun, 09 Nov 2025 01:24:37 GMT</pubDate>
    <dc:creator>Brian_B</dc:creator>
    <dc:date>2025-11-09T01:24:37Z</dc:date>
    <item>
      <title>imx8mp SAI bit counter not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-SAI-bit-counter-not-working/m-p/2201219#M242012</link>
      <description>&lt;P&gt;I am working with the imx8mp processor, receiving serial data over SAI2.&amp;nbsp; The SAI's VERID register indicates version 3.1 with timestamp registers.&amp;nbsp; I have the SAI2 receive working and dumping the incoming data into a DMA buffer.&amp;nbsp; The master clock, bit clock, and frame clock are all generated externally.&amp;nbsp; I expected to get values in the timestamp counter (RTSR), bit counter (RBCR), and bit timestamp (RBCTR), but they stay at zero even as I am receiving valid data.&amp;nbsp; I have verified via readback that the receive timestamp control (RTCR) is 0x000003, which should allow the timestamp counter to increment even without the bit counter incrementing.&amp;nbsp; Is there anything else I need to configure to get the bit counter and timestamp working?&lt;/P&gt;</description>
      <pubDate>Sun, 09 Nov 2025 01:24:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-SAI-bit-counter-not-working/m-p/2201219#M242012</guid>
      <dc:creator>Brian_B</dc:creator>
      <dc:date>2025-11-09T01:24:37Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp SAI bit counter not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-SAI-bit-counter-not-working/m-p/2201222#M242014</link>
      <description>&lt;P&gt;Never mind - apparently the&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;regmap_read function I was using was reading back cached values.&amp;nbsp; I switched to readl and now I am getting valid values.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks anyway!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 09 Nov 2025 01:52:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-SAI-bit-counter-not-working/m-p/2201222#M242014</guid>
      <dc:creator>Brian_B</dc:creator>
      <dc:date>2025-11-09T01:52:45Z</dc:date>
    </item>
  </channel>
</rss>