<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx95 m7 core edma issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx95-m7-core-edma-issue/m-p/2195300#M241766</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Linux kernel version is 6.12.34 a clone of:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/nxp-imx/linux-imx.git" target="_blank" rel="noopener"&gt;https://github.com/nxp-imx/linux-imx.git&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here are device tree and a dtsi&lt;/P&gt;&lt;P&gt;main ucm-imx95-som.dts:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/compulab-yokneam/linux-compulab/blob/linux-compulab_v6.12.34/arch/arm64/boot/dts/compulab/ucm-imx95-som.dts" target="_blank" rel="noopener"&gt;https://github.com/compulab-yokneam/linux-compulab/blob/linux-compulab_v6.12.34/arch/arm64/boot/dts/compulab/ucm-imx95-som.dts&lt;/A&gt;&lt;/P&gt;&lt;P&gt;dtsi ucm-imx95-rpmsg.dtsi:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/compulab-yokneam/linux-compulab/blob/linux-compulab_v6.12.34/arch/arm64/boot/dts/compulab/ucm-imx95-rpmsg.dtsi" target="_blank" rel="noopener"&gt;https://github.com/compulab-yokneam/linux-compulab/blob/linux-compulab_v6.12.34/arch/arm64/boot/dts/compulab/ucm-imx95-rpmsg.dtsi&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Makefile:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/compulab-yokneam/linux-compulab/blob/linux-compulab_v6.12.34/arch/arm64/boot/dts/compulab/Makefile.ucm-imx95#L22-L23" target="_self"&gt;https://github.com/compulab-yokneam/linux-compulab/blob/linux-compulab_v6.12.34/arch/arm64/boot/dts/compulab/Makefile.ucm-imx95#L22-L23&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;imx-system-manager:&lt;/P&gt;&lt;P&gt;version:&amp;nbsp;&lt;SPAN&gt;lf-6.12.34-2.1.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;config: imx95evkrpmsg.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Valentin.&lt;/P&gt;</description>
    <pubDate>Wed, 29 Oct 2025 22:20:48 GMT</pubDate>
    <dc:creator>vraevsky</dc:creator>
    <dc:date>2025-10-29T22:20:48Z</dc:date>
    <item>
      <title>imx95 m7 core edma issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx95-m7-core-edma-issue/m-p/2194577#M241737</link>
      <description>&lt;P&gt;Dear NXP Support,&lt;/P&gt;&lt;P&gt;We have an issue with the imx95 M7 core.&lt;BR /&gt;We are using the NXP provided &lt;EM&gt;&lt;STRONG&gt;SDK_25_06_00_IMX95LPD5EVK-19.tar.gz.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;Compiled all driver_examples/lpuart:&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;edma_transfer, interrupt, interrupt_rb_transfer, interrupt_transfer, polling.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;Issued the same procedure for each one from the Linux console:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;echo stop &amp;gt; /sys/class/remoteproc/remoteproc1/state&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;echo &amp;lt;sample-name&amp;gt;.elf &amp;gt; /sys/class/remoteproc/remoteproc1/firmware&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;echo start &amp;gt; /sys/class/remoteproc/remoteproc1/state&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The M7 core serial console shows prompt, and it is possible to interact with the loaded driver.&lt;BR /&gt;Almost everything is okay, except for the lpuart_edma_transfer_cm7.elf that shows nothing on the M7 core serial console. Discovered that the driver configures the M7 serial console:&lt;BR /&gt;the M33 md command shows the correct values for the pinmux registers.&lt;/P&gt;&lt;P&gt;We’d appreciate it if you could shed light on the problem and help us in resolving the issue.&lt;/P&gt;&lt;P&gt;Thanks in advances,&lt;BR /&gt;Valentin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Oct 2025 21:41:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx95-m7-core-edma-issue/m-p/2194577#M241737</guid>
      <dc:creator>vraevsky</dc:creator>
      <dc:date>2025-10-28T21:41:20Z</dc:date>
    </item>
    <item>
      <title>Re: imx95 m7 core edma issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx95-m7-core-edma-issue/m-p/2195056#M241753</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207755"&gt;@vraevsky&lt;/a&gt;&amp;nbsp;, which linux bsp and dtb are you using to boot the board ?&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 10:43:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx95-m7-core-edma-issue/m-p/2195056#M241753</guid>
      <dc:creator>gaurav_sharma</dc:creator>
      <dc:date>2025-10-29T10:43:39Z</dc:date>
    </item>
    <item>
      <title>Re: imx95 m7 core edma issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx95-m7-core-edma-issue/m-p/2195300#M241766</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Linux kernel version is 6.12.34 a clone of:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/nxp-imx/linux-imx.git" target="_blank" rel="noopener"&gt;https://github.com/nxp-imx/linux-imx.git&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here are device tree and a dtsi&lt;/P&gt;&lt;P&gt;main ucm-imx95-som.dts:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/compulab-yokneam/linux-compulab/blob/linux-compulab_v6.12.34/arch/arm64/boot/dts/compulab/ucm-imx95-som.dts" target="_blank" rel="noopener"&gt;https://github.com/compulab-yokneam/linux-compulab/blob/linux-compulab_v6.12.34/arch/arm64/boot/dts/compulab/ucm-imx95-som.dts&lt;/A&gt;&lt;/P&gt;&lt;P&gt;dtsi ucm-imx95-rpmsg.dtsi:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/compulab-yokneam/linux-compulab/blob/linux-compulab_v6.12.34/arch/arm64/boot/dts/compulab/ucm-imx95-rpmsg.dtsi" target="_blank" rel="noopener"&gt;https://github.com/compulab-yokneam/linux-compulab/blob/linux-compulab_v6.12.34/arch/arm64/boot/dts/compulab/ucm-imx95-rpmsg.dtsi&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Makefile:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/compulab-yokneam/linux-compulab/blob/linux-compulab_v6.12.34/arch/arm64/boot/dts/compulab/Makefile.ucm-imx95#L22-L23" target="_self"&gt;https://github.com/compulab-yokneam/linux-compulab/blob/linux-compulab_v6.12.34/arch/arm64/boot/dts/compulab/Makefile.ucm-imx95#L22-L23&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;imx-system-manager:&lt;/P&gt;&lt;P&gt;version:&amp;nbsp;&lt;SPAN&gt;lf-6.12.34-2.1.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;config: imx95evkrpmsg.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Valentin.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 22:20:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx95-m7-core-edma-issue/m-p/2195300#M241766</guid>
      <dc:creator>vraevsky</dc:creator>
      <dc:date>2025-10-29T22:20:48Z</dc:date>
    </item>
  </channel>
</rss>