<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Troubleshooting 8ULP EVK Boot Fuses in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Troubleshooting-8ULP-EVK-Boot-Fuses/m-p/2195203#M241762</link>
    <description>&lt;P&gt;I pulled down&amp;nbsp;LF_v6.12.34-2.1.0_images_IMX8ULPEVK, updated the&amp;nbsp;samples/uuu_8ulp_dual.auto to point to the local bin files, burned the images and same result.&lt;/P&gt;&lt;P&gt;When I POR, with Boot Switch set to xxxx_xx00, I see nothing and the SDPS device appears.&amp;nbsp; I do not have any SRK or certs or any of the CST set up.&lt;/P&gt;</description>
    <pubDate>Wed, 29 Oct 2025 15:08:59 GMT</pubDate>
    <dc:creator>KipW</dc:creator>
    <dc:date>2025-10-29T15:08:59Z</dc:date>
    <item>
      <title>Troubleshooting 8ULP EVK Boot Fuses</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Troubleshooting-8ULP-EVK-Boot-Fuses/m-p/2193739#M241691</link>
      <description>&lt;P&gt;I am testing recovery methods using the MCIMX8ULP-BB EVK.&amp;nbsp; I successfully burned&amp;nbsp;&lt;SPAN&gt;BT_FUSE_SEL and BT0_CFG1 (Boot from A35/eMMC and M33/QSPI) using u-boot's fuse command. When I set my boot pins to "00" I get the serial bootloader. However, since I have working images in A35's eMMC and M33's NOR, I should be seeing the the kernel boot and the output from M33's image.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Ideas on how to troubleshoot this?&amp;nbsp; Does booting from the fuses *require* that I use signed/secure images?&lt;/P&gt;</description>
      <pubDate>Mon, 27 Oct 2025 20:19:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Troubleshooting-8ULP-EVK-Boot-Fuses/m-p/2193739#M241691</guid>
      <dc:creator>KipW</dc:creator>
      <dc:date>2025-10-27T20:19:46Z</dc:date>
    </item>
    <item>
      <title>Re: Troubleshooting 8ULP EVK Boot Fuses</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Troubleshooting-8ULP-EVK-Boot-Fuses/m-p/2194453#M241727</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256209"&gt;@KipW&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For that usage you should flash the images following the next instructions:&lt;BR /&gt;&lt;BR /&gt;To burn dual-boot image and rootfs to eMMC and FlexSPI0 NOR flash, perform the following steps:&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;1. Prepare imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33, imx-boot-imx8ulpevk-&lt;BR /&gt;sd.bin-flash_dualboot, imx-boot-imx8ulpevk-sd.bin-flash_dualboot_m33, and&lt;BR /&gt;&amp;lt;rootfs.wic&amp;gt;.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;2. Update the UUU script file uuu_8ulp_dual.auto with the file path and name of the images above.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;3. Run uuu mfgtools/scripts/samples/uuu_8ulp_dual.auto.&lt;BR /&gt;For detailed usage of UUU, see github.com/NXPmicro/mfgtools/wiki.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Oct 2025 17:14:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Troubleshooting-8ULP-EVK-Boot-Fuses/m-p/2194453#M241727</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2025-10-28T17:14:38Z</dc:date>
    </item>
    <item>
      <title>Re: Troubleshooting 8ULP EVK Boot Fuses</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Troubleshooting-8ULP-EVK-Boot-Fuses/m-p/2195203#M241762</link>
      <description>&lt;P&gt;I pulled down&amp;nbsp;LF_v6.12.34-2.1.0_images_IMX8ULPEVK, updated the&amp;nbsp;samples/uuu_8ulp_dual.auto to point to the local bin files, burned the images and same result.&lt;/P&gt;&lt;P&gt;When I POR, with Boot Switch set to xxxx_xx00, I see nothing and the SDPS device appears.&amp;nbsp; I do not have any SRK or certs or any of the CST set up.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 15:08:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Troubleshooting-8ULP-EVK-Boot-Fuses/m-p/2195203#M241762</guid>
      <dc:creator>KipW</dc:creator>
      <dc:date>2025-10-29T15:08:59Z</dc:date>
    </item>
    <item>
      <title>Re: Troubleshooting 8ULP EVK Boot Fuses</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Troubleshooting-8ULP-EVK-Boot-Fuses/m-p/2195990#M241799</link>
      <description>Turns out that the 'fuse' command in u-boot requires a little-endian value for burning. The u-boot command does not perform the endian swap for you</description>
      <pubDate>Thu, 30 Oct 2025 16:27:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Troubleshooting-8ULP-EVK-Boot-Fuses/m-p/2195990#M241799</guid>
      <dc:creator>KipW</dc:creator>
      <dc:date>2025-10-30T16:27:49Z</dc:date>
    </item>
  </channel>
</rss>