<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: I.MX8M Plus Enter JTAG Debug</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-Plus-Enter-JTAG-Debug/m-p/2192867#M241647</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have some questions regarding JTAG connectivity and boot options for a custom i.MX8M Plus board.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;How do you typically connect your board for debugging — using JTAG or another interface?&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;If JTAG is used, do you connect &lt;STRONG&gt;after U-Boot&lt;/STRONG&gt; has executed or &lt;STRONG&gt;before boot (at power-on reset)&lt;/STRONG&gt;?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;In our custom board, &lt;STRONG&gt;USB and SD interfaces are not populated&lt;/STRONG&gt;, so we currently have &lt;STRONG&gt;only JTAG&lt;/STRONG&gt; available for communication and detection.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Could you please advise on the correct procedure or configuration to bring up the board only via JTAG (&amp;nbsp; DSTREAM-ST)?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there any additional configuration needed in the &lt;STRONG&gt;&amp;nbsp;JTAG_MOD / Boot Mode&lt;/STRONG&gt;&amp;nbsp;pins for enabling debug access when no boot device is present?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/OL&gt;</description>
    <pubDate>Sat, 25 Oct 2025 12:43:00 GMT</pubDate>
    <dc:creator>NXP_USER_05</dc:creator>
    <dc:date>2025-10-25T12:43:00Z</dc:date>
    <item>
      <title>I.MX8M Plus Enter JTAG Debug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-Plus-Enter-JTAG-Debug/m-p/1576651#M199439</link>
      <description>&lt;P&gt;When using NXP I.MX8M Plus chip for bare metal development and debugging, and using DStream emulator to connect to the JTAG interface of I.MX8M Plus processor through JTAG, pin JTAG_ MOD has been set to low level, but the development board cannot enter the JATG debugging mode, and the ROM Table of the chip cannot be read using the J-Link emulator. Does the I.MX8M Plus chip disable the JTAG function when it leaves the factory? How can I enable the Cortex-A53 processor in I.MX8M Plus chip to enter the bare metal debugging mode through JTAG? Thank you&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jan 2023 16:26:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-Plus-Enter-JTAG-Debug/m-p/1576651#M199439</guid>
      <dc:creator>hjc</dc:creator>
      <dc:date>2023-01-03T16:26:05Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8M Plus Enter JTAG Debug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-Plus-Enter-JTAG-Debug/m-p/1577211#M199517</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, JTAG is disable when is leaving the factory, but this is just for rom access you can access to the rest of the code.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jan 2023 15:24:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-Plus-Enter-JTAG-Debug/m-p/1577211#M199517</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-01-04T15:24:16Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8M Plus Enter JTAG Debug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-Plus-Enter-JTAG-Debug/m-p/1577793#M199572</link>
      <description>&lt;P&gt;if i no use rom access, how can i do that use the jtag for debug Cortex-a53 bare metal program ?&lt;/P&gt;&lt;P&gt;how can i do that enter jtag debug mode, thank you&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 08:09:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-Plus-Enter-JTAG-Debug/m-p/1577793#M199572</guid>
      <dc:creator>hjc</dc:creator>
      <dc:date>2023-01-05T08:09:14Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8M Plus Enter JTAG Debug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-Plus-Enter-JTAG-Debug/m-p/2192867#M241647</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have some questions regarding JTAG connectivity and boot options for a custom i.MX8M Plus board.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;How do you typically connect your board for debugging — using JTAG or another interface?&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;If JTAG is used, do you connect &lt;STRONG&gt;after U-Boot&lt;/STRONG&gt; has executed or &lt;STRONG&gt;before boot (at power-on reset)&lt;/STRONG&gt;?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;In our custom board, &lt;STRONG&gt;USB and SD interfaces are not populated&lt;/STRONG&gt;, so we currently have &lt;STRONG&gt;only JTAG&lt;/STRONG&gt; available for communication and detection.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Could you please advise on the correct procedure or configuration to bring up the board only via JTAG (&amp;nbsp; DSTREAM-ST)?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there any additional configuration needed in the &lt;STRONG&gt;&amp;nbsp;JTAG_MOD / Boot Mode&lt;/STRONG&gt;&amp;nbsp;pins for enabling debug access when no boot device is present?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/OL&gt;</description>
      <pubDate>Sat, 25 Oct 2025 12:43:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-Plus-Enter-JTAG-Debug/m-p/2192867#M241647</guid>
      <dc:creator>NXP_USER_05</dc:creator>
      <dc:date>2025-10-25T12:43:00Z</dc:date>
    </item>
  </channel>
</rss>