<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8MQ with DDR4 (not LPDDR4) valid configuration needed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2186992#M241447</link>
    <description>&lt;P&gt;Hello pengyong_zhang, thank you for your quick response.&lt;BR /&gt;&lt;BR /&gt;I attach an archive with ISSI memory that I have to start,&lt;BR /&gt;screenshot with configuration on DDR Config Tool page, and the Debug log of 'Firmware Init test'&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The UART is dual CP2105, the same as on EVK&lt;BR /&gt;The power manager is MC32PF4210 &lt;STRONG&gt;A2,&lt;/STRONG&gt; thus DDR voltage is 1.2V.&lt;/P&gt;&lt;P&gt;I attached an IMX8MQ-EVK board to the same USB cables, and all tests passed, so USB connection is not an issue.&lt;/P&gt;&lt;P&gt;The board runs correctly with Micron memory MT40A512M16-8Gb-ddr4, but it is EOL, that's why&lt;BR /&gt;I am busy on replacement with ISSI or SK Hynix.&lt;BR /&gt;In the archive I added also currently working ddr4 config .c file, but I do not have the original&lt;BR /&gt;config how the file was generated.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
    <pubDate>Thu, 16 Oct 2025 00:22:33 GMT</pubDate>
    <dc:creator>janmodaal</dc:creator>
    <dc:date>2025-10-16T00:22:33Z</dc:date>
    <item>
      <title>IMX8MQ with DDR4 (not LPDDR4) valid configuration needed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2186450#M241417</link>
      <description>&lt;P&gt;Hello all,&lt;BR /&gt;I am busy with starting custom IMX8MQ board using 2x 1GB DDR4 (not LPDDR4).&lt;BR /&gt;This application is used: "Config Tools for i.MX Applications Processors".&lt;/P&gt;&lt;P&gt;The power part is copied from IMX8MQ-EVK design, same chip, the DDR voltage is increased to 1.2V.&lt;/P&gt;&lt;P&gt;Tested the app also with MaaX board, the same DDR4 layout.&lt;/P&gt;&lt;P&gt;The DDR tool fails in 'Firmware Init test', and also the rest of DDR tests.&lt;/P&gt;&lt;P&gt;When tested against IMX8MQ-EVK board (LPDDR4), all DDR tests are passed OK.&lt;/P&gt;&lt;P&gt;So my question is - is this DDR tool tested with IMX8MQ with DDR4 ?&lt;BR /&gt;If yes - could you provide any link or document with valid configuration ?&lt;/P&gt;&lt;P&gt;I tested all Windows and Linux versions starting from version 24.12, no success with DDR4,&lt;BR /&gt;only LPDDR4 of EVK board was OK.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;More details below:&lt;/P&gt;&lt;P&gt;This application is installed, starting as Administrator in Windows11 (EN):&lt;BR /&gt;"Config Tools for i.MX Applications Processors"&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-development-boards/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-development-boards/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The power part is copied from IMX8MQ-EVK design, the same MC32PF4210, i2c address etc&lt;BR /&gt;The RAM is 2 pieces ISSI IS43QR16512A-075VBL ( 512Mbitx16)&lt;BR /&gt;&lt;A href="https://www.issi.com/WW/pdf/43-46QR81024A-16512A.pdf" target="_blank"&gt;https://www.issi.com/WW/pdf/43-46QR81024A-16512A.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;DDR voltage is set to 1.2V in power manager&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;MaaX board with IMX8MQ, RAM is DDR4 2x 8Gbit H5AN8G6NAFR-UHC&lt;BR /&gt;&lt;A href="https://www.tria-technologies.com/product/maaxboard/" target="_blank"&gt;https://www.tria-technologies.com/product/maaxboard/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Wed, 15 Oct 2025 08:23:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2186450#M241417</guid>
      <dc:creator>janmodaal</dc:creator>
      <dc:date>2025-10-15T08:23:12Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ with DDR4 (not LPDDR4) valid configuration needed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2186505#M241420</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/102614"&gt;@janmodaal&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please share your DDR4 datasheet file, and your configuration on DDR Config Tool page, and the ""Init test" fail log.&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Wed, 15 Oct 2025 09:21:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2186505#M241420</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2025-10-15T09:21:38Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ with DDR4 (not LPDDR4) valid configuration needed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2186992#M241447</link>
      <description>&lt;P&gt;Hello pengyong_zhang, thank you for your quick response.&lt;BR /&gt;&lt;BR /&gt;I attach an archive with ISSI memory that I have to start,&lt;BR /&gt;screenshot with configuration on DDR Config Tool page, and the Debug log of 'Firmware Init test'&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The UART is dual CP2105, the same as on EVK&lt;BR /&gt;The power manager is MC32PF4210 &lt;STRONG&gt;A2,&lt;/STRONG&gt; thus DDR voltage is 1.2V.&lt;/P&gt;&lt;P&gt;I attached an IMX8MQ-EVK board to the same USB cables, and all tests passed, so USB connection is not an issue.&lt;/P&gt;&lt;P&gt;The board runs correctly with Micron memory MT40A512M16-8Gb-ddr4, but it is EOL, that's why&lt;BR /&gt;I am busy on replacement with ISSI or SK Hynix.&lt;BR /&gt;In the archive I added also currently working ddr4 config .c file, but I do not have the original&lt;BR /&gt;config how the file was generated.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Thu, 16 Oct 2025 00:22:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2186992#M241447</guid>
      <dc:creator>janmodaal</dc:creator>
      <dc:date>2025-10-16T00:22:33Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ with DDR4 (not LPDDR4) valid configuration needed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2187203#M241451</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/102614"&gt;@janmodaal&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please share your schematic file.&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Thu, 16 Oct 2025 06:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2187203#M241451</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2025-10-16T06:33:55Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ with DDR4 (not LPDDR4) valid configuration needed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2188386#M241484</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202673"&gt;@pengyong_zhang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;Here is an archive with relevant imx8 pieces.&lt;/DIV&gt;&lt;DIV&gt;The imx8 first USB port is connected with usb2.0 cable, not shown in diagram&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;What is different with EVK board - the watchdog output pin GPIO1_IO02 is not connected as nWDOG.&lt;/DIV&gt;&lt;DIV&gt;As a workaround, we use pin PMIC_ON_REQ to request power toggling of IMX8+eMMC+DDR to external FPGA controller.&lt;/DIV&gt;&lt;DIV&gt;In arm-trusted-boot is done with a patch proposed for imx7 from&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="https://community.toradex.com/t/e10574-watchdog-a-watchdog-timeout-or-software-trigger-will-not-reset-the-soc/18205" target="_blank"&gt;https://community.toradex.com/t/e10574-watchdog-a-watchdog-timeout-or-software-trigger-will-not-reset-the-soc/18205&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;...&lt;/DIV&gt;&lt;DIV&gt;static void __dead2 imx_wdog_restart(bool external_reset)&lt;/DIV&gt;&lt;DIV&gt;{&lt;/DIV&gt;&lt;DIV&gt;...&lt;/DIV&gt;&lt;DIV&gt;#pragma message "ATF: toggle pin PWR_ON for reboot"&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;uint32_t val2 = mmio_read_32(IMX_SNVS_BASE + SNVS_LPCR);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;val2 |= SNVS_LPCR_SRTC_ENV | SNVS_LPCR_DP_EN | SNVS_LPCR_TOP;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;mmio_write_32(IMX_SNVS_BASE + SNVS_LPCR, val2);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;</description>
      <pubDate>Fri, 17 Oct 2025 14:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2188386#M241484</guid>
      <dc:creator>janmodaal</dc:creator>
      <dc:date>2025-10-17T14:48:20Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ with DDR4 (not LPDDR4) valid configuration needed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2188908#M241502</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/102614"&gt;@janmodaal&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Your DDR configuration is no problem. pleaser try use the below DDR stress tool. and use the attachment .ds file for the DDR stress.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Mon, 20 Oct 2025 05:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2188908#M241502</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2025-10-20T05:35:29Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ with DDR4 (not LPDDR4) valid configuration needed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2189755#M241535</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202673"&gt;@pengyong_zhang&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thanks for the .ds file, I see it was generated from MX8M_DDR4_RPA_v18.xlsx&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8M-m850D-DDR-Register-Programming-Aid-RPA/ta-p/1172441" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8M-m850D-DDR-Register-Programming-Aid-RPA/ta-p/1172441&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;It worked with Program mscale_ddr_tool_v3.31_setup.exe.zip downloaded from&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It did not work with more recent "Config Tools for i.MX Applications Processors"&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-development-boards/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-development-boards/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX&lt;/A&gt;&lt;BR /&gt;I tried importing the .ds file there, but UART communication with IMX8 during "DDR Test" -&amp;gt; "Firmware Init test" always resulted in timeout (no response from target)&lt;BR /&gt;Tested all linux and windows versions 24.12, 25.03, 25.06, 25.09.&lt;/P&gt;&lt;P&gt;What I did as extra settings - in windows Device manager for COM port settings of CP2105 I disabled power management + set the speed to 115200.&lt;BR /&gt;Also, enabled Windows sounds when a USB device is added/removed, to be clear when IMX8 serial download HID device was detected&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Oct 2025 08:05:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-with-DDR4-not-LPDDR4-valid-configuration-needed/m-p/2189755#M241535</guid>
      <dc:creator>janmodaal</dc:creator>
      <dc:date>2025-10-21T08:05:09Z</dc:date>
    </item>
  </channel>
</rss>