<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Post Quantization Model Runs on iMX93 NPU, but Output is Incorrect in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2186805#M241439</link>
    <description>&lt;P&gt;I am working with a custom implementation of MobileNet designed to do binary classification on sparks. After converting to tflite and quantizing it to int8, the model runs on the NPU as expected, but the output does not make sense. The model had good accuracy before quantization, but the int8 outputs seem to be totally random. After testing on some of the training data, frames that should be positive are ranging from -128 to 127, and so are frames that should have been negative. Am I misinterpreting the output, or did something go wrong while converting or quantizing the model?&lt;/P&gt;</description>
    <pubDate>Wed, 15 Oct 2025 16:57:12 GMT</pubDate>
    <dc:creator>Skramer</dc:creator>
    <dc:date>2025-10-15T16:57:12Z</dc:date>
    <item>
      <title>Post Quantization Model Runs on iMX93 NPU, but Output is Incorrect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2186805#M241439</link>
      <description>&lt;P&gt;I am working with a custom implementation of MobileNet designed to do binary classification on sparks. After converting to tflite and quantizing it to int8, the model runs on the NPU as expected, but the output does not make sense. The model had good accuracy before quantization, but the int8 outputs seem to be totally random. After testing on some of the training data, frames that should be positive are ranging from -128 to 127, and so are frames that should have been negative. Am I misinterpreting the output, or did something go wrong while converting or quantizing the model?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Oct 2025 16:57:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2186805#M241439</guid>
      <dc:creator>Skramer</dc:creator>
      <dc:date>2025-10-15T16:57:12Z</dc:date>
    </item>
    <item>
      <title>Re: Post Quantization Model Runs on iMX93 NPU, but Output is Incorrect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2187650#M241465</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Please provide the model and which BSP are you testing?&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 16 Oct 2025 16:18:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2187650#M241465</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-10-16T16:18:07Z</dc:date>
    </item>
    <item>
      <title>Re: Post Quantization Model Runs on iMX93 NPU, but Output is Incorrect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2190250#M241550</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have attached the model. The BSP is Linux BSP.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 21 Oct 2025 21:10:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2190250#M241550</guid>
      <dc:creator>Skramer</dc:creator>
      <dc:date>2025-10-21T21:10:56Z</dc:date>
    </item>
    <item>
      <title>Re: Post Quantization Model Runs on iMX93 NPU, but Output is Incorrect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2190262#M241551</link>
      <description>&lt;P&gt;Your model can run with the latest BSP, it uses GPU besides the performance it run very well, I can not see any error.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Oct 2025 21:52:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2190262#M241551</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-10-21T21:52:47Z</dc:date>
    </item>
    <item>
      <title>Re: Post Quantization Model Runs on iMX93 NPU, but Output is Incorrect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2190263#M241552</link>
      <description>&lt;P&gt;Would you mind sharing the script you used to successfully run it? Perhaps I have written my script incorrectly.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 21 Oct 2025 21:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2190263#M241552</guid>
      <dc:creator>Skramer</dc:creator>
      <dc:date>2025-10-21T21:56:02Z</dc:date>
    </item>
    <item>
      <title>Re: Post Quantization Model Runs on iMX93 NPU, but Output is Incorrect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2190896#M241575</link>
      <description>&lt;P&gt;Here is attached!!&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 22 Oct 2025 16:25:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Post-Quantization-Model-Runs-on-iMX93-NPU-but-Output-is/m-p/2190896#M241575</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-10-22T16:25:24Z</dc:date>
    </item>
  </channel>
</rss>