<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8M Mini Gstreamer  imx_2d_device_g2d in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-Gstreamer-imx-2d-device-g2d/m-p/2183124#M241279</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You should contact you maxboard vendor since this should work o MX8MiniEVK&lt;/P&gt;
&lt;P&gt;Please make sure you are using linux-imx kernel and install the gpu library.&amp;nbsp;And the gpu dts node should be enabled in your dts like imx8mm-evk.dts&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 09 Oct 2025 15:35:59 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2025-10-09T15:35:59Z</dc:date>
    <item>
      <title>IMX8M Mini Gstreamer  imx_2d_device_g2d</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-Gstreamer-imx-2d-device-g2d/m-p/2181528#M241222</link>
      <description>&lt;P&gt;Any help debugging this issue with the Maaxboard-min and the ov5640 MIPI-CSI2 camera:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@maaxboardmini:~# v4l2-ctl -d /dev/video0 -D
Driver Info:
	Driver name      : mx6s-csi
	Card type        : i.MX6S_CSI
	Bus info         : platform:32e20000.csi1_bridge
	Driver version   : 6.1.22
	Capabilities     : 0x84200001
		Video Capture
		Streaming
		Extended Pix Format
		Device Capabilities
	Device Caps      : 0x04200001
		Video Capture
		Streaming
		Extended Pix Format
root@maaxboardmini:~# &lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have this Error message&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;0:00:00.110175250 1540 0xaaaaf4e8bcf0 ERROR imx2ddevice imx_2d_device_g2d.c:147:imx_g2d_open: imx_g2d_open Failed to open g2d device.
0:00:00.110209875 1540 0xaaaaf4e8bcf0 ERROR imxvideoconvert gstimxvideoconvert.c:1940:gst_imx_video_convert_init: Open video process device failed.&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;Cmd:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@maaxboardmini:~# GST_DEBUG=3 gst-launch-1.0 v4l2src device=/dev/video0 ! 'video/x-raw,width=1920,height=1080,framerate=30/1' ! imxvideoconvert_g2d ! vpuenc_h264 ! mp4mux ! filesink location=video_ov5640.mp4
[     1] HAL user version: 6.4.11.608260
[     2] HAL kernel version: 6.4.11.658245
g2d_open: fail with status -24
0:00:00.110175250  1540 0xaaaaf4e8bcf0 ERROR            imx2ddevice imx_2d_device_g2d.c:147:imx_g2d_open: imx_g2d_open Failed to open g2d device.
0:00:00.110209875  1540 0xaaaaf4e8bcf0 ERROR        imxvideoconvert gstimxvideoconvert.c:1940:gst_imx_video_convert_init: Open video process device failed.
Setting pipeline to PAUSED ...
====== VPUENC: 4.7.3 build on Feb  3 2023 05:14:46. ======
	wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Jan 12 2023 01:49:28)
	vpulib: 1.1.1
	firmware: 1.1.1.43690
0:00:00.129913750  1540 0xaaaaf4e62d20 WARN                 v4l2src gstv4l2src.c:794:gst_v4l2src_query:&amp;lt;v4l2src0&amp;gt; Can't give latency since framerate isn't fixated !
0:00:00.130004875  1540 0xaaaaf4e62d20 WARN              aggregator gstaggregator.c:2099:gst_aggregator_query_latency_unlocked:&amp;lt;mp4mux0&amp;gt; Latency query failed
Pipeline is live and does not need PREROLL ...
0:00:00.133896125  1540 0xaaaaf4e62c60 FIXME                v4l2src gstv4l2src.c:572:gst_v4l2src_query_preferred_size:&amp;lt;v4l2src0&amp;gt; missing support for video standards
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
0:00:00.134743625  1540 0xaaaaf4e62d20 WARN                 v4l2src gstv4l2src.c:794:gst_v4l2src_query:&amp;lt;v4l2src0&amp;gt; Can't give latency since framerate isn't fixated !
0:00:00.134808125  1540 0xaaaaf4e62d20 WARN              aggregator gstaggregator.c:2099:gst_aggregator_query_latency_unlocked:&amp;lt;mp4mux0&amp;gt; Latency query failed
New clock: GstSystemClock
0:00:00.594056000  1540 0xaaaaf4e62c60 WARN          v4l2bufferpool gstv4l2bufferpool.c:1424:gst_v4l2_buffer_pool_dqbuf:&amp;lt;v4l2src0:pool0:src&amp;gt; Driver should never set v4l2_buffer.field to ANY
0:00:00.598324625  1540 0xaaaaf4e62c60 WARN                 basesrc gstbasesrc.c:3127:gst_base_src_loop:&amp;lt;v4l2src0&amp;gt; error: Internal data stream error.
0:00:00.598394250  1540 0xaaaaf4e62c60 WARN                 basesrc gstbasesrc.c:3127:gst_base_src_loop:&amp;lt;v4l2src0&amp;gt; error: streaming stopped, reason error (-5)
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Internal data stream error.
Additional debug info:
/usr/src/debug/gstreamer1.0/1.20.3.imx-r0/libs/gst/base/gstbasesrc.c(3127): gst_base_src_loop (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
streaming stopped, reason error (-5)
0:00:00.599017750  1540 0xaaaaf4e62d20 FIXME               basesink gstbasesink.c:3395:gst_base_sink_default_event:&amp;lt;filesink0&amp;gt; stream-start event without group-id. Consider implementing group-id handling in the upstream elements
Execution ended after 0:00:00.464760125
Setting pipeline to NULL ...
0:00:00.599406125  1540 0xaaaaf4e62d20 WARN                   qtmux gstqtmux.c:1913:gst_qt_mux_send_buffer:&amp;lt;mp4mux0&amp;gt; Failed to send buffer (0xaaaaf4ec9b40) size 32
0:00:00.599456250  1540 0xaaaaf4e62d20 FIXME             aggregator gstaggregator.c:1410:gst_aggregator_aggregate_func:&amp;lt;mp4mux0&amp;gt; Subclass should call gst_aggregator_selected_samples() from its aggregate implementation.
Freeing pipeline ...&lt;/LI-CODE&gt;&lt;LI-CODE lang="markup"&gt;root@maaxboardmini:~# v4l2-ctl -d /dev/video0 -D
Driver Info:
	Driver name      : mx6s-csi
	Card type        : i.MX6S_CSI
	Bus info         : platform:32e20000.csi1_bridge
	Driver version   : 6.1.22
	Capabilities     : 0x84200001
		Video Capture
		Streaming
		Extended Pix Format
		Device Capabilities
	Device Caps      : 0x04200001
		Video Capture
		Streaming
		Extended Pix Format
root@maaxboardmini:~# &lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Oct 2025 22:41:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-Gstreamer-imx-2d-device-g2d/m-p/2181528#M241222</guid>
      <dc:creator>fahd000</dc:creator>
      <dc:date>2025-10-07T22:41:16Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M Mini Gstreamer  imx_2d_device_g2d</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-Gstreamer-imx-2d-device-g2d/m-p/2183124#M241279</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You should contact you maxboard vendor since this should work o MX8MiniEVK&lt;/P&gt;
&lt;P&gt;Please make sure you are using linux-imx kernel and install the gpu library.&amp;nbsp;And the gpu dts node should be enabled in your dts like imx8mm-evk.dts&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 09 Oct 2025 15:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-Gstreamer-imx-2d-device-g2d/m-p/2183124#M241279</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-10-09T15:35:59Z</dc:date>
    </item>
  </channel>
</rss>