<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX8MP returns No HAB Events Found for unsigned Kernel image.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-returns-No-HAB-Events-Found-for-unsigned-Kernel-image/m-p/2182799#M241268</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I'm working on Secure Boot using the UG10163 (10.9 Security Reference Design). I generated a wic image that includes signed bootloader and signed kernel images.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;After flashing this image to an SD card, I manually replaced the signed kernel image in the /boot folder with an &lt;STRONG&gt;unsigned kernel image&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Then, on the target device, I executed the following command in U-Boot:&lt;/P&gt;&lt;P&gt;hab_auth_img ${loadaddr} ${filesize} 0x1a90000&lt;/P&gt;&lt;P&gt;I expected HAB events to be triggered due to the unsigned kernel image, but the output showed:&lt;/P&gt;&lt;PRE&gt;No HAB Events Found!&lt;/PRE&gt;&lt;P&gt;&lt;STRONG&gt;Why is no HAB event being reported even though the kernel image is unsigned?&lt;/STRONG&gt;&lt;BR /&gt;I've attached the log below for reference.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Kartheek&lt;/P&gt;</description>
    <pubDate>Thu, 09 Oct 2025 07:24:18 GMT</pubDate>
    <dc:creator>kartheek</dc:creator>
    <dc:date>2025-10-09T07:24:18Z</dc:date>
    <item>
      <title>IMX8MP returns No HAB Events Found for unsigned Kernel image.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-returns-No-HAB-Events-Found-for-unsigned-Kernel-image/m-p/2182799#M241268</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I'm working on Secure Boot using the UG10163 (10.9 Security Reference Design). I generated a wic image that includes signed bootloader and signed kernel images.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;After flashing this image to an SD card, I manually replaced the signed kernel image in the /boot folder with an &lt;STRONG&gt;unsigned kernel image&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Then, on the target device, I executed the following command in U-Boot:&lt;/P&gt;&lt;P&gt;hab_auth_img ${loadaddr} ${filesize} 0x1a90000&lt;/P&gt;&lt;P&gt;I expected HAB events to be triggered due to the unsigned kernel image, but the output showed:&lt;/P&gt;&lt;PRE&gt;No HAB Events Found!&lt;/PRE&gt;&lt;P&gt;&lt;STRONG&gt;Why is no HAB event being reported even though the kernel image is unsigned?&lt;/STRONG&gt;&lt;BR /&gt;I've attached the log below for reference.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Kartheek&lt;/P&gt;</description>
      <pubDate>Thu, 09 Oct 2025 07:24:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-returns-No-HAB-Events-Found-for-unsigned-Kernel-image/m-p/2182799#M241268</guid>
      <dc:creator>kartheek</dc:creator>
      <dc:date>2025-10-09T07:24:18Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP returns No HAB Events Found for unsigned Kernel image.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-returns-No-HAB-Events-Found-for-unsigned-Kernel-image/m-p/2183726#M241293</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Are these steps tested after board reboot? and make sure if that the singed image was replaced.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 10 Oct 2025 08:44:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-returns-No-HAB-Events-Found-for-unsigned-Kernel-image/m-p/2183726#M241293</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-10-10T08:44:19Z</dc:date>
    </item>
  </channel>
</rss>