<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/2179828#M241136</link>
    <description>&lt;P&gt;Any Update I am facing same issue with Omnivision 9732&lt;/P&gt;</description>
    <pubDate>Fri, 03 Oct 2025 09:51:40 GMT</pubDate>
    <dc:creator>IXM</dc:creator>
    <dc:date>2025-10-03T09:51:40Z</dc:date>
    <item>
      <title>i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/1772341#M217160</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a custom i.MX93 based board. Using the provided CSI-2 interface I want to use a bayer pattern camera (IMX327) transferring RAW10 data.&lt;/P&gt;&lt;P&gt;My device tree setup and media-ctl configuration is correct so far, but once I start the pipeline I get an IRQ storm from dwc-mipi-csi2 increasing "&lt;SPAN&gt;IPI Interface Fatal Error events" counter. The register value of INT_ST_IPI_FATAL is 0x2a indicating a IPI FIFO overflow. I suspect IPI is not pushing data to ISI at all, having not a single IRQ.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Reading&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/About-settings-to-operate-ov5640camera-on-i-MX93EVK/m-p/1716885/highlight/true#M212016" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/About-settings-to-operate-ov5640camera-on-i-MX93EVK/m-p/1716885/highlight/true#M212016&lt;/A&gt;&amp;nbsp;there seems to some kind of special configuration. I tried to adapt these values to RAW10, but I was wondering about CAMERA_MUX[DATA_TYPE] value 0x31 (user define16). Why is this not 0x2b for CSI-2 data type RAW10 but user define?&lt;/P&gt;&lt;P&gt;What could be the cause for IPI errors? How I could I firther debug this issue?&lt;/P&gt;&lt;P&gt;Thank and best regards,&lt;BR /&gt;Alexander&lt;/P&gt;</description>
      <pubDate>Mon, 11 Dec 2023 13:56:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/1772341#M217160</guid>
      <dc:creator>steina</dc:creator>
      <dc:date>2023-12-11T13:56:57Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/1775779#M217480</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200210"&gt;@steina&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for contacting NXP Support.&lt;/P&gt;&lt;P&gt;I will review this case with the internal team, and I will contact you as soon as possible.&lt;/P&gt;&lt;P&gt;Have a great day!&lt;/P&gt;</description>
      <pubDate>Fri, 15 Dec 2023 21:45:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/1775779#M217480</guid>
      <dc:creator>brian14</dc:creator>
      <dc:date>2023-12-15T21:45:02Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/1792962#M219010</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;any news on this topic?&lt;/P&gt;&lt;P&gt;Thanks and best regards,&lt;BR /&gt;Alexander&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jan 2024 11:51:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/1792962#M219010</guid>
      <dc:creator>steina</dc:creator>
      <dc:date>2024-01-22T11:51:52Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/1818839#M220594</link>
      <description>Hello,&lt;BR /&gt;&lt;BR /&gt;any news? Another month has passed.&lt;BR /&gt;&lt;BR /&gt;Thanks, Alexander</description>
      <pubDate>Thu, 29 Feb 2024 14:35:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/1818839#M220594</guid>
      <dc:creator>steina</dc:creator>
      <dc:date>2024-02-29T14:35:42Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/1840778#M222125</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207096"&gt;@brian14&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;we are facing the same problem with i.MX93 and camera sensor that outputs RAW10/12 Bayer data.&lt;/P&gt;&lt;P&gt;Any ideas / suggestions?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Apr 2024 13:22:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/1840778#M222125</guid>
      <dc:creator>wooosaiiii</dc:creator>
      <dc:date>2024-04-04T13:22:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/2179828#M241136</link>
      <description>&lt;P&gt;Any Update I am facing same issue with Omnivision 9732&lt;/P&gt;</description>
      <pubDate>Fri, 03 Oct 2025 09:51:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-using-MIPI-CSI-2-with-a-Bayer-Pattern-camera-RAW10/m-p/2179828#M241136</guid>
      <dc:creator>IXM</dc:creator>
      <dc:date>2025-10-03T09:51:40Z</dc:date>
    </item>
  </channel>
</rss>