<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MX8ULP_DDR_Tool</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2179265#M241103</link>
    <description>&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;can we have access to the sources of that Ramtest image? Thank you in advance.&lt;/P&gt;</description>
    <pubDate>Thu, 02 Oct 2025 10:07:21 GMT</pubDate>
    <dc:creator>Joerg_Ks</dc:creator>
    <dc:date>2025-10-02T10:07:21Z</dc:date>
    <item>
      <title>MX8ULP_DDR_Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2175032#M240899</link>
      <description>&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;we use your&amp;nbsp;MX8ULP_DDR_Tool to check our LPDDR4x design. I have a question regarding the tool. Is the code that runs the tests located in the internal ram of 8ulp? When I run the stress test on several boards, I see that sometimes the tools hangs without an error or message from the cpu in the terminal.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;BR Joerg&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 12:38:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2175032#M240899</guid>
      <dc:creator>Joerg_Ks</dc:creator>
      <dc:date>2025-09-24T12:38:03Z</dc:date>
    </item>
    <item>
      <title>Re: MX8ULP_DDR_Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2175184#M240911</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The tool is running on the PC side which downloads a test image to the i.MX series processor’s internal RAM through a USB connection.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 17:10:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2175184#M240911</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-09-24T17:10:34Z</dc:date>
    </item>
    <item>
      <title>Re: MX8ULP_DDR_Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2175200#M240913</link>
      <description>&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;this was also my understanding. So the external RAM is only for testing and it should not matter if there is something wrong, the image should run. I would expect some error messages when there is a test that fails. But what I see is, that the test image stops running. Is there a way to check if the image is still running over the serial port?&lt;/P&gt;&lt;P&gt;BR Joerg&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 18:08:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2175200#M240913</guid>
      <dc:creator>Joerg_Ks</dc:creator>
      <dc:date>2025-09-24T18:08:07Z</dc:date>
    </item>
    <item>
      <title>Re: MX8ULP_DDR_Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2176483#M240973</link>
      <description>&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;to narrow it in another way, can NXP provide a list of errormessages, that the image can send to the customer? Maybe you can send me a link to the source o the image git?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;BR Joerg&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 09:10:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2176483#M240973</guid>
      <dc:creator>Joerg_Ks</dc:creator>
      <dc:date>2025-09-26T09:10:38Z</dc:date>
    </item>
    <item>
      <title>Re: MX8ULP_DDR_Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2176816#M240984</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;We do not have a&amp;nbsp;list of error messages from the tool.&lt;/P&gt;
&lt;P&gt;Usually the error log shows the cause of the issue.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 19:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2176816#M240984</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-09-26T19:15:33Z</dc:date>
    </item>
    <item>
      <title>Re: MX8ULP_DDR_Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2179265#M241103</link>
      <description>&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;can we have access to the sources of that Ramtest image? Thank you in advance.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Oct 2025 10:07:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2179265#M241103</guid>
      <dc:creator>Joerg_Ks</dc:creator>
      <dc:date>2025-10-02T10:07:21Z</dc:date>
    </item>
    <item>
      <title>Re: MX8ULP_DDR_Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2179418#M241119</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Unfortunately there are no source code available of DDR tool.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Oct 2025 14:27:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8ULP-DDR-Tool/m-p/2179418#M241119</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-10-02T14:27:16Z</dc:date>
    </item>
  </channel>
</rss>