<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Error while executing eIQ GenAI Flow Demonstrator on advantech aom-5521(iMX95)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2179145#M241095</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;As outlined in the hardware requirements, the current demo is limited to EVKs equipped with the &lt;STRONG&gt;WM8962 audio codec&lt;/STRONG&gt;. That’s why it doesn’t work with other codecs like the &lt;STRONG&gt;SGTL5000&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;The upcoming release, planned for this quarter,&amp;nbsp; will lift this restriction and allow the use of any codec — stay tuned!&lt;/P&gt;
&lt;P&gt;Thanks and best regards,&lt;BR /&gt;Pierre&lt;/P&gt;</description>
    <pubDate>Thu, 02 Oct 2025 06:32:28 GMT</pubDate>
    <dc:creator>Pierre_M</dc:creator>
    <dc:date>2025-10-02T06:32:28Z</dc:date>
    <item>
      <title>Error while executing eIQ GenAI Flow Demonstrator on advantech aom-5521(iMX95)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2175590#M240934</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am getting the following ALSA error when running eiq_genai_flow with asr enabled&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Currently we are using the SGTL5000 module, the system can detect it.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;Is it possible to configure the default sound card?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="python"&gt;root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow# ./eiq_genai_flow

Target Device: i.MX95

LLM used: danube-onnx

TTS model used 16kHz quantized

ALSA lib confmisc.c:855:(parse_card) cannot find card 'default'

ALSA lib conf.c:5204:(_snd_config_evaluate) function snd_func_card_inum returned error: No such device

ALSA lib confmisc.c:422:(snd_func_concat) error evaluating strings

ALSA lib conf.c:5204:(_snd_config_evaluate) function snd_func_concat returned error: No such device

ALSA lib confmisc.c:1342:(snd_func_refer) error evaluating name

ALSA lib conf.c:5204:(_snd_config_evaluate) function snd_func_refer returned error: No such device

ALSA lib conf.c:5727:(snd_config_expand) Evaluate error: No such device

ALSA lib pcm.c:2721:(snd_pcm_open_noupdate) Unknown PCM sysdefault:CARD=default

Exception in thread Thread-5 (handle_playback):

Traceback (most recent call last):

  File "threading.py", line 1075, in _bootstrap_inner

  File "threading.py", line 1012, in run

  File "tts/model.py", line 179, in handle_playback

  File "tts/player.py", line 23, in __init__

  File "tts/player.py", line 28, in open_pcm_device

alsaaudio.ALSAAudioError: No such device [sysdefault:CARD=default]&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="python"&gt;root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow# arecord -l

**** List of CAPTURE Hardware Devices ****

card 0: soundhdmi [sound-hdmi], device 0: 42670000.sai-i2s-hifi i2s-hifi-0 [42670000.sai-i2s-hifi i2s-hifi-0]

  Subdevices: 1/1

  Subdevice #0: subdevice #0

card 1: sgtl5000 [sgtl5000], device 0: HiFi sgtl5000-0 [HiFi sgtl5000-0]

  Subdevices: 1/1

  Subdevice #0: subdevice #0

root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow#&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Sep 2025 08:03:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2175590#M240934</guid>
      <dc:creator>yuii13</dc:creator>
      <dc:date>2025-09-25T08:03:23Z</dc:date>
    </item>
    <item>
      <title>Re: Error while executing eIQ GenAI Flow Demonstrator on advantech aom-5521(iMX95)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2176193#M240963</link>
      <description>&lt;P&gt;this configure file is for audio card and device configuration, maybe you can try to set your own codec here&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-appcodehub/dm-eiq-genai-flow-demonstrator/blob/main/eiq_genai_flow/audio_config.sh" target="_blank"&gt;https://github.com/nxp-appcodehub/dm-eiq-genai-flow-demonstrator/blob/main/eiq_genai_flow/audio_config.sh&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 02:32:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2176193#M240963</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-09-26T02:32:55Z</dc:date>
    </item>
    <item>
      <title>Re: Error while executing eIQ GenAI Flow Demonstrator on advantech aom-5521(iMX95)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2176272#M240966</link>
      <description>&lt;P&gt;After modifying "audio_config.sh", another error message occurs&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="python"&gt;root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow# ./audio_config.sh  capture
i.MX95
sysdefault:CARD=sgtl5000
Simple mixer control 'Capture',0
  Capabilities: cvolume cswitch cswitch-joined
  Capture channels: Front Left - Front Right
  Limits: Capture 0 - 15
  Front Left: Capture 15 [100%] [on]
  Front Right: Capture 15 [100%] [on]
root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow# ./audio_config.sh playback
i.MX95
sysdefault:CARD=sgtl5000
Simple mixer control 'Headphone',0
  Capabilities: pvolume pswitch pswitch-joined
  Playback channels: Front Left - Front Right
  Limits: Playback 0 - 127
  Mono:
  Front Left: Playback 110 [87%] [3.50dB] [on]
  Front Right: Playback 110 [87%] [3.50dB] [on]&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is the configure script I modified:&lt;/P&gt;&lt;LI-CODE lang="python"&gt;#!/bin/bash

# Copyright 2025 NXP
# NXP Proprietary.
# This software is owned or controlled by NXP and may only be used strictly in
# accordance with the applicable license terms. By expressly accepting such
# terms or by downloading, installing, activating and/or otherwise using the
# software, you are agreeing that you have read, and that you agree to comply
# with and are bound by, such license terms. If you do not agree to be bound
# by the applicable license terms, then you may not retain, install, activate
# or otherwise use the software.


audio_card_list() {
  cards=$(awk -F '[][]' '/\[.*\]/ {print $2}' /proc/asound/cards)
  echo "$cards"
}

get_audio_card() {
  supported_cards=$1
  device_cards=$2
  for s_card in $supported_cards; do
    for d_card in $device_cards; do
      if [[ "$s_card" == "$d_card" ]]; then
        echo "$d_card"
        return 1
      fi
    done
  done
  echo "default"
}

get_device() {
  # get architecture type
  arch=$(uname -m)
  soc_id=/sys/devices/soc0/soc_id
  if [ "$arch" == "x86_64" ]; then
    echo "PC"
  elif [ -f "$soc_id" ]; then
    cat $soc_id
  else
    echo "ERROR"
  fi
}

audio_setup() {
  mode=$1
  device=$(get_device)
  echo $(get_device)
  #supported_cards="wm8962audio wm8960audio"
  supported_cards="sgtl5000 wm8960audio"
  cards=$(audio_card_list)
  cur_card=$(get_audio_card "$supported_cards" "$cards")
  if [[ "$device" != "PC" ]]; then
    echo "sysdefault:CARD=$cur_card"
    if [[ $mode == "capture" ]]; then
      if [[ $cur_card == "sgtl5000" ]]; then
        amixer -c sgtl5000 sset 'Capture' 60
      elif [[ $cur_card == "wm8960audio" ]]; then
        amixer -c micfilaudio cset name='MICFIL Quality Select' 'High'
        amixer -c sgtl5000 sset 'Capture' 60
      else
        echo "'$cur_card' audio card doesn't exist"
      fi
    elif [[ $mode == "playback" ]]; then
      if [[ $cur_card == "sgtl5000" ]]; then
        amixer -c sgtl5000 set 'Headphone' 110 on
      elif [[ $cur_card == "wm8960audio" ]]; then
        amixer -c sgtl5000 set 'Headphone' 125
      else
        echo "'$cur_card' audio card doesn't exist"
      fi
    else
      echo "'$mode' mode doesn't exist use 'capture' or 'playback'"
    fi
  else # PC
    echo "$cur_card"
  fi
}

if [ $# -eq 1 ]; then
  audio_setup "$1"
else
  echo "ERROR!"
  echo "setup audio for capture or playback"
  echo "usage: audio_config.sh {capture,playback}"
fi&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 05:08:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2176272#M240966</guid>
      <dc:creator>yuii13</dc:creator>
      <dc:date>2025-09-26T05:08:52Z</dc:date>
    </item>
    <item>
      <title>Re: Error while executing eIQ GenAI Flow Demonstrator on advantech aom-5521(iMX95)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2177076#M240997</link>
      <description>&lt;P&gt;do you have any local DFAE support? currently, imx95 is still under prepordcution stage, I couldn't share any internal document or code with you, I suggest that you can contact local DFAE to get further support, and what new errors do you get? let me check if I can share anything here with you&lt;/P&gt;</description>
      <pubDate>Mon, 29 Sep 2025 00:18:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2177076#M240997</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-09-29T00:18:24Z</dc:date>
    </item>
    <item>
      <title>Re: Error while executing eIQ GenAI Flow Demonstrator on advantech aom-5521(iMX95)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2177436#M241014</link>
      <description>&lt;P&gt;Here is the new error message&lt;/P&gt;&lt;LI-CODE lang="python"&gt;root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow# ls
LICENSE.txt  _internal  asr  audio_config.sh  eiq_genai_flow  install.sh  llm  rag  tts
root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow# ./eiq_genai_flow
Target Device: i.MX95
LLM used: danube-onnx
TTS model used 16kHz quantized
ALSA lib pcm.c:2721:(snd_pcm_open_noupdate) Unknown PCM i.MX95
Exception in thread Thread-5 (handle_playback):
Traceback (most recent call last):
  File "threading.py", line 1075, in _bootstrap_inner
  File "threading.py", line 1012, in run
  File "tts/model.py", line 179, in handle_playback
  File "tts/player.py", line 23, in __init__
  File "tts/player.py", line 28, in open_pcm_device
alsaaudio.ALSAAudioError: No such file or directory [i.MX95]

Please type your question:&lt;/LI-CODE&gt;</description>
      <pubDate>Mon, 29 Sep 2025 11:23:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2177436#M241014</guid>
      <dc:creator>yuii13</dc:creator>
      <dc:date>2025-09-29T11:23:43Z</dc:date>
    </item>
    <item>
      <title>Re: Error while executing eIQ GenAI Flow Demonstrator on advantech aom-5521(iMX95)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2179145#M241095</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;As outlined in the hardware requirements, the current demo is limited to EVKs equipped with the &lt;STRONG&gt;WM8962 audio codec&lt;/STRONG&gt;. That’s why it doesn’t work with other codecs like the &lt;STRONG&gt;SGTL5000&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;The upcoming release, planned for this quarter,&amp;nbsp; will lift this restriction and allow the use of any codec — stay tuned!&lt;/P&gt;
&lt;P&gt;Thanks and best regards,&lt;BR /&gt;Pierre&lt;/P&gt;</description>
      <pubDate>Thu, 02 Oct 2025 06:32:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-executing-eIQ-GenAI-Flow-Demonstrator-on-advantech/m-p/2179145#M241095</guid>
      <dc:creator>Pierre_M</dc:creator>
      <dc:date>2025-10-02T06:32:28Z</dc:date>
    </item>
  </channel>
</rss>