<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Reducing i.MX6ULL Yocto boot time</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-i-MX6ULL-Yocto-boot-time/m-p/2177946#M241043</link>
    <description>Hello, thank you for the link. Do you have any advice on how to reduce the systemd-udev-trigger.service time? I have to use systemd on my system.</description>
    <pubDate>Tue, 30 Sep 2025 06:51:19 GMT</pubDate>
    <dc:creator>Phill231</dc:creator>
    <dc:date>2025-09-30T06:51:19Z</dc:date>
    <item>
      <title>Reducing i.MX6ULL Yocto boot time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-i-MX6ULL-Yocto-boot-time/m-p/2176963#M240992</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I’m working on a custom board based on i.MX6ULL running Yocto, and I would like to reduce the boot time as much as possible.&lt;/P&gt;&lt;P&gt;So far, I have:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Disabled all unnecessary options from the kernel (menuconfig)&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Reduced the Yocto image to the bare minimum, keeping only the required components&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;From the attached systemd-analyze plot (which also shows the Yocto and kernel versions used), I noticed that &lt;STRONG&gt;systemd-udev-trigger.service&amp;nbsp;&lt;/STRONG&gt;is taking a significant amount of time during boot.&lt;BR /&gt;I already tried to disable some unused udev rules (e.g. by linking them to /dev/null such as ln -s /dev/null /etc/udev/rules.d/60-cdrom_id.rules), but the impact was limited.&lt;/P&gt;&lt;P&gt;Is there any recommended approach or best practice to further reduce the boot time in this case?&lt;BR /&gt;Any tips or experiences from others working with i.MX6ULL fast boot would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Sat, 27 Sep 2025 21:40:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reducing-i-MX6ULL-Yocto-boot-time/m-p/2176963#M240992</guid>
      <dc:creator>Phill231</dc:creator>
      <dc:date>2025-09-27T21:40:10Z</dc:date>
    </item>
    <item>
      <title>Re: Reducing i.MX6ULL Yocto boot time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-i-MX6ULL-Yocto-boot-time/m-p/2177642#M241029</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can refer to this post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-Fast-Boot-on-i-MX6-Sabresd-Board/ta-p/1102298" target="_self"&gt;Linux Fast Boot on i.MX6 Sabresd Board&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Mon, 29 Sep 2025 17:51:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reducing-i-MX6ULL-Yocto-boot-time/m-p/2177642#M241029</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-09-29T17:51:28Z</dc:date>
    </item>
    <item>
      <title>Re: Reducing i.MX6ULL Yocto boot time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-i-MX6ULL-Yocto-boot-time/m-p/2177946#M241043</link>
      <description>Hello, thank you for the link. Do you have any advice on how to reduce the systemd-udev-trigger.service time? I have to use systemd on my system.</description>
      <pubDate>Tue, 30 Sep 2025 06:51:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reducing-i-MX6ULL-Yocto-boot-time/m-p/2177946#M241043</guid>
      <dc:creator>Phill231</dc:creator>
      <dc:date>2025-09-30T06:51:19Z</dc:date>
    </item>
  </channel>
</rss>