<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX95 is equipped with the GC05A2 camera in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX95-is-equipped-with-the-GC05A2-camera/m-p/2177390#M241010</link>
    <description>&lt;P&gt;HI NXP&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;1.&lt;SPAN&gt;I want to debug the GC05A2 now. This camera does not have an ISP. How should I configure it to process through the CPU's ISP after modification?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 29 Sep 2025 10:03:19 GMT</pubDate>
    <dc:creator>yrj</dc:creator>
    <dc:date>2025-09-29T10:03:19Z</dc:date>
    <item>
      <title>IMX95 is equipped with the GC05A2 camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX95-is-equipped-with-the-GC05A2-camera/m-p/2177390#M241010</link>
      <description>&lt;P&gt;HI NXP&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;1.&lt;SPAN&gt;I want to debug the GC05A2 now. This camera does not have an ISP. How should I configure it to process through the CPU's ISP after modification?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Sep 2025 10:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX95-is-equipped-with-the-GC05A2-camera/m-p/2177390#M241010</guid>
      <dc:creator>yrj</dc:creator>
      <dc:date>2025-09-29T10:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: IMX95 is equipped with the GC05A2 camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX95-is-equipped-with-the-GC05A2-camera/m-p/2177630#M241026</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253076"&gt;@yrj&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Unfortunately, the GC05A2 camera is not currently supported in our BSP.&lt;/P&gt;
&lt;P&gt;However, if your sensor is compatible with the RAW Bayer format and adheres to the Linux camera subsystem (V4L2/media controller framework), the &lt;A href="https://www.nxp.com/docs/en/user-guide/UG10215.pdf" target="_self"&gt;&lt;STRONG&gt;i.MX 95 Camera Porting Guide&lt;/STRONG&gt; &lt;/A&gt;(UG10215) can help you develop the appropriate driver for integration with the i.MX95 platform.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Sep 2025 17:29:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX95-is-equipped-with-the-GC05A2-camera/m-p/2177630#M241026</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2025-09-29T17:29:35Z</dc:date>
    </item>
  </channel>
</rss>