<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.m.x 8M Plus linux image build error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-m-x-8M-Plus-linux-image-build-error/m-p/2175750#M240943</link>
    <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working with i.m.x 8M plus processor, i have followed the required steps to build multimedia image. I am facing bitbake time out error.&lt;/P&gt;&lt;P&gt;followed this below document as reference. And attaching the error image for reference.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Used build command: bitbake imx-image-multimedia&lt;/P&gt;&lt;P&gt;Ubuntu version : 22.04&lt;/P&gt;&lt;P&gt;RAM : 16 GB.&lt;/P&gt;&lt;P&gt;Please provide a solution to solve this error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Naveen&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Thu, 25 Sep 2025 10:45:21 GMT</pubDate>
    <dc:creator>Naveen_N1</dc:creator>
    <dc:date>2025-09-25T10:45:21Z</dc:date>
    <item>
      <title>i.m.x 8M Plus linux image build error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-m-x-8M-Plus-linux-image-build-error/m-p/2175750#M240943</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working with i.m.x 8M plus processor, i have followed the required steps to build multimedia image. I am facing bitbake time out error.&lt;/P&gt;&lt;P&gt;followed this below document as reference. And attaching the error image for reference.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Used build command: bitbake imx-image-multimedia&lt;/P&gt;&lt;P&gt;Ubuntu version : 22.04&lt;/P&gt;&lt;P&gt;RAM : 16 GB.&lt;/P&gt;&lt;P&gt;Please provide a solution to solve this error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Naveen&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 25 Sep 2025 10:45:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-m-x-8M-Plus-linux-image-build-error/m-p/2175750#M240943</guid>
      <dc:creator>Naveen_N1</dc:creator>
      <dc:date>2025-09-25T10:45:21Z</dc:date>
    </item>
    <item>
      <title>Re: i.m.x 8M Plus linux image build error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-m-x-8M-Plus-linux-image-build-error/m-p/2176200#M240964</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Below are my suggestions to the error.&lt;/P&gt;
&lt;P&gt;Firstly As the size of RAM 16GB, which is not recommended to the Yocto image build. However, you can try to reduce concurrency and ease memory in con/local.conf&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;!--ScriptorStartFragment--&gt;BB_NUMBER_THREADS = "N"&lt;!--ScriptorEndFragment--&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;!--ScriptorStartFragment--&gt;PARALLEL_MAKE = "-j N"&lt;!--ScriptorEndFragment--&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;More details, you can refer to&amp;nbsp;&lt;A href="https://docs.yoctoproject.org/dev-manual/speeding-up-build.html" target="_self"&gt;here&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Then can check if stale lock files in build directory if so, then remove and restart the build.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 03:07:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-m-x-8M-Plus-linux-image-build-error/m-p/2176200#M240964</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-09-26T03:07:39Z</dc:date>
    </item>
  </channel>
</rss>