<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Image problem for imx95</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2175649#M240939</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I use a IMX 95 verdin toradex A1 (not a B0)&lt;/P&gt;&lt;P&gt;The current Yocto on gitlab is made for B0&lt;/P&gt;&lt;P&gt;i get a prebuild image for A1 , it works&lt;/P&gt;&lt;P&gt;Olivier&lt;/P&gt;</description>
    <pubDate>Thu, 25 Sep 2025 09:04:23 GMT</pubDate>
    <dc:creator>OlivierG</dc:creator>
    <dc:date>2025-09-25T09:04:23Z</dc:date>
    <item>
      <title>Image problem for imx95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2159186#M240355</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I created an image for imx95 in full mode.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Once I had the image, to flash the image to an SD card, I ran: &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;sudo dd if=imx-image-full-imx95-95-19x19-verdin.rootfs.wic of=/dev/sda bs=1M $$ sync &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;The "root" volume is correct.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;But the "boot" volume is incorrect.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Instead of being named "boot," it's named "268 MB volume" and it's empty.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Obviously, this SD card won't boot.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;What's the problem?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Is there an existing full imx95 verdin image?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Greetings&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Olivier&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Aug 2025 12:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2159186#M240355</guid>
      <dc:creator>OlivierG</dc:creator>
      <dc:date>2025-08-27T12:16:18Z</dc:date>
    </item>
    <item>
      <title>Re: Image problem for imx95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2159207#M240356</link>
      <description>&lt;P&gt;finally the boot volume is present&lt;/P&gt;&lt;P&gt;But the image dos not boot , no log on the debug channel, no screen display&lt;/P&gt;&lt;P&gt;i have a Toradex&amp;nbsp; IMX95 Verdin EVk&amp;nbsp;&lt;/P&gt;&lt;P&gt;i build the kernel with&lt;/P&gt;&lt;P&gt;MACHINE=imx95-19x19-verdin&lt;/P&gt;&lt;P&gt;is it right ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Olivier&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Aug 2025 13:14:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2159207#M240356</guid>
      <dc:creator>OlivierG</dc:creator>
      <dc:date>2025-08-27T13:14:43Z</dc:date>
    </item>
    <item>
      <title>Re: Image problem for imx95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2159234#M240357</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245939"&gt;@OlivierG&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing very well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please share your part number?&lt;/P&gt;
&lt;P&gt;Also, Have you tried flashing the image with UUU tool instead with the direct dd command?&lt;/P&gt;
&lt;P&gt;In our BSP we support the Machine imx95-19x19-verdin, so it is correct.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Aug 2025 14:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2159234#M240357</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2025-08-27T14:20:30Z</dc:date>
    </item>
    <item>
      <title>Re: Image problem for imx95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2159723#M240372</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;i launch :&amp;nbsp;sudo uuu -lsusb&lt;/P&gt;&lt;P&gt;i get&lt;/P&gt;&lt;DIV&gt;uuu (Universal Update Utility) for nxp imx chips -- lib1.5.141&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Connected Known USB Devices&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Path Chip Pro Vid Pid BcdVersion&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;==================================================&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;1:2 MX95 SDPS: 0x1FC9 0x015D 0x0001&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;i launch&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;sudo uuu -b sd imx-boot-imx95-19x19-verdin-sd.bin-flash_all&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;i get&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;uuu (Universal Update Utility) for nxp imx chips -- lib1.5.141&lt;/P&gt;&lt;P&gt;Success 0 Failure 1&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;1:2 1/ 1 [HID(W):&lt;STRONG&gt;LIBUSB_ERROR_NO_DEVICE&lt;/STRONG&gt; ] SDPS: boot -f imx-boot-imx95-19x19-verdin-sd.bin-flash_all&lt;/P&gt;&lt;P&gt;These commands are launch from a Linux ubuntu 24&lt;/P&gt;&lt;P&gt;Where is the problem ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Olivier&lt;/P&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Aug 2025 07:31:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2159723#M240372</guid>
      <dc:creator>OlivierG</dc:creator>
      <dc:date>2025-08-28T07:31:53Z</dc:date>
    </item>
    <item>
      <title>Re: Image problem for imx95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2161663#M240447</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245939"&gt;@OlivierG&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please try with:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;$ sudo uuu -b sd_all imx-boot-imx95-19x19-verdin-sd.bin-flash_all &amp;lt;your image.wic&amp;gt;&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 01:52:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2161663#M240447</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2025-09-02T01:52:02Z</dc:date>
    </item>
    <item>
      <title>Re: Image problem for imx95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2175649#M240939</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I use a IMX 95 verdin toradex A1 (not a B0)&lt;/P&gt;&lt;P&gt;The current Yocto on gitlab is made for B0&lt;/P&gt;&lt;P&gt;i get a prebuild image for A1 , it works&lt;/P&gt;&lt;P&gt;Olivier&lt;/P&gt;</description>
      <pubDate>Thu, 25 Sep 2025 09:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2175649#M240939</guid>
      <dc:creator>OlivierG</dc:creator>
      <dc:date>2025-09-25T09:04:23Z</dc:date>
    </item>
    <item>
      <title>Re: Image problem for imx95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2301341#M243648</link>
      <description>Hello, we also encountered a similar issue when using IMX95. We compiled the image using the Android 15.0.0_1.2.0 source code, and initially it could be burned and used normally. However, when the hardware engineer replaced the CPU with a new one, we used the same burning command but encountered errors such as LIBUSB-ERRORD_IO (-1) or LIBUSB-ERRORD_DEVICED (-4),&lt;BR /&gt;The burning command is as follows:&lt;BR /&gt;sudo ./uuu_imx_android_flash.sh -f imx95 -e -u dual -d mipi-panel&lt;BR /&gt;We used Android 15.0.0_2.0.0 source code to compile the image, but when burning it, we received the same error message;&lt;BR /&gt;How to correctly burn and write</description>
      <pubDate>Tue, 27 Jan 2026 12:30:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Image-problem-for-imx95/m-p/2301341#M243648</guid>
      <dc:creator>zhou1211</dc:creator>
      <dc:date>2026-01-27T12:30:48Z</dc:date>
    </item>
  </channel>
</rss>