<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: iMX8ULP XIP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8ULP-XIP/m-p/2175328#M240918</link>
    <description>Thanks for the reply! I assume after running that uuu command, I can also flash the A35 image to eMMC the same as usual?</description>
    <pubDate>Thu, 25 Sep 2025 01:26:09 GMT</pubDate>
    <dc:creator>sb_3</dc:creator>
    <dc:date>2025-09-25T01:26:09Z</dc:date>
    <item>
      <title>iMX8ULP XIP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8ULP-XIP/m-p/2174549#M240878</link>
      <description>&lt;P&gt;I'm haven't come across any resources for flashing the M33 on the iMX8ULP to execute in place from NOR.&lt;/P&gt;&lt;P&gt;I can run the flash_debug.sh script to build the app and place the sections based on the flash linker file. My assumption is that I need to run `mkimage_imx8` with the target of "flash_dualboot_m33_xip" (memory address of MCU_XIP_ADDR aligns with the interrupts/text section in the linker file). After creating that flash.bin (result of flash_dualboot_m33_xip), I'm having issues flashing with UUU. I've downloaded LF_v6.6.52-2.2.0_images_IMX8ULPEVK from the NXP page for the system, but I don't see any references to the XIP used.&lt;/P&gt;&lt;P&gt;My end goal is to have my M33 app execute in place from NOR and my A35 app be in eMMC.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 20:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8ULP-XIP/m-p/2174549#M240878</guid>
      <dc:creator>sb_3</dc:creator>
      <dc:date>2025-09-23T20:31:08Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8ULP XIP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8ULP-XIP/m-p/2175259#M240914</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;For this you will need to have 2 boot images, where one would be used as a flashing tool and the image to be flashed. With this you may used the following&amp;nbsp; command:&lt;/P&gt;
&lt;P&gt;uuu –b qspi flash-singleboot.bin flash-dualboot-m33_xip.bin&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 21:54:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8ULP-XIP/m-p/2175259#M240914</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-09-24T21:54:02Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8ULP XIP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8ULP-XIP/m-p/2175328#M240918</link>
      <description>Thanks for the reply! I assume after running that uuu command, I can also flash the A35 image to eMMC the same as usual?</description>
      <pubDate>Thu, 25 Sep 2025 01:26:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8ULP-XIP/m-p/2175328#M240918</guid>
      <dc:creator>sb_3</dc:creator>
      <dc:date>2025-09-25T01:26:09Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8ULP XIP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8ULP-XIP/m-p/2175945#M240952</link>
      <description>Hello,&lt;BR /&gt;&lt;BR /&gt;Yes, you may do so without a problem.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.</description>
      <pubDate>Thu, 25 Sep 2025 15:48:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8ULP-XIP/m-p/2175945#M240952</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-09-25T15:48:12Z</dc:date>
    </item>
  </channel>
</rss>