<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSDK for IMX8M PLUS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SDK-for-IMX8M-PLUS/m-p/2174475#M240877</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;I am starting development with the i.MX 8M Plus processor and I need guidance on which SDK/toolchain to use to build my projects and generate binaries that will run on the processor.&lt;/P&gt;&lt;P&gt;For the CORTEX A53&amp;nbsp;(Linux/Android side):&lt;BR /&gt;&amp;nbsp;-Should I use the NXP BSP for building Linux images and applications?&lt;BR /&gt;&amp;nbsp;-For application development (e.g., Qt GUI, multimedia), do I use the SDK/toolchain generated from (cross-compilation environment), or is there a separate SDK package?&lt;/P&gt;</description>
    <pubDate>Tue, 23 Sep 2025 17:56:06 GMT</pubDate>
    <dc:creator>parvathitp</dc:creator>
    <dc:date>2025-09-23T17:56:06Z</dc:date>
    <item>
      <title>SDK for IMX8M PLUS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDK-for-IMX8M-PLUS/m-p/2174475#M240877</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I am starting development with the i.MX 8M Plus processor and I need guidance on which SDK/toolchain to use to build my projects and generate binaries that will run on the processor.&lt;/P&gt;&lt;P&gt;For the CORTEX A53&amp;nbsp;(Linux/Android side):&lt;BR /&gt;&amp;nbsp;-Should I use the NXP BSP for building Linux images and applications?&lt;BR /&gt;&amp;nbsp;-For application development (e.g., Qt GUI, multimedia), do I use the SDK/toolchain generated from (cross-compilation environment), or is there a separate SDK package?&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 17:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDK-for-IMX8M-PLUS/m-p/2174475#M240877</guid>
      <dc:creator>parvathitp</dc:creator>
      <dc:date>2025-09-23T17:56:06Z</dc:date>
    </item>
    <item>
      <title>Re: SDK for IMX8M PLUS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDK-for-IMX8M-PLUS/m-p/2175152#M240910</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/255147"&gt;@parvathitp&lt;/a&gt;,&lt;BR /&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;For Linux development, you can use the ARM toolchain; however, I recommend generating the Yocto SDK to obtain a fully compatible toolchain for cross-compiling your applications.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;You can find the Yocto SDK deployment instructions at the following link:&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-compile-Linux-Kernel-Image-and-device-tree-using-Yocto/ta-p/2022759" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-compile-Linux-Kernel-Image-and-device-tree-using-Yocto/ta-p/2022759&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 16:21:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDK-for-IMX8M-PLUS/m-p/2175152#M240910</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2025-09-24T16:21:03Z</dc:date>
    </item>
  </channel>
</rss>