<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using SCU_GPIO0_01 as a GPIO from A35 on i.MX 8QuadXPlus in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-SCU-GPIO0-01-as-a-GPIO-from-A35-on-i-MX-8QuadXPlus/m-p/2172937#M240836</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Is needed to modify SCFW to modify IOMUX registers as you can check in:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Pad-configuration-service/ta-p/1124213" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Pad-configuration-service/ta-p/1124213&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest you take a look in the next post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/How-to-access-SCU-GPIO0-00-from-core-A35-u-boot-or-Linux/td-p/1423541" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/How-to-access-SCU-GPIO0-00-from-core-A35-u-boot-or-Linux/td-p/1423541&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Fri, 19 Sep 2025 18:48:49 GMT</pubDate>
    <dc:creator>JorgeCas</dc:creator>
    <dc:date>2025-09-19T18:48:49Z</dc:date>
    <item>
      <title>Using SCU_GPIO0_01 as a GPIO from A35 on i.MX 8QuadXPlus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-SCU-GPIO0-01-as-a-GPIO-from-A35-on-i-MX-8QuadXPlus/m-p/2172860#M240832</link>
      <description>&lt;P&gt;Is it possible to change the output of SCU_GPIO0_01 from the A35 in Yocto Linux 6.6.y without changing either the SCU or the M40 firmware?&lt;/P&gt;&lt;P&gt;I am working with a hardware design that is already mature and has&amp;nbsp;SCU_GPIO0_01 wired out to other logic circuits that I need to control.&lt;/P&gt;&lt;P&gt;Or, is it possible to change the pinmux function of that pin from Linux userspace?&amp;nbsp; I have found that switching between the functions&amp;nbsp;SCU_GPIO0_IO01 and M40_UART0_TX by changing device trees and rebooting gives the low and high outputs on that pin that I am seeking, so changing the pinmux from userspace would be another way that I could control that line if changing the drive directly is not an option.&lt;/P&gt;</description>
      <pubDate>Fri, 19 Sep 2025 15:03:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-SCU-GPIO0-01-as-a-GPIO-from-A35-on-i-MX-8QuadXPlus/m-p/2172860#M240832</guid>
      <dc:creator>wmr-veranex</dc:creator>
      <dc:date>2025-09-19T15:03:57Z</dc:date>
    </item>
    <item>
      <title>Re: Using SCU_GPIO0_01 as a GPIO from A35 on i.MX 8QuadXPlus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-SCU-GPIO0-01-as-a-GPIO-from-A35-on-i-MX-8QuadXPlus/m-p/2172937#M240836</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Is needed to modify SCFW to modify IOMUX registers as you can check in:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Pad-configuration-service/ta-p/1124213" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Pad-configuration-service/ta-p/1124213&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest you take a look in the next post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/How-to-access-SCU-GPIO0-00-from-core-A35-u-boot-or-Linux/td-p/1423541" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/How-to-access-SCU-GPIO0-00-from-core-A35-u-boot-or-Linux/td-p/1423541&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Fri, 19 Sep 2025 18:48:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-SCU-GPIO0-01-as-a-GPIO-from-A35-on-i-MX-8QuadXPlus/m-p/2172937#M240836</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-09-19T18:48:49Z</dc:date>
    </item>
  </channel>
</rss>