<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic [imx8mm] tinycompress test tool not working on Yocto image in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-tinycompress-test-tool-not-working-on-Yocto-image/m-p/2172689#M240825</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have &lt;STRONG&gt;imx8mm EVK&lt;/STRONG&gt; platform with image:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;LF_v6.6.52-2.2.1_images_IMX8MMEVK/imx-image-full-imx8mmevk.wic&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;flashed on it. When I was trying to use a test tool &lt;STRONG&gt;cplay&lt;/STRONG&gt; that is shipped with package tinycompress, I encountered following error:&lt;/P&gt;&lt;PRE&gt;root@imx8mmevk:~# cplay test.mp3&lt;BR /&gt;Unable to open Compress device 0:0&lt;BR /&gt;ERR: cannot open device '/dev/snd/comprC0D0': No such file or directory&lt;/PRE&gt;&lt;P&gt;In fact, I don't see any &lt;STRONG&gt;comprCxDy&lt;/STRONG&gt; devices under &lt;STRONG&gt;/dev/snd/&lt;/STRONG&gt;, so modifying the tool call with flags has no effect as it always ends up looking for compress devices. Could you help me determine if it's possible to make this example work? I suppose tinycompress is installed mostly as a gstreamer dependency, but I was wondering if it can work standalone, e.g. via mentioned &lt;STRONG&gt;cplay&lt;/STRONG&gt;&amp;nbsp;tool example.&lt;/P&gt;</description>
    <pubDate>Fri, 19 Sep 2025 09:19:19 GMT</pubDate>
    <dc:creator>krzysztof-buczak-red</dc:creator>
    <dc:date>2025-09-19T09:19:19Z</dc:date>
    <item>
      <title>[imx8mm] tinycompress test tool not working on Yocto image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-tinycompress-test-tool-not-working-on-Yocto-image/m-p/2172689#M240825</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have &lt;STRONG&gt;imx8mm EVK&lt;/STRONG&gt; platform with image:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;LF_v6.6.52-2.2.1_images_IMX8MMEVK/imx-image-full-imx8mmevk.wic&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;flashed on it. When I was trying to use a test tool &lt;STRONG&gt;cplay&lt;/STRONG&gt; that is shipped with package tinycompress, I encountered following error:&lt;/P&gt;&lt;PRE&gt;root@imx8mmevk:~# cplay test.mp3&lt;BR /&gt;Unable to open Compress device 0:0&lt;BR /&gt;ERR: cannot open device '/dev/snd/comprC0D0': No such file or directory&lt;/PRE&gt;&lt;P&gt;In fact, I don't see any &lt;STRONG&gt;comprCxDy&lt;/STRONG&gt; devices under &lt;STRONG&gt;/dev/snd/&lt;/STRONG&gt;, so modifying the tool call with flags has no effect as it always ends up looking for compress devices. Could you help me determine if it's possible to make this example work? I suppose tinycompress is installed mostly as a gstreamer dependency, but I was wondering if it can work standalone, e.g. via mentioned &lt;STRONG&gt;cplay&lt;/STRONG&gt;&amp;nbsp;tool example.&lt;/P&gt;</description>
      <pubDate>Fri, 19 Sep 2025 09:19:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-tinycompress-test-tool-not-working-on-Yocto-image/m-p/2172689#M240825</guid>
      <dc:creator>krzysztof-buczak-red</dc:creator>
      <dc:date>2025-09-19T09:19:19Z</dc:date>
    </item>
    <item>
      <title>Re: [imx8mm] tinycompress test tool not working on Yocto image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-tinycompress-test-tool-not-working-on-Yocto-image/m-p/2172871#M240834</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Cplay is not the default in yocto bsp, you should try&amp;nbsp;&lt;SPAN data-huuid="10866126959677342151"&gt; &lt;CODE class="mv6bHd"&gt;aplay -D plughw:0,0 your_sound.wav&lt;/CODE&gt; &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 19 Sep 2025 15:26:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-tinycompress-test-tool-not-working-on-Yocto-image/m-p/2172871#M240834</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-09-19T15:26:54Z</dc:date>
    </item>
  </channel>
</rss>