<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx95 MIPI display abnormality</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx95-MIPI-display-abnormality/m-p/2171640#M240788</link>
    <description>&lt;P&gt;You can see that they are two difference boards, you can see board dts file are seperate:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/linux-imx/tree/lf-6.12.y/arch/arm64/boot/dts/freescale" target="_blank"&gt;linux-imx/arch/arm64/boot/dts/freescale at lf-6.12.y · nxp-imx/linux-imx · GitHub&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Here for the screen it is supply with the EVK board, or you need to porting to the&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;imx95-15x15-evk?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 18 Sep 2025 05:31:35 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2025-09-18T05:31:35Z</dc:date>
    <item>
      <title>imx95 MIPI display abnormality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx95-MIPI-display-abnormality/m-p/2170341#M240745</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 1.The environment is: yocto version: 6.12.20&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 2.The issue is: the MIPI display is abnormal, as shown in the attached image.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 3.The reference device tree is: kernel/arch/arm64/boot/dts/freescale/imx95-15x15-evk-rm692c9.dtso&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 4.Add driver location: kernel/drivers/gpu/drm/panel/panel-gnl-n91.c&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1167ac76b15af49acd7d67f842174851.jpg"&gt;&lt;img src="https://community.nxp.com/skins/images/1952261F51BAC158583A3F3DFA7EA645/responsive_peak/images/image_not_found.png" alt="1167ac76b15af49acd7d67f842174851.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Tue, 16 Sep 2025 09:29:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx95-MIPI-display-abnormality/m-p/2170341#M240745</guid>
      <dc:creator>yrj</dc:creator>
      <dc:date>2025-09-16T09:29:02Z</dc:date>
    </item>
    <item>
      <title>Re: imx95 MIPI display abnormality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx95-MIPI-display-abnormality/m-p/2171564#M240784</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253076"&gt;@yrj&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Which board are you using? I see that you said you are using the&amp;nbsp;&lt;SPAN&gt;imx95-15x15-evk board, but in the log I see "imx95-19x19-lpddr5-evk log in", are you uisng this board X-IMX95LP5EVK-15?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For the MIPI display, the screen is you buy from our NXP, or other company , here you porting it to NXP board? Thanks.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Wish you have a nice day&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Rita&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 02:56:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx95-MIPI-display-abnormality/m-p/2171564#M240784</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-09-18T02:56:37Z</dc:date>
    </item>
    <item>
      <title>Re: imx95 MIPI display abnormality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx95-MIPI-display-abnormality/m-p/2171571#M240785</link>
      <description>Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57740"&gt;@Rita_Wang&lt;/a&gt;&lt;BR /&gt;1.I am using the imx95-15x15-evk.&lt;BR /&gt;2.Does the filename (imx95-19x19-lpddr5-evk) in the file system /etc/hostname have an impact?</description>
      <pubDate>Thu, 18 Sep 2025 03:12:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx95-MIPI-display-abnormality/m-p/2171571#M240785</guid>
      <dc:creator>yrj</dc:creator>
      <dc:date>2025-09-18T03:12:27Z</dc:date>
    </item>
    <item>
      <title>Re: imx95 MIPI display abnormality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx95-MIPI-display-abnormality/m-p/2171640#M240788</link>
      <description>&lt;P&gt;You can see that they are two difference boards, you can see board dts file are seperate:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/linux-imx/tree/lf-6.12.y/arch/arm64/boot/dts/freescale" target="_blank"&gt;linux-imx/arch/arm64/boot/dts/freescale at lf-6.12.y · nxp-imx/linux-imx · GitHub&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Here for the screen it is supply with the EVK board, or you need to porting to the&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;imx95-15x15-evk?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 05:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx95-MIPI-display-abnormality/m-p/2171640#M240788</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-09-18T05:31:35Z</dc:date>
    </item>
  </channel>
</rss>