<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Custom HDMI Resolution on i.MX 8M Plus (Yocto) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Custom-HDMI-Resolution-on-i-MX-8M-Plus-Yocto/m-p/2168749#M240685</link>
    <description>&lt;P&gt;Repost: Hello, I'm using Yocto on an &lt;STRONG&gt;i.MX 8M Plus&lt;/STRONG&gt; and I need to get HDMI output at &lt;STRONG&gt;3840x726@60Hz&lt;/STRONG&gt; and &lt;STRONG&gt;3840x1080@60Hz&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;These aren't available in Weston, so I believe I need to modify the kernel. Can anyone provide guidance on how to add these custom resolutions to the kernel or device tree?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Fri, 12 Sep 2025 08:30:07 GMT</pubDate>
    <dc:creator>masalcp</dc:creator>
    <dc:date>2025-09-12T08:30:07Z</dc:date>
    <item>
      <title>Custom HDMI Resolution on i.MX 8M Plus (Yocto)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-HDMI-Resolution-on-i-MX-8M-Plus-Yocto/m-p/2168749#M240685</link>
      <description>&lt;P&gt;Repost: Hello, I'm using Yocto on an &lt;STRONG&gt;i.MX 8M Plus&lt;/STRONG&gt; and I need to get HDMI output at &lt;STRONG&gt;3840x726@60Hz&lt;/STRONG&gt; and &lt;STRONG&gt;3840x1080@60Hz&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;These aren't available in Weston, so I believe I need to modify the kernel. Can anyone provide guidance on how to add these custom resolutions to the kernel or device tree?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Fri, 12 Sep 2025 08:30:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-HDMI-Resolution-on-i-MX-8M-Plus-Yocto/m-p/2168749#M240685</guid>
      <dc:creator>masalcp</dc:creator>
      <dc:date>2025-09-12T08:30:07Z</dc:date>
    </item>
  </channel>
</rss>