<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Secure Boot selecting key types and sizes</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-selecting-key-types-and-sizes/m-p/2166620#M240650</link>
    <description>&lt;P&gt;Hi Harvey&lt;/P&gt;&lt;P&gt;thanks a lot.&lt;BR /&gt;Are there any reasons not to use RSA 4096 or&amp;nbsp;ECC-P521? Seems to be supported for i.MX8Plus and QuadMax.&lt;/P&gt;&lt;P&gt;Best Regards&lt;BR /&gt;Thomas&lt;/P&gt;</description>
    <pubDate>Wed, 10 Sep 2025 11:21:24 GMT</pubDate>
    <dc:creator>ThomasGu</dc:creator>
    <dc:date>2025-09-10T11:21:24Z</dc:date>
    <item>
      <title>Secure Boot selecting key types and sizes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-selecting-key-types-and-sizes/m-p/2163751#M240526</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;As there is currently heated debate about which cryptographic methods will still be secure in the future, the question arises as to what keys should be used for Secure Boot.&lt;BR /&gt;Currently we have i.MX8M Plus (HAB4) and i.MX8 QuadMax (AHAB).&lt;BR /&gt;Questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is it possible to mix key types (e.g. 2 RSA keys and 2 EC keys)?&lt;/LI&gt;&lt;LI&gt;Which key types should be used to ensure the security of Secure Boot over the next 10 years?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thanks in Advance&lt;BR /&gt;Thomas&lt;/P&gt;</description>
      <pubDate>Thu, 04 Sep 2025 15:06:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-selecting-key-types-and-sizes/m-p/2163751#M240526</guid>
      <dc:creator>ThomasGu</dc:creator>
      <dc:date>2025-09-04T15:06:10Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Boot selecting key types and sizes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-selecting-key-types-and-sizes/m-p/2164822#M240563</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Would suggest to choose key length, at least, 3K for RSA and 384 for ECC for help. Our HAB/AHAB architecture based on PKI tree to generate key and certificate with one type of key.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Sep 2025 03:49:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-selecting-key-types-and-sizes/m-p/2164822#M240563</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-09-08T03:49:42Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Boot selecting key types and sizes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-selecting-key-types-and-sizes/m-p/2166620#M240650</link>
      <description>&lt;P&gt;Hi Harvey&lt;/P&gt;&lt;P&gt;thanks a lot.&lt;BR /&gt;Are there any reasons not to use RSA 4096 or&amp;nbsp;ECC-P521? Seems to be supported for i.MX8Plus and QuadMax.&lt;/P&gt;&lt;P&gt;Best Regards&lt;BR /&gt;Thomas&lt;/P&gt;</description>
      <pubDate>Wed, 10 Sep 2025 11:21:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-selecting-key-types-and-sizes/m-p/2166620#M240650</guid>
      <dc:creator>ThomasGu</dc:creator>
      <dc:date>2025-09-10T11:21:24Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Boot selecting key types and sizes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-selecting-key-types-and-sizes/m-p/2167309#M240658</link>
      <description>&lt;P&gt;hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201938"&gt;@ThomasGu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, the key length supported. To consider the key security, so I mentioned, at least, to choose 3k and p384. instead of 2k and p256.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Thu, 11 Sep 2025 02:00:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-selecting-key-types-and-sizes/m-p/2167309#M240658</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-09-11T02:00:39Z</dc:date>
    </item>
  </channel>
</rss>