<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic COCKPIT_A53 picked for IMX8 Quad Max, watchdog keeps resetting in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/COCKPIT-A53-picked-for-IMX8-Quad-Max-watchdog-keeps-resetting/m-p/2165951#M240620</link>
    <description>&lt;P&gt;I have watchdogs enabled originally for all 6 processors active on a Quad Max, then I enabled the COCKPIT_A53 setting in ATF. Now it appears that there is a watchdog triggering if the A72 processors are disabled (at the SCFW level/ not the device tree level).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any idea how to disable the watchdogs just for the A72 processors?&lt;/P&gt;</description>
    <pubDate>Tue, 09 Sep 2025 13:45:46 GMT</pubDate>
    <dc:creator>flobro</dc:creator>
    <dc:date>2025-09-09T13:45:46Z</dc:date>
    <item>
      <title>COCKPIT_A53 picked for IMX8 Quad Max, watchdog keeps resetting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/COCKPIT-A53-picked-for-IMX8-Quad-Max-watchdog-keeps-resetting/m-p/2165951#M240620</link>
      <description>&lt;P&gt;I have watchdogs enabled originally for all 6 processors active on a Quad Max, then I enabled the COCKPIT_A53 setting in ATF. Now it appears that there is a watchdog triggering if the A72 processors are disabled (at the SCFW level/ not the device tree level).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any idea how to disable the watchdogs just for the A72 processors?&lt;/P&gt;</description>
      <pubDate>Tue, 09 Sep 2025 13:45:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/COCKPIT-A53-picked-for-IMX8-Quad-Max-watchdog-keeps-resetting/m-p/2165951#M240620</guid>
      <dc:creator>flobro</dc:creator>
      <dc:date>2025-09-09T13:45:46Z</dc:date>
    </item>
    <item>
      <title>Re: COCKPIT_A53 picked for IMX8 Quad Max, watchdog keeps resetting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/COCKPIT-A53-picked-for-IMX8-Quad-Max-watchdog-keeps-resetting/m-p/2166074#M240627</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198929"&gt;@flobro&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for reaching out to NXP Support!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You're absolutely right, to prevent resets caused by the watchdog, it’s necessary to configure it properly within the SCFW as well.&lt;/P&gt;
&lt;P&gt;You can download the SCFW source code from the link below, based on the BSP version you're using:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_self"&gt;Embedded Linux for i.MX Applications Processors&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Once downloaded, run the binary file located in the&lt;STRONG&gt; packages&lt;/STRONG&gt; folder to extract the source code and documentation for SCFW.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Tue, 09 Sep 2025 17:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/COCKPIT-A53-picked-for-IMX8-Quad-Max-watchdog-keeps-resetting/m-p/2166074#M240627</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2025-09-09T17:23:33Z</dc:date>
    </item>
  </channel>
</rss>