<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDTS overlay for IMX8m Plus debix model B SCB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DTS-overlay-for-IMX8m-Plus-debix-model-B-SCB/m-p/2164531#M240553</link>
    <description>&lt;P&gt;Need documentation to help create a device tree overlay file to be able to implement on SAI5, and also to integrate an ADC6140EVM-PDK from TI to use audio capture at a sample rate of 786 kHz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Linux Ububtu 22.04.&lt;/P&gt;</description>
    <pubDate>Fri, 05 Sep 2025 18:04:40 GMT</pubDate>
    <dc:creator>rcfcpereira</dc:creator>
    <dc:date>2025-09-05T18:04:40Z</dc:date>
    <item>
      <title>DTS overlay for IMX8m Plus debix model B SCB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DTS-overlay-for-IMX8m-Plus-debix-model-B-SCB/m-p/2164531#M240553</link>
      <description>&lt;P&gt;Need documentation to help create a device tree overlay file to be able to implement on SAI5, and also to integrate an ADC6140EVM-PDK from TI to use audio capture at a sample rate of 786 kHz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Linux Ububtu 22.04.&lt;/P&gt;</description>
      <pubDate>Fri, 05 Sep 2025 18:04:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DTS-overlay-for-IMX8m-Plus-debix-model-B-SCB/m-p/2164531#M240553</guid>
      <dc:creator>rcfcpereira</dc:creator>
      <dc:date>2025-09-05T18:04:40Z</dc:date>
    </item>
    <item>
      <title>Re: DTS overlay for IMX8m Plus debix model B SCB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DTS-overlay-for-IMX8m-Plus-debix-model-B-SCB/m-p/2165202#M240588</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It turns out you do need to specify the channel in a multilane sai port. In any case., have to do this inside the codec:&lt;/P&gt;
&lt;P&gt;dailink0_master: simple-audio-card,cpu {&lt;BR /&gt;sound-dai = &amp;lt;&amp;amp;sai5 0&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is no documentation about this. The binding documentation and examples I found online were all referencing one lane sai.&lt;/P&gt;
&lt;P&gt;Hope this help.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Sep 2025 13:40:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DTS-overlay-for-IMX8m-Plus-debix-model-B-SCB/m-p/2165202#M240588</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-09-08T13:40:41Z</dc:date>
    </item>
  </channel>
</rss>