<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic android on imx95 verdin sd in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/android-on-imx95-verdin-sd/m-p/2162847#M240495</link>
    <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;How can I flash the android that nxp provides on a sd card for my imx95 verdin board that toradex makes? I need the full flash string, as when I use the params that contain "verdin" i keep getting: can not flash "trusty" on sd card.&lt;/P&gt;&lt;P&gt;Br,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ahelion&lt;/P&gt;</description>
    <pubDate>Wed, 03 Sep 2025 11:04:05 GMT</pubDate>
    <dc:creator>Ahelion</dc:creator>
    <dc:date>2025-09-03T11:04:05Z</dc:date>
    <item>
      <title>android on imx95 verdin sd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-on-imx95-verdin-sd/m-p/2162847#M240495</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;How can I flash the android that nxp provides on a sd card for my imx95 verdin board that toradex makes? I need the full flash string, as when I use the params that contain "verdin" i keep getting: can not flash "trusty" on sd card.&lt;/P&gt;&lt;P&gt;Br,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ahelion&lt;/P&gt;</description>
      <pubDate>Wed, 03 Sep 2025 11:04:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-on-imx95-verdin-sd/m-p/2162847#M240495</guid>
      <dc:creator>Ahelion</dc:creator>
      <dc:date>2025-09-03T11:04:05Z</dc:date>
    </item>
    <item>
      <title>Re: android on imx95 verdin sd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-on-imx95-verdin-sd/m-p/2163059#M240507</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225423"&gt;@Ahelion&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To flash the Android image, you can use the generated script uuu_imx_android_flash.sh with the following command:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;sudo ./uuu_imx_android_flash.sh -f imx95 -a -e -t sd&lt;/LI-CODE&gt;
&lt;P&gt;For detailed information about this script and the flashing process, please refer to the &lt;A href="https://www.nxp.com/docs/en/quick-reference-guide/ANDROID_QUICK_START_GUIDE.pdf" target="_self"&gt;Android Quick Start Guide&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Wed, 03 Sep 2025 17:54:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-on-imx95-verdin-sd/m-p/2163059#M240507</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2025-09-03T17:54:32Z</dc:date>
    </item>
  </channel>
</rss>