<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx93 uuu example_kernel_emmc commands stop after booting initramfs</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2162280#M240471</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196227"&gt;@Hector_Jimenez&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;If uuu isn't detecting the FBK ID, it usually means the bootloader isn't properly initializing the USB gadget or the image isn't entering the expected boot mode.&lt;/P&gt;
&lt;P&gt;Check your bootloader configuration: Make sure your custom image includes the correct USB gadget setup (e.g., fastboot or FBK mode).&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Use serial console logs: Connect via UART to see if the board is booting correctly and entering the expected mode.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 02 Sep 2025 16:03:44 GMT</pubDate>
    <dc:creator>Chavira</dc:creator>
    <dc:date>2025-09-02T16:03:44Z</dc:date>
    <item>
      <title>imx93 uuu example_kernel_emmc commands stop after booting initramfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2160781#M240412</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I'm using latest uuu aplication (windows11) with example_kernel_emmc commands (from LF_v6.6.52-2.2.1_images_IMX93EVK zip file) in order to define a partition table and drop some files there in an imx93 based device.&lt;/P&gt;&lt;P&gt;u-boot, kernel and initramfs image files used were provided in same zip file as example commands, device tree is customized to my device.&lt;/P&gt;&lt;P&gt;uuu executes all commands until:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;and remains there forever. No FBK Id is shown after booting:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;.\uuu.exe -lsusb&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.201-0-g727fc2b&lt;/P&gt;&lt;P&gt;Connected Known USB Devices&lt;BR /&gt;Path Chip Pro Vid Pid BcdVersion Serial_no&lt;BR /&gt;====================================================================&lt;BR /&gt;1:1 FB: 0x1FC9 0x0152 0x0221&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;so no FBK command is executed such as :&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;# get mmc dev number from kernel command line&lt;BR /&gt;# Wait for emmc&lt;BR /&gt;FBK: ucmd while [ ! -e /dev/mmcblk*boot0 ]; do sleep 1; echo "wait for /dev/mmcblk*boot* appear"; done;&lt;/P&gt;&lt;P&gt;# serach emmc device number, if your platform have more than two emmc chip, please echo dev number &amp;gt;/tmp/mmcdev&lt;BR /&gt;FBK: ucmd dev=`ls /dev/mmcblk*boot*`; dev=($dev); dev=${dev[0]}; dev=${dev#/dev/mmcblk}; dev=${dev%boot*}; echo $dev &amp;gt; /tmp/mmcdev;&lt;/P&gt;&lt;P&gt;# dd to clear the possible MBR&lt;BR /&gt;FBK: ucmd mmc=`cat /tmp/mmcdev`; dd if=/dev/zero of=/dev/mmcblk${mmc} bs=512 count=1&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;This is my boot messages (initramfs):&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050]&lt;BR /&gt;[ 0.000000] Linux version 6.6.52-lts-next-g90192c5d29cb (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240723) #1 SMP PREEMPT Tue Jul 8 12:00:06 UTC 2025&lt;BR /&gt;[ 0.000000] KASLR disabled due to lack of seed&lt;BR /&gt;[ 0.000000] Machine model: ICOM100 GMV board, DTS version 1.0&lt;BR /&gt;[ 0.000000] efi: UEFI not found.&lt;BR /&gt;[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000086000000, size 256 MiB&lt;BR /&gt;[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x0000000086000000..0x0000000095ffffff (262144 KiB) map reusable linux,cma&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x000000002021e000..0x000000002021efff (4 KiB) nomap non-reusable rsc-table@2021e000&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x0000000096000000..0x0000000097dfffff (30720 KiB) nomap non-reusable optee_core@96000000&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x0000000097e00000..0x0000000097ffffff (2048 KiB) nomap non-reusable optee_shm@97e00000&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a4000000..0x00000000a4007fff (32 KiB) nomap non-reusable vdev0vring0@a4000000&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a4008000..0x00000000a400ffff (32 KiB) nomap non-reusable vdev0vring1@a4008000&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a4010000..0x00000000a4017fff (32 KiB) nomap non-reusable vdev1vring0@a4010000&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a4018000..0x00000000a401ffff (32 KiB) nomap non-reusable vdev1vring1@a4018000&lt;BR /&gt;[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4020000, size 1 MiB&lt;BR /&gt;[ 0.000000] OF: reserved mem: initialized node vdevbuffer@a4020000, compatible id shared-dma-pool&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a4020000..0x00000000a411ffff (1024 KiB) nomap non-reusable vdevbuffer@a4020000&lt;BR /&gt;[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4120000, size 1 MiB&lt;BR /&gt;[ 0.000000] OF: reserved mem: initialized node ele-reserved@a4120000, compatible id shared-dma-pool&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a4120000..0x00000000a421ffff (1024 KiB) nomap non-reusable ele-reserved@a4120000&lt;BR /&gt;[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a8000000, size 128 MiB&lt;BR /&gt;[ 0.000000] OF: reserved mem: initialized node ethosu_region@A8000000, compatible id shared-dma-pool&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a8000000..0x00000000afffffff (131072 KiB) map reusable ethosu_region@A8000000&lt;BR /&gt;[ 0.000000] NUMA: No NUMA configuration found&lt;BR /&gt;[ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x00000000dfffffff]&lt;BR /&gt;[ 0.000000] NUMA: NODE_DATA [mem 0xdfcde6c0-0xdfce0fff]&lt;BR /&gt;[ 0.000000] Zone ranges:&lt;BR /&gt;[ 0.000000] DMA [mem 0x0000000080000000-0x00000000dfffffff]&lt;BR /&gt;[ 0.000000] DMA32 empty&lt;BR /&gt;[ 0.000000] Normal empty&lt;BR /&gt;[ 0.000000] Movable zone start for each node&lt;BR /&gt;[ 0.000000] Early memory node ranges&lt;BR /&gt;[ 0.000000] node 0: [mem 0x0000000080000000-0x0000000095ffffff]&lt;BR /&gt;[ 0.000000] node 0: [mem 0x0000000098000000-0x00000000a3ffffff]&lt;BR /&gt;[ 0.000000] node 0: [mem 0x00000000a4000000-0x00000000a421ffff]&lt;BR /&gt;[ 0.000000] node 0: [mem 0x00000000a4220000-0x00000000dfffffff]&lt;BR /&gt;[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000dfffffff]&lt;BR /&gt;[ 0.000000] On node 0, zone DMA: 8192 pages in unavailable ranges&lt;BR /&gt;[ 0.000000] psci: probing for conduit method from DT.&lt;BR /&gt;[ 0.000000] psci: PSCIv1.1 detected in firmware.&lt;BR /&gt;[ 0.000000] psci: Using standard PSCI v0.2 function IDs&lt;BR /&gt;[ 0.000000] psci: Trusted OS migration not required&lt;BR /&gt;[ 0.000000] psci: SMC Calling Convention v1.4&lt;BR /&gt;[ 0.000000] percpu: Embedded 22 pages/cpu s50920 r8192 d31000 u90112&lt;BR /&gt;[ 0.000000] Detected VIPT I-cache on CPU0&lt;BR /&gt;[ 0.000000] CPU features: detected: GIC system register CPU interface&lt;BR /&gt;[ 0.000000] CPU features: detected: Virtualization Host Extensions&lt;BR /&gt;[ 0.000000] CPU features: detected: Qualcomm erratum 1009, or ARM erratum 1286807, 2441009&lt;BR /&gt;[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923&lt;BR /&gt;[ 0.000000] alternatives: applying boot alternatives&lt;BR /&gt;[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon,115200 rdinit=/linuxrc clk_ignore_unused&lt;BR /&gt;[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)&lt;BR /&gt;[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)&lt;BR /&gt;[ 0.000000] Fallback order for Node 0: 0&lt;BR /&gt;[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 378880&lt;BR /&gt;[ 0.000000] Policy zone: DMA&lt;BR /&gt;[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off&lt;BR /&gt;[ 0.000000] software IO TLB: area num 1.&lt;BR /&gt;[ 0.000000] software IO TLB: mapped [mem 0x00000000da100000-0x00000000de100000] (64MB)&lt;BR /&gt;[ 0.000000] Memory: 999188K/1540096K available (21120K kernel code, 1646K rwdata, 7816K rodata, 4032K init, 643K bss, 147692K reserved, 393216K cma-reserved)&lt;BR /&gt;[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;BR /&gt;[ 0.000000] rcu: Preemptible hierarchical RCU implementation.&lt;BR /&gt;[ 0.000000] rcu: RCU event tracing is enabled.&lt;BR /&gt;[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=1.&lt;BR /&gt;[ 0.000000] Trampoline variant of Tasks RCU enabled.&lt;BR /&gt;[ 0.000000] Tracing variant of Tasks RCU enabled.&lt;BR /&gt;[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.&lt;BR /&gt;[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1&lt;BR /&gt;[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0&lt;BR /&gt;[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode&lt;BR /&gt;[ 0.000000] GICv3: 960 SPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: 0 Extended SPIs implemented&lt;BR /&gt;[ 0.000000] Root IRQ handler: gic_handle_irq&lt;BR /&gt;[ 0.000000] GICv3: GICv3 features: 16 PPIs&lt;BR /&gt;[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000048040000&lt;BR /&gt;[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.&lt;BR /&gt;[ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (phys).&lt;BR /&gt;[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns&lt;BR /&gt;[ 0.000000] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns&lt;BR /&gt;[ 0.000311] Console: colour dummy device 80x25&lt;BR /&gt;[ 0.000372] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)&lt;BR /&gt;[ 0.000381] pid_max: default: 32768 minimum: 301&lt;BR /&gt;[ 0.000431] LSM: initializing lsm=capability,integrity&lt;BR /&gt;[ 0.000507] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.000517] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.001203] cacheinfo: Unable to detect cache hierarchy for CPU 0&lt;BR /&gt;[ 0.001723] RCU Tasks: Setting shift to 0 and lim to 1 rcu_task_cb_adjust=1.&lt;BR /&gt;[ 0.001783] RCU Tasks Trace: Setting shift to 0 and lim to 1 rcu_task_cb_adjust=1.&lt;BR /&gt;[ 0.001938] rcu: Hierarchical SRCU implementation.&lt;BR /&gt;[ 0.001941] rcu: Max phase no-delay instances is 1000.&lt;BR /&gt;[ 0.002653] EFI services will not be available.&lt;BR /&gt;[ 0.002732] smp: Bringing up secondary CPUs ...&lt;BR /&gt;[ 0.002754] smp: Brought up 1 node, 1 CPU&lt;BR /&gt;[ 0.002758] SMP: Total of 1 processors activated.&lt;BR /&gt;[ 0.002762] CPU features: detected: 32-bit EL0 Support&lt;BR /&gt;[ 0.002765] CPU features: detected: 32-bit EL1 Support&lt;BR /&gt;[ 0.002769] CPU features: detected: Data cache clean to the PoU not required for I/D coherence&lt;BR /&gt;[ 0.002773] CPU featL▒▒▒ detected: Common not Private translations&lt;BR /&gt;[ 0.002775] CPU features: detected: CRC32 instructions&lt;BR /&gt;[ 0.002782] CPU feed 256 KiB GFP▒FERNEL|GFP_DMA pool for atomic allocations&lt;BR /&gt;[ 0.020831] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations&lt;BR /&gt;[ 0.020885] audit: initializing netlink subsys (disabled)&lt;BR /&gt;[ 0.021046] audit: type=2000 audit(0.016:1): state=initialized audit_enabled=0 res=1&lt;BR /&gt;[ 0.021459] thermal_sys: Registered thermal governor 'step_wise'&lt;BR /&gt;[ 0.021463] thermal_sys: Registered thermal governor 'power_allocator'&lt;BR /&gt;[ 0.021494] cpuidle: using governor menu&lt;BR /&gt;[ 0.021671] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.&lt;BR /&gt;[ 0.021700] ASID allocator initialised with 65536 entries&lt;BR /&gt;[ 0.022299] Serial: AMBA PL011 UART driver&lt;BR /&gt;[ 0.022356] imx mu driver is registered.&lt;BR /&gt;[ 0.022368] imx rpmsg driver is registered.&lt;BR /&gt;[ 0.026827] imx93-pinctrl 443c0000.pinctrl: no fsl,pins and pins property in node /soc@0/bus@44000000/pinctrl@443c0000/usdhc3grp-gpio&lt;BR /&gt;[ 0.026892] imx93-pinctrl 443c0000.pinctrl: initialized IMX pinctrl driver&lt;BR /&gt;[ 0.032912] Modules: 23888 pages in range for non-PLT usage&lt;BR /&gt;[ 0.032922] Modules: 515408 pages in range for PLT usage&lt;BR /&gt;[ 0.033526] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.033536] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page&lt;BR /&gt;[ 0.033540] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.033542] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page&lt;BR /&gt;[ 0.033545] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.033547] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page&lt;BR /&gt;[ 0.033550] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.033552] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page&lt;BR /&gt;[ 0.034889] ACPI: Interpreter disabled.&lt;BR /&gt;[ 0.035812] iommu: Default domain type: Translated&lt;BR /&gt;[ 0.035821] iommu: DMA domain TLB invalidation policy: strict mode&lt;BR /&gt;[ 0.036048] SCSI subsystem initialized&lt;BR /&gt;[ 0.036331] usbcore: registered new interface driver usbfs&lt;BR /&gt;[ 0.036350] usbcore: registered new interface driver hub&lt;BR /&gt;[ 0.036378] usbcore: rePkѕɕ▒▒new device driver usb&lt;BR /&gt;[ 0.036914] mc: Linux media interface: v0.10&lt;BR /&gt;[ 0.036946] videodev: Linux video capture intlinear)&lt;BR /&gt;A▒established hash table entries: 16384 (order: 5, 131072 bytes, linear)&lt;BR /&gt;[ 0.045825] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)&lt;BR /&gt;[ 0.046277] TCP: Hash tables configured (established 16384 bind 16384)&lt;BR /&gt;[ 0.046391] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.046433] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.046577] NET: Registered PF_UNIX/PF_LOCAL protocol family&lt;BR /&gt;[ 0.047005] RPC: Registered named UNIX socket transport module.&lt;BR /&gt;[ 0.047010] RPC: Registered udp transport module.&lt;BR /&gt;[ 0.047013] RPC: Registered tcp transport module.&lt;BR /&gt;[ 0.047014] RPC: Registered tcp-with-tls transport module.&lt;BR /&gt;[ 0.047016] RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;[ 0.047825] PCI: CLS 0 bytes, default 64&lt;BR /&gt;[ 0.048002] Unpacking initramfs...&lt;BR /&gt;[ 0.051636] kvm [1]: IPA Size Limit: 40 bits&lt;BR /&gt;[ 0.051665] kvm [1]: GICv3: no GICV resource entry&lt;BR /&gt;[ 0.051668] kvm [1]: disabling GICv2 emulation&lt;BR /&gt;[ 0.051683] kvm [1]: GIC system register CPU interface enabled&lt;BR /&gt;[ 0.051711] kvm [1]: vgic interrupt IRQ9&lt;BR /&gt;[ 0.051732] kvm [1]: VHE mode initialized successfully&lt;BR /&gt;[ 0.052628] Initialise system trusted keyrings&lt;BR /&gt;[ 0.052809] workingset: timestamp_bits=42 max_order=19 bucket_order=0&lt;BR /&gt;[ 0.053047] squashfs: version 4.0 (2009/01/31) Phillip Lougher&lt;BR /&gt;[ 0.053269] NFS: Registering the id_resolver key type&lt;BR /&gt;[ 0.053290] Key type id_resolver registered&lt;BR /&gt;[ 0.053292] Key type id_legacy registered&lt;BR /&gt;[ 0.053306] nfs4filelayout_init: NFSv4 File Layout Dr@W▒▒Registering...&lt;BR /&gt;[ 0.053310] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...&lt;BR /&gt;[ 0.053323] jffs2: v&lt;BR /&gt;▒[ 1.942431] Freeing initrd memory: 12700K&lt;BR /&gt;[ 1.948478] imx-drm display-subsystem: no available port&lt;BR /&gt;[ 1.960806] loop: module loaded&lt;BR /&gt;[ 1.965058] megasas: 07.725.01.00-rc1&lt;BR /&gt;[ 1.972902] tun: Universal TUN/TAP device driver, 1.6&lt;BR /&gt;[ 1.978535] thunder_xcv, ver 1.0&lt;BR /&gt;[ 1.981847] thunder_bgx, ver 1.0&lt;BR /&gt;[ 1.985102] nicpf, ver 1.0&lt;BR /&gt;[ 1.988836] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version&lt;BR /&gt;[ 1.996062] hns3: Copyright (c) 2017 Huawei Corporation.&lt;BR /&gt;[ 2.001395] hclge is initializing&lt;BR /&gt;[ 2.004742] e1000: Intel(R) PRO/1000 Network Driver&lt;BR /&gt;[ 2.009611] e1000: Copyright (c) 1999-2006 Intel Corporation.&lt;BR /&gt;[ 2.015364] e1000e: Intel(R) PRO/1000 Network Driver&lt;BR /&gt;[ 2.020385] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.&lt;BR /&gt;[ 2.026314] igb: Intel(R) Gigabit Ethernet Network Driver&lt;BR /&gt;[ 2.031703] igb: Copyright (c) 2007-2014 Intel Corporation.&lt;BR /&gt;[ 2.037285] igbvf: Intel(R) Gigabit Virtual Function Network Driver&lt;BR /&gt;[ 2.043545] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.&lt;BR /&gt;[ 2.049553] sky2: driver version 1.30&lt;BR /&gt;[ 2.053532] usbcore: registered new device driver r8152-cfgselector&lt;BR /&gt;[ 2.059817] usbcore: registered new interface driver r8152&lt;BR /&gt;[ 2.065707] VFIO - User Level meta-driver version: 0.3&lt;BR /&gt;[ 2.072397] usbcore: registered new interface driver uas&lt;BR /&gt;[ 2.077768] usbcore: registered new interface driver usb-storage&lt;BR /&gt;[ 2.083815] usbcore: registered new interface driver usbserial_generic&lt;BR /&gt;[ 2.090347] usbserial: USB Serial support registered for generic&lt;BR /&gt;[ 2.096353] usbcore: registered new interface driver ftdi_sio&lt;BR /&gt;[ 2.102096] usbserial: USB Serial support registered for FTDI USB Serial Device&lt;BR /&gt;[ 2.109405] usbcore: registered new interface driver usb_serial_simple&lt;BR /&gt;[ 2.115931] usbserial: USB Serial support registered for carelink&lt;BR /&gt;[ 2.122033] usbserial: USB Serial support registered for flashloader&lt;BR /&gt;[ 2.128383] usbserial: USB Serial support registered for funsoft&lt;BR /&gt;[ 2.134387] usbserial: USB Serial support registered for google&lt;BR /&gt;[ 2.140306] usbserial: USB Serial support registered for hp4x&lt;BR /&gt;[ 2.146052] usbserial: USB Serial support registered for kaufmann&lt;BR /&gt;[ 2.152153] usbserial: USB Serial support registered for libtransistor&lt;BR /&gt;[ 2.158681] usbserial: USB Serial support registered for moto_modem&lt;BR /&gt;[ 2.164946] usbserial: USB Serial support registered for motorola_tetra&lt;BR /&gt;[ 2.171558] usbserial: USB Serial support registered for nokia&lt;BR /&gt;[ 2.177395] usbserial: USB Serial support registered for novatel_gps&lt;BR /&gt;[ 2.183744] usbserial: USB Serial support registered for siemens_mpi&lt;BR /&gt;[ 2.190097] usbserial: USB Serial support registered for suunto&lt;BR /&gt;[ 2.196016] usbserial: USB Serial support registered for vivopay&lt;BR /&gt;[ 2.202022] usbserial: USB Serial support registered for zio&lt;BR /&gt;[ 2.207685] usbcore: registered new interface driver usb_ehset_test&lt;BR /&gt;[ 2.216695] input: 44440000.bbnsm:pwrkey as /devices/platform/soc@0/44000000.bus/44440000.bbnsm/44440000.bbnsm:pwrkey/input/input0&lt;BR /&gt;[ 2.231892] bbnsm_rtc 44440000.bbnsm:rtc: registered as rtc0&lt;BR /&gt;[ 2.238230] bbnsm_rtc 44440000.bbnsm:rtc: setting system clock to 1970-01-01T00:00:00 UTC (0)&lt;BR /&gt;[ 2.247408] i2c_dev: i2c /dev entries driver&lt;BR /&gt;[ 2.254412] imx7ulp-wdt 42490000.watchdog: imx93 wdt probe&lt;BR /&gt;[ 2.286678] Bluetooth: HCI UART driver ver 2.3&lt;BR /&gt;[ 2.291154] Bluetooth: HCI UART protocol H4 registered&lt;BR /&gt;[ 2.296301] Bluetooth: HCI UART protocol BCSP registered&lt;BR /&gt;[ 2.301627] Bluetooth: HCI UART protocol LL registered&lt;BR /&gt;[ 2.306764] Bluetooth: HCI UART protocol ATH3K registered&lt;BR /&gt;[ 2.312169] Bluetooth: HCI UART protocol Three-wire (H5) registered&lt;BR /&gt;[ 2.318540] Bluetooth: HCI UART protocol Broadcom registered&lt;BR /&gt;[ 2.324210] Bluetooth: HCI UART protocol QCA registered&lt;BR /&gt;[ 2.330394] sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;[ 2.336617] sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;[ 2.341231] Synopsys Designware Multimedia Card Interface Driver&lt;BR /&gt;[ 2.347536] sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;[ 2.355446] ledtrig-cpu: registered to indicate activity on CPUs&lt;BR /&gt;[ 2.362335] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....&lt;BR /&gt;[ 2.369126] usbcore: registered new interface driver usbhid&lt;BR /&gt;[ 2.374759] usbhid: USB HID core driver&lt;BR /&gt;[ 2.385410] mmc0: SDHCI controller on 42850000.mmc [42850000.mmc] using ADMA&lt;BR /&gt;[ 2.416967] hw perfevents: enabled with armv8_cortex_a55 PMU driver, 7 counters available&lt;BR /&gt;[ 2.426958] cs_system_cfg: CoreSight Configuration manager initialised&lt;BR /&gt;[ 2.434432] No matching index found for soc_id = 37632.&lt;BR /&gt;[ 2.434445] fsl-ocotp-fsb-s400 47510000.efuse: failed to get the se-fw2 device&lt;BR /&gt;[ 2.447388] optee: probing for conduit method.&lt;BR /&gt;[ 2.451879] optee: revision 4.2 (612bc5a6)&lt;BR /&gt;[ 2.452323] optee: dynamic shared memory is enabled&lt;BR /&gt;[ 2.461667] optee: initialized driver&lt;BR /&gt;[ 2.468246] NET: Registered PF_LLC protocol family&lt;BR /&gt;[ 2.473175] u32 classifier&lt;BR /&gt;[ 2.475899] input device check on&lt;BR /&gt;[ 2.479628] Actions configured&lt;BR /&gt;[ 2.483410] NET: Registered PF_INET6 protocol family&lt;BR /&gt;[ 2.489032] Segment Routing with IPv6&lt;BR /&gt;[ 2.492765] In-situ OAM (IOAM) with IPv6&lt;BR /&gt;[ 2.496792] NET: Registered PF_PACKET protocol family&lt;BR /&gt;[ 2.501896] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.&lt;BR /&gt;[ 2.515055] Bluetooth: RFCOMM TTY layer initialized&lt;BR /&gt;[ 2.520027] Bluetooth: RFCOMM socket layer initialized&lt;BR /&gt;[ 2.525203] Bluetooth: RFCOMM ver 1.11&lt;BR /&gt;[ 2.528975] Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;BR /&gt;[ 2.534324] mmc0: new HS400 Enhanced strobe MMC card at address 0001&lt;BR /&gt;[ 2.541125] mmcblk0: mmc0:0001 DG4008 7.28 GiB&lt;BR /&gt;[ 2.545633] Bluetooth: BNEP filters: protocol multicast&lt;BR /&gt;[ 2.551904] Bluetooth: BNEP socket layer initialized&lt;BR /&gt;[ 2.556954] mmcblk0: p1 p2&lt;BR /&gt;[ 2.559759] Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;BR /&gt;[ 2.566183] mmcblk0boot0: mmc0:0001 DG4008 4.00 MiB&lt;BR /&gt;[ 2.571128] Bluetooth: HIDP socket layer initialized&lt;BR /&gt;[ 2.577141] mmcblk0boot1: mmc0:0001 DG4008 4.00 MiB&lt;BR /&gt;[ 2.582279] 8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;[ 2.587386] mmcblk0rpmb: mmc0:0001 DG4008 4.00 MiB, chardev (234:0)&lt;BR /&gt;[ 2.593702] lib80211: common routines for IEEE802.11 drivers&lt;BR /&gt;[ 2.599474] 9pnet: Installing 9P2000 support&lt;BR /&gt;[ 2.603862] Key type dns_resolver registered&lt;BR /&gt;[ 2.608236] NET: Registered PF_VSOCK protocol family&lt;BR /&gt;[ 2.628135] registered taskstats version 1&lt;BR /&gt;[ 2.633034] Loading compiled-in X.509 certificates&lt;BR /&gt;[ 2.653505] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests&lt;BR /&gt;[ 2.661895] usb_phy_generic usbphynop2: dummy supplies not allowed for exclusive requests&lt;BR /&gt;[ 2.688736] remoteproc remoteproc0: imx-rproc is available&lt;BR /&gt;[ 2.695541] No matching index found for soc_id = 37632.&lt;BR /&gt;[ 2.695557] fsl-ocotp-fsb-s400 47510000.efuse: failed to get the se-fw2 device&lt;BR /&gt;[ 2.709808] i2c i2c-0: LPI2C adapter registered&lt;BR /&gt;[ 2.715332] nxp-pf9453 1-0032: No IRQ configured?&lt;BR /&gt;[ 2.720170] i2c i2c-1: LPI2C adapter registered&lt;BR /&gt;[ 2.724701] nxp-pf9453: probe of 1-0032 failed with error -22&lt;BR /&gt;[ 2.731450] i2c i2c-2: LPI2C adapter registered&lt;BR /&gt;[ 2.738038] No matching index found for soc_id = 37632.&lt;BR /&gt;[ 2.738056] fsl-ocotp-fsb-s400 47510000.efuse: failed to get the se-fw2 device&lt;BR /&gt;[ 2.753586] No matching index found for soc_id = 37632.&lt;BR /&gt;[ 2.753603] fsl-ocotp-fsb-s400 47510000.efuse: failed to get the se-fw2 device&lt;BR /&gt;[ 2.768255] cfg80211: Loading compiled-in X.509 certificates for regulatory database&lt;BR /&gt;[ 2.781972] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'&lt;BR /&gt;[ 2.788249] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'&lt;BR /&gt;[ 2.795658] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2&lt;BR /&gt;[ 2.804380] clk: Not disabling unused clocks&lt;BR /&gt;[ 2.808680] ALSA device list:&lt;BR /&gt;[ 2.811651] No soundcards found.&lt;BR /&gt;[ 2.815391] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db&lt;BR /&gt;[ 2.824654] Freeing unused kernel memory: 4032K&lt;BR /&gt;[ 2.829511] Run /linuxrc as init process&lt;BR /&gt;Found New UDC: ci_hdrc.0&lt;BR /&gt;ci_hdrc.0 0&lt;BR /&gt;ffs.utp0&lt;BR /&gt;[ 2.883040] file system registered&lt;BR /&gt;run utp at /dev/usb-utp0/ep0&lt;BR /&gt;[ 2.902580] read descriptors&lt;/P&gt;&lt;P&gt;uuu fastboot client 1.0.0 [built[ 2.907891] bcdVersion must be 0x0100, stored in Little Endian order. Userspace driver should be fixed, accepting 0x0001 for compatibility.&lt;BR /&gt;Nov 8 2024 16:[ 2.921188] bcdVersion must be 0x0100, stored in Little Endian order. Userspace driver should be fixed, accepting 0x0001 for compatibility.&lt;BR /&gt;52:01]&lt;BR /&gt;Start in[ 2.935076] read strings&lt;BR /&gt;it usb&lt;BR /&gt;write string&lt;BR /&gt;Start handle command&lt;BR /&gt;[ 3.911389] bcdVersion must be 0x0100, stored in Little Endian order. Userspace driver should be fixed, accepting 0x0001 for compatibility.&lt;BR /&gt;[ 3.923927] bcdVersion must be 0x0100, stored in Little Endian order. Userspace driver should be fixed, accepting 0x0001 for compatibility.&lt;BR /&gt;[ 3.938384] No matching index found for soc_id = 37632.&lt;BR /&gt;[ 3.938400] fsl-ocotp-fsb-s400 47510000.efuse: failed to get the se-fw2 device&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I've tried with FRDM board (with FRDM BSP files) and got same output.&lt;/P&gt;&lt;P&gt;Any ideas about what is happening and why FBK commands are not working?&lt;/P&gt;&lt;P&gt;thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Aug 2025 15:59:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2160781#M240412</guid>
      <dc:creator>Hector_Jimenez</dc:creator>
      <dc:date>2025-08-29T15:59:22Z</dc:date>
    </item>
    <item>
      <title>Re: imx93 uuu example_kernel_emmc commands stop after booting initramfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2160810#M240415</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196227"&gt;@Hector_Jimenez&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thank you for reaching out to NXP Support!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have you tried flashing the precompiled images for the FRDM-IMX93 or iMX93-EVK onto your custom board?&lt;/P&gt;
&lt;P&gt;If so, that could be the root of the issue. Precompiled images are specifically built for their respective reference boards and may not work correctly on custom hardware.&lt;/P&gt;
&lt;P&gt;For custom boards, it's essential to adapt the BSP to match your hardware configuration. We recommend using our porting guide to help you through this process.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Fri, 29 Aug 2025 17:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2160810#M240415</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2025-08-29T17:34:24Z</dc:date>
    </item>
    <item>
      <title>Re: imx93 uuu example_kernel_emmc commands stop after booting initramfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2161239#M240426</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206761"&gt;@Chavira&lt;/a&gt;&amp;nbsp;, thank you for your quick answer.&lt;/P&gt;&lt;P&gt;Yes, I've flashed a full customized image using uuu tool by flashing the whole mmc with:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN&gt;.\uuu.exe -b emmc_all .\imx-boot .\bringup-image.rootfs.wic&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN&gt;With this image the device boots correctly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What I need now is to define the partition table using an initramfs in order to keep kernel (Image and dtb) and RFS in separate partitions and made it redundant.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I've built a custom initramfs but it boots the same as with NxP provided initramfs image, no FBK ID nor FBK commands.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;As long as my device boots properly flashing customized kernel and RFS, I assume they are OK. Initramfs boots well too, it just doesn't show any FBK ID so uuu script remains waiting for them.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there any kernel option which I should enable? I didn't find any "FASTBOOT" configuration in config file or menuconfig.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; Héctor&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Sep 2025 07:13:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2161239#M240426</guid>
      <dc:creator>Hector_Jimenez</dc:creator>
      <dc:date>2025-09-01T07:13:16Z</dc:date>
    </item>
    <item>
      <title>Re: imx93 uuu example_kernel_emmc commands stop after booting initramfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2161502#M240436</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206761"&gt;@Chavira&lt;/a&gt;&amp;nbsp;.&lt;/P&gt;&lt;P&gt;I've tried tried flashing my customized firmware image, which boots alright.&lt;/P&gt;&lt;P&gt;Precompiled image was used when I started working with FRDM board.&lt;/P&gt;&lt;P&gt;Then I've tried to boot an initramfs in my custom board, but none of my custom images, nor initramfs + kernel image provided in NxP present in&amp;nbsp;&lt;SPAN&gt;LF_v6.6.52-2.2.1_images_IMX93EVK package, were able to show FBK ID which uuu application can see and then execute FBK commands.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I need to create a partition table in order to deploy RFS and kernel in different partitions and make them redundant as well.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Sep 2025 14:19:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2161502#M240436</guid>
      <dc:creator>Hector_Jimenez</dc:creator>
      <dc:date>2025-09-01T14:19:32Z</dc:date>
    </item>
    <item>
      <title>Re: imx93 uuu example_kernel_emmc commands stop after booting initramfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2162280#M240471</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196227"&gt;@Hector_Jimenez&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;If uuu isn't detecting the FBK ID, it usually means the bootloader isn't properly initializing the USB gadget or the image isn't entering the expected boot mode.&lt;/P&gt;
&lt;P&gt;Check your bootloader configuration: Make sure your custom image includes the correct USB gadget setup (e.g., fastboot or FBK mode).&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Use serial console logs: Connect via UART to see if the board is booting correctly and entering the expected mode.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 16:03:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2162280#M240471</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2025-09-02T16:03:44Z</dc:date>
    </item>
    <item>
      <title>Re: imx93 uuu example_kernel_emmc commands stop after booting initramfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2163765#M240528</link>
      <description>&lt;P&gt;USB and FASTBOOT u-boot configuration was OK&lt;/P&gt;&lt;P&gt;I finally achieved to get FBK ID from uuu.&lt;/P&gt;&lt;P&gt;It was just a matter of usbotg definition in kernel device-tree.&lt;/P&gt;&lt;P&gt;I had it defined with several options, just as it’s in evk device tree:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&amp;amp;usbotg1 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dr_mode = "otg";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; hnp-disable;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; srp-disable;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; adp-disable;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; usb-role-switch;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disable-over-current;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; samsung,picophy-pre-emp-curr-control = &amp;lt;3&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; samsung,picophy-dc-vol-level-adjust = &amp;lt;7&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; status = "okay";&lt;BR /&gt;};&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But it finally worked when I defined it as:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&amp;amp;usbotg1 {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; dr_mode = "otg";&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; disable-over-current;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; status = "okay";&lt;BR /&gt;};&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;disable-over-currrent was the only option needed. I first tried defining only dr_mode = “otg” and status=“okay”, but didn’t work so I included all options defined in evk device-tree.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;</description>
      <pubDate>Thu, 04 Sep 2025 15:41:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-uuu-example-kernel-emmc-commands-stop-after-booting/m-p/2163765#M240528</guid>
      <dc:creator>Hector_Jimenez</dc:creator>
      <dc:date>2025-09-04T15:41:35Z</dc:date>
    </item>
  </channel>
</rss>