<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Test i.MX8M plus USB type A eye pattern in Ubuntu</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Test-i-MX8M-plus-USB-type-A-eye-pattern-in-Ubuntu/m-p/2161796#M240451</link>
    <description>&lt;P&gt;Hi Salas,&lt;/P&gt;&lt;P&gt;Image show&lt;/P&gt;&lt;P&gt;Operating System: Ubuntu 24.04.2 LTS&lt;BR /&gt;Kernel: Linux 6.6.52&lt;/P&gt;&lt;P&gt;Can't found /unit_tests folder&lt;/P&gt;&lt;P&gt;Does apt install memtool use for registors setting?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 02 Sep 2025 05:41:29 GMT</pubDate>
    <dc:creator>Maotom</dc:creator>
    <dc:date>2025-09-02T05:41:29Z</dc:date>
    <item>
      <title>Test i.MX8M plus USB type A eye pattern in Ubuntu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Test-i-MX8M-plus-USB-type-A-eye-pattern-in-Ubuntu/m-p/2160541#M240402</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I would like to perform USB eye pattern from i.MX8M Plus in Ubuntu system. Refer to&amp;nbsp;&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12409.pdf" target="_self"&gt;AN12409&lt;/A&gt;&amp;nbsp;, the &lt;A href="https://github.com/nxp-imx/imx-test.git" target="_self"&gt;memtool&lt;/A&gt; utility need to build and perform the specify registors on section 8.4 of AN12409.&lt;/P&gt;&lt;P&gt;Did I check wrong document or the place of link?&lt;/P&gt;&lt;P&gt;Doesn't find the registers from&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/preview/PREVIEW_IMX8MPRM.pdf" target="_self"&gt;i.MX 8M Plus Applications Processor Reference Manual.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Can't build the memtool utility either.&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#i.mx8mp #USB&lt;/P&gt;</description>
      <pubDate>Fri, 29 Aug 2025 08:49:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Test-i-MX8M-plus-USB-type-A-eye-pattern-in-Ubuntu/m-p/2160541#M240402</guid>
      <dc:creator>Maotom</dc:creator>
      <dc:date>2025-08-29T08:49:06Z</dc:date>
    </item>
    <item>
      <title>Re: Test i.MX8M plus USB type A eye pattern in Ubuntu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Test-i-MX8M-plus-USB-type-A-eye-pattern-in-Ubuntu/m-p/2161664#M240448</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253341"&gt;@Maotom&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing very well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Which i.MX8MP Image are you using? (Multimedia, Full, core, etc.).&lt;/P&gt;
&lt;P&gt;Normally, the memtool is located under&amp;nbsp;/unit_tests/memtool on the i.MX BSPs.&lt;/P&gt;
&lt;P&gt;About the registers, there are not described on the reference manual, but please follow the&amp;nbsp;i.MX 6/7/8 series USB Certification Guide (&lt;A href="https://www.nxp.com/docs/en/application-note/AN12409.pdf?_gl=1*195c3sf*_gcl_au*MTI3Njk1MzUwOS4xNzU2NzM0MDgz*_ga*MTQ3MDkwMDM5MC4xNzQ5MDg5ODQ2*_ga_WM5LE0KMSH*czE3NTY3NzU4MDUkbzEyJGcxJHQxNzU2Nzc3OTUwJGo0NCRsMCRoMTg3MzIxNzI5OA.." target="_self"&gt;AN12409&lt;/A&gt;).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 01:57:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Test-i-MX8M-plus-USB-type-A-eye-pattern-in-Ubuntu/m-p/2161664#M240448</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2025-09-02T01:57:07Z</dc:date>
    </item>
    <item>
      <title>Re: Test i.MX8M plus USB type A eye pattern in Ubuntu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Test-i-MX8M-plus-USB-type-A-eye-pattern-in-Ubuntu/m-p/2161796#M240451</link>
      <description>&lt;P&gt;Hi Salas,&lt;/P&gt;&lt;P&gt;Image show&lt;/P&gt;&lt;P&gt;Operating System: Ubuntu 24.04.2 LTS&lt;BR /&gt;Kernel: Linux 6.6.52&lt;/P&gt;&lt;P&gt;Can't found /unit_tests folder&lt;/P&gt;&lt;P&gt;Does apt install memtool use for registors setting?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 05:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Test-i-MX8M-plus-USB-type-A-eye-pattern-in-Ubuntu/m-p/2161796#M240451</guid>
      <dc:creator>Maotom</dc:creator>
      <dc:date>2025-09-02T05:41:29Z</dc:date>
    </item>
    <item>
      <title>Re: Test i.MX8M plus USB type A eye pattern in Ubuntu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Test-i-MX8M-plus-USB-type-A-eye-pattern-in-Ubuntu/m-p/2162269#M240469</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It seems that you are looking for the /&lt;SPAN&gt;unit_tests&amp;nbsp;&lt;/SPAN&gt;directory on your host.&lt;/P&gt;
&lt;P&gt;/&lt;SPAN&gt;unit_tests is located in the target OS.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Salas.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 15:47:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Test-i-MX8M-plus-USB-type-A-eye-pattern-in-Ubuntu/m-p/2162269#M240469</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2025-09-02T15:47:10Z</dc:date>
    </item>
  </channel>
</rss>