<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 SPL bootup issue for IMX7D</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPL-bootup-issue-for-IMX7D/m-p/2160251#M240392</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I have an issue with SPL boot up. I am currently using fastboot eMMC in uboot and uuu tools for loading. I loaded SPL into bootloader0 which is 0x2 block in boot partition. The normal u-boot used to be loaded to that place as well.&lt;/P&gt;&lt;P&gt;The command I use is "FB[-t 60000]: flash bootloader0 SPL" , but there are nothing showing when device restart and seems bootROM can't find the image.&lt;/P&gt;&lt;P&gt;The SPL image has the IVT header and DCD, the CSF security stuff is disabled.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I use "DP: boot -f SPL", I can see that SPL is running in RAM.&lt;/P&gt;&lt;P&gt;Does anyone have idea that will it can't boot from eMMC?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The attach file is SPL.imx. I rename it to .bin for upload.&lt;/P&gt;&lt;P&gt;#imx #uboot&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 29 Aug 2025 01:50:39 GMT</pubDate>
    <dc:creator>patrickzhang1024</dc:creator>
    <dc:date>2025-08-29T01:50:39Z</dc:date>
    <item>
      <title>SPL bootup issue for IMX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPL-bootup-issue-for-IMX7D/m-p/2160251#M240392</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I have an issue with SPL boot up. I am currently using fastboot eMMC in uboot and uuu tools for loading. I loaded SPL into bootloader0 which is 0x2 block in boot partition. The normal u-boot used to be loaded to that place as well.&lt;/P&gt;&lt;P&gt;The command I use is "FB[-t 60000]: flash bootloader0 SPL" , but there are nothing showing when device restart and seems bootROM can't find the image.&lt;/P&gt;&lt;P&gt;The SPL image has the IVT header and DCD, the CSF security stuff is disabled.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I use "DP: boot -f SPL", I can see that SPL is running in RAM.&lt;/P&gt;&lt;P&gt;Does anyone have idea that will it can't boot from eMMC?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The attach file is SPL.imx. I rename it to .bin for upload.&lt;/P&gt;&lt;P&gt;#imx #uboot&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Aug 2025 01:50:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPL-bootup-issue-for-IMX7D/m-p/2160251#M240392</guid>
      <dc:creator>patrickzhang1024</dc:creator>
      <dc:date>2025-08-29T01:50:39Z</dc:date>
    </item>
    <item>
      <title>Re: SPL bootup issue for IMX7D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPL-bootup-issue-for-IMX7D/m-p/2161241#M240427</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243077"&gt;@patrickzhang1024&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please share&amp;nbsp; your UUU script file.&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Mon, 01 Sep 2025 07:14:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPL-bootup-issue-for-IMX7D/m-p/2161241#M240427</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2025-09-01T07:14:05Z</dc:date>
    </item>
  </channel>
</rss>