<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: LPUART3 support in verdin imx95</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LPUART3-support-in-verdin-imx95/m-p/2159708#M240370</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The LPUART3 is assigned for M7 in scmi. Need to modify&amp;nbsp;&lt;A href="https://github.com/nxp-imx/imx-sm/blob/master/configs/mx95evk.cfg#L373" target="_blank"&gt;https://github.com/nxp-imx/imx-sm/blob/master/configs/mx95evk.cfg#L373&lt;/A&gt;&amp;nbsp;, remove this line from M7 resources.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;LPUART3             OWNER, test&lt;/LI-CODE&gt;
&lt;P&gt;And try to add below line in A55 resources.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;PERLPI_LPUART3      ALL&lt;/LI-CODE&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
    <pubDate>Thu, 28 Aug 2025 07:19:47 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2025-08-28T07:19:47Z</dc:date>
    <item>
      <title>LPUART3 support in verdin imx95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPUART3-support-in-verdin-imx95/m-p/2159671#M240368</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am working on an verdin i.MX95 19x19 EVK and trying to enable LPUART3 in the device tree. After my changes, the kernel panics during boot.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Device tree changes&lt;/STRONG&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;diff --git a/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts b/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts
index 4aa2d000df8b..55d660ce38aa 100644
--- a/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts
+++ b/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts
@@ -570,6 +570,12 @@ &amp;amp;lpuart1 {
status = "okay";
};

+&amp;amp;lpuart3 {
+ pinctrl-names = "default";
+ pinctrl-0 = &amp;lt;&amp;amp;pinctrl_uart3&amp;gt;;
+ status = "okay";
+};
+
&amp;amp;lpuart5 {
/* BT */
pinctrl-names = "default";
@@ -980,6 +986,13 @@ IMX95_PAD_UART1_TXD__AONMIX_TOP_LPUART1_TX 0x31e
&amp;gt;;
};

+ pinctrl_uart3: uart3grp {
+ fsl,pins = &amp;lt;
+ IMX95_PAD_ENET1_RD0__LPUART3_RX 0x31e
+ IMX95_PAD_ENET1_TD0__LPUART3_TX 0x31e
+ &amp;gt;;
+ };
+
pinctrl_uart5: uart5grp {
fsl,pins = &amp;lt;
IMX95_PAD_DAP_TDO_TRACESWO__LPUART5_TX 0x31e&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Boot Logs&lt;/STRONG&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[    2.234704] /soc/bus@42000000/i2c@426d0000/tcpc@52/connector: Fixed dependency cycle(s) with /soc/phy@4c1f0040
[    2.244734] i2c i2c-6: LPI2C adapter registered
[    2.250234] adp5585 1-0034: error -EIO: Failed to read device ID
[    2.256064] adp5585 1-0034: probe with driver adp5585 failed with error -5
[    2.262925] i2c i2c-1: LPI2C adapter registered
[    2.268342] imx8mq-usb-phy 4c1f0040.phy: supply vbus not found, using dummy regulator
[    2.281775] /soc/bridge@4b0d0000/channel@0: Fixed dependency cycle(s) with /soc/syscon@4b010000/bridge@8
[    2.291122] /soc/syscon@4b0c0000/ldb@4/channel@0: Fixed dependency cycle(s) with /soc/syscon@4b010000/bridge@8
[    2.301094] /soc/syscon@4b010000/bridge@8: Fixed dependency cycle(s) with /soc/syscon@4b0c0000/ldb@4/channel@0
[    2.310967] /soc/syscon@4b010000/bridge@8: Fixed dependency cycle(s) with /soc/bridge@4b0d0000/channel@0
[    2.321873] /soc/syscon@4b0c0000/ldb@4/channel@0: Fixed dependency cycle(s) with /lvds0_panel
[    2.330249] /soc/syscon@4b0c0000/ldb@4/channel@0: Fixed dependency cycle(s) with /soc/syscon@4b010000/bridge@8
[    2.342922] scmi-pinctrl-imx scmi_dev.8: Error set config -13
[    2.348464] scmi-pinctrl-imx scmi_dev.8: pin_config_set op failed for pin 56
[    2.355438] fsl-lpuart 42570000.serial: Error applying setting, reverse things back
[    2.363245] Internal error: synchronous external abort: 0000000096000010 [#1] PREEMPT SMP
[    2.371199] Modules linked in:
[    2.374234] CPU: 0 UID: 0 PID: 60 Comm: kworker/u24:3 Not tainted 6.12.20-lts-next-gdfaf2136deb2-dirty #1
[    2.383764] Hardware name: NXP i.MX95 19X19 board (DT)
[    2.388879] Workqueue: events_unbound deferred_probe_work_func
[    2.394685] pstate: 60400009 (nZCv daif +PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[    2.401611] pc : lpuart_probe+0x55c/0x630
[    2.405598] lr : lpuart_probe+0x33c/0x630
[    2.409591] sp : ffff800083083b20
[    2.412884] x29: ffff800083083b30 x28: 0000000000000000 x27: 0000000000000000
[    2.419991] x26: ffff000080b4c240 x25: 0000000000000000 x24: ffff800080876bf0
[    2.427091] x23: ffff8000822d9bc8 x22: ffff000080208410 x21: ffff000080208400
[    2.434198] x20: 0000000000000000 x19: ffff00008177a880 x18: ffffffffffffffff
[    2.441304] x17: ffff0000815ee000 x16: ffff0000815ede00 x15: 0000000000000002
[    2.448411] x14: ffffffffffffffff x13: ffff0000807bc580 x12: 0000000000000001
[    2.455518] x11: 000000008bb15db4 x10: 0000000000000a90 x9 : ffff800083083830
[    2.462624] x8 : ffff0003fdf58c80 x7 : 1000000000000104 x6 : 0000000000000002
[    2.469731] x5 : 1000000000000004 x4 : ffff0000807bc500 x3 : 0000000000000000
[    2.476838] x2 : ffff800082400278 x1 : 0000000000000003 x0 : ffff8000825c3018
[    2.483951] Call trace:
[    2.486378]  lpuart_probe+0x55c/0x630
[    2.490018]  platform_probe+0x68/0xc8
[    2.493651]  really_probe+0xbc/0x29c
[    2.497205]  __driver_probe_device+0x78/0x12c
[    2.501538]  driver_probe_device+0x3c/0x15c
[    2.505698]  __device_attach_driver+0xb8/0x134
[    2.510118]  bus_for_each_drv+0x88/0xe8
[    2.513931]  __device_attach+0xa0/0x190
[    2.517744]  device_initial_probe+0x14/0x20
[    2.521904]  bus_probe_device+0xac/0xb0
[    2.525718]  deferred_probe_work_func+0x80/0xb8
[    2.530224]  process_one_work+0x148/0x28c
[    2.534211]  worker_thread+0x2c8/0x3d0
[    2.537938]  kthread+0x110/0x114
[    2.541144]  ret_from_fork+0x10/0x20
[    2.544707] Code: f9411260 97fbe006 17ffff17 91002000 (b940001a) 
[    2.550772] ---[ end trace 0000000000000000 ]---
&lt;/LI-CODE&gt;&lt;P&gt;&lt;STRONG&gt;Question&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Are ENET1_RD0 and ENET1_TD0 the correct pads for LPUART3 RX/TX on this board?&lt;/LI&gt;&lt;LI&gt;Do I need to adjust SCMI/firmware ownership of these pins for Linux to use them?&lt;/LI&gt;&lt;LI&gt;Does anyone have a known-good DTS snippet for LPUART3 on the i.MX95 EVK?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Aug 2025 06:34:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPUART3-support-in-verdin-imx95/m-p/2159671#M240368</guid>
      <dc:creator>junaidh12</dc:creator>
      <dc:date>2025-08-28T06:34:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART3 support in verdin imx95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPUART3-support-in-verdin-imx95/m-p/2159708#M240370</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The LPUART3 is assigned for M7 in scmi. Need to modify&amp;nbsp;&lt;A href="https://github.com/nxp-imx/imx-sm/blob/master/configs/mx95evk.cfg#L373" target="_blank"&gt;https://github.com/nxp-imx/imx-sm/blob/master/configs/mx95evk.cfg#L373&lt;/A&gt;&amp;nbsp;, remove this line from M7 resources.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;LPUART3             OWNER, test&lt;/LI-CODE&gt;
&lt;P&gt;And try to add below line in A55 resources.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;PERLPI_LPUART3      ALL&lt;/LI-CODE&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Thu, 28 Aug 2025 07:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPUART3-support-in-verdin-imx95/m-p/2159708#M240370</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-08-28T07:19:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART3 support in verdin imx95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPUART3-support-in-verdin-imx95/m-p/2164728#M240558</link>
      <description>&lt;P&gt;Thank you&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788"&gt;@Zhiming_Liu&lt;/a&gt;;&amp;nbsp;The solution you provided worked. I did the following changes in the imx-system-manager code related to lpuart3 along with my device tree changes and build a new yocto image. ttyLP2 was in the /dev/ and I also used it in my application and was also running successfully.&lt;BR /&gt;&lt;BR /&gt;Changes in imx-system-manager code:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;--- a/configs/mx95evk.cfg
+++ b/configs/mx95evk.cfg
@@ -370,7 +370,6 @@ LPIT1               OWNER
 LPTMR1              OWNER
 LPTMR2              OWNER
 LPTPM1              OWNER
-LPUART3             OWNER, test
 MSGINTR1            OWNER
 MSGINTR2            OWNER
 MU5_A               OWNER
@@ -477,6 +476,7 @@ PERLPI_GPIO3        ALL
 PERLPI_GPIO4        ALL
 PERLPI_GPIO5        ALL
 PERLPI_LPUART1      ALL
+PERLPI_LPUART3      ALL
 PERLPI_LPUART4      ALL
 PERLPI_LPUART5      ALL
 PERLPI_LPUART6      ALL
@@ -760,6 +760,7 @@ LPTPM4              OWNER
 LPTPM5              OWNER
 LPTPM6              OWNER
 LPUART1             OWNER
+LPUART3             OWNER
 LPUART4             OWNER
 LPUART5             OWNER
 LPUART6             OWNER&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;my /dev directory&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx95:~# ls -al /dev/ttyLP2
crw-rw---- 1 root dialout 241, 2 Sep  7 14:30 /dev/ttyLP2
root@imx95:~# dmesg | grep ttyLP2
[    2.426195] 42570000.serial: ttyLP2 at MMIO 0x42570010 (irq = 141, base_baud = 1500000) is a FSL_LPUART&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 07 Sep 2025 14:57:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPUART3-support-in-verdin-imx95/m-p/2164728#M240558</guid>
      <dc:creator>junaidh12</dc:creator>
      <dc:date>2025-09-07T14:57:40Z</dc:date>
    </item>
  </channel>
</rss>