<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックFRDM93 IMX9352 P11(GPIO_IO00 to GPIO_IO29) under linux control How can I keep off under linux?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FRDM93-IMX9352-P11-GPIO-IO00-to-GPIO-IO29-under-linux-control/m-p/2159042#M240347</link>
    <description>&lt;P&gt;Hi, I'm using FRDM93 , I want to free pin of P11 (GPIO_IO00 to GPIO_IO29) from linux to use them with core M33 and to initializate them by my C code. I'm using the file imx93-11x11-frdm.dtb and image LF_v6.6.36-2.1.0_images_FRDM_4.0_IMX9. I tried with file dtbo, but without success.How can I do ?&lt;/P&gt;</description>
    <pubDate>Wed, 27 Aug 2025 09:09:50 GMT</pubDate>
    <dc:creator>Gutenberg-coder</dc:creator>
    <dc:date>2025-08-27T09:09:50Z</dc:date>
    <item>
      <title>FRDM93 IMX9352 P11(GPIO_IO00 to GPIO_IO29) under linux control How can I keep off under linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM93-IMX9352-P11-GPIO-IO00-to-GPIO-IO29-under-linux-control/m-p/2159042#M240347</link>
      <description>&lt;P&gt;Hi, I'm using FRDM93 , I want to free pin of P11 (GPIO_IO00 to GPIO_IO29) from linux to use them with core M33 and to initializate them by my C code. I'm using the file imx93-11x11-frdm.dtb and image LF_v6.6.36-2.1.0_images_FRDM_4.0_IMX9. I tried with file dtbo, but without success.How can I do ?&lt;/P&gt;</description>
      <pubDate>Wed, 27 Aug 2025 09:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM93-IMX9352-P11-GPIO-IO00-to-GPIO-IO29-under-linux-control/m-p/2159042#M240347</guid>
      <dc:creator>Gutenberg-coder</dc:creator>
      <dc:date>2025-08-27T09:09:50Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM93 IMX9352 P11(GPIO_IO00 to GPIO_IO29) under linux control How can I keep off under linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM93-IMX9352-P11-GPIO-IO00-to-GPIO-IO29-under-linux-control/m-p/2160932#M240416</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245785"&gt;@Gutenberg-coder&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can let the M33 own the P11 header pins (GPIO_IO00...GPIO_IO29) , you need to&lt;/P&gt;
&lt;P&gt;1. stop Linux from touching those pads (disable any Linux drivers/pinctl groups that use them)&lt;/P&gt;
&lt;P&gt;2. Make sure M33 has permission to the IOMUXC/GPIO blocks (TRDC settings)&lt;/P&gt;
&lt;P&gt;3 Mux and initialize from M33 C code.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Sat, 30 Aug 2025 05:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM93-IMX9352-P11-GPIO-IO00-to-GPIO-IO29-under-linux-control/m-p/2160932#M240416</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2025-08-30T05:53:06Z</dc:date>
    </item>
  </channel>
</rss>