<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSECURE BOOT IMX8MP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SECURE-BOOT-IMX8MP/m-p/2152401#M240116</link>
    <description>&lt;P&gt;While implementing Secure Boot on an i.MX8MP-based device, we thoroughly tested using hab_status. Everything worked as expected—no HAB events were reported. We ran tests over 10 times with different image-signing setups and consistently saw no HAB events when the image was properly signed (we did see events when the image was unsigned).&lt;/P&gt;&lt;P&gt;After finalizing the setup, we closed the device. However, with the same device and the exact same signed image, the boot image started getting rejected.&lt;BR /&gt;If there had been an issue with image signing or SRK keys, it should have been reflected in hab_status, but there were no such errors during testing.&lt;/P&gt;&lt;P&gt;I’m attaching our Secure Boot rejection logs:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;SPL_ONLY.txt&lt;/STRONG&gt; – Default configuration without FIT image optional configs&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;SPL_FIT.txt&lt;/STRONG&gt; – With FIT image optional configs and csf_fit.txt&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Thu, 14 Aug 2025 13:57:03 GMT</pubDate>
    <dc:creator>xae-abhishek</dc:creator>
    <dc:date>2025-08-14T13:57:03Z</dc:date>
    <item>
      <title>SECURE BOOT IMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SECURE-BOOT-IMX8MP/m-p/2152401#M240116</link>
      <description>&lt;P&gt;While implementing Secure Boot on an i.MX8MP-based device, we thoroughly tested using hab_status. Everything worked as expected—no HAB events were reported. We ran tests over 10 times with different image-signing setups and consistently saw no HAB events when the image was properly signed (we did see events when the image was unsigned).&lt;/P&gt;&lt;P&gt;After finalizing the setup, we closed the device. However, with the same device and the exact same signed image, the boot image started getting rejected.&lt;BR /&gt;If there had been an issue with image signing or SRK keys, it should have been reflected in hab_status, but there were no such errors during testing.&lt;/P&gt;&lt;P&gt;I’m attaching our Secure Boot rejection logs:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;SPL_ONLY.txt&lt;/STRONG&gt; – Default configuration without FIT image optional configs&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;SPL_FIT.txt&lt;/STRONG&gt; – With FIT image optional configs and csf_fit.txt&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Thu, 14 Aug 2025 13:57:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SECURE-BOOT-IMX8MP/m-p/2152401#M240116</guid>
      <dc:creator>xae-abhishek</dc:creator>
      <dc:date>2025-08-14T13:57:03Z</dc:date>
    </item>
    <item>
      <title>Re: SECURE BOOT IMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SECURE-BOOT-IMX8MP/m-p/2152663#M240128</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253061"&gt;@xae-abhishek&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I've already replied back to you in another ticket from you. Please let me know if any from there.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 15 Aug 2025 03:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SECURE-BOOT-IMX8MP/m-p/2152663#M240128</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-08-15T03:57:58Z</dc:date>
    </item>
  </channel>
</rss>