<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic VSCode J-link settings file and startup command in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/VSCode-J-link-settings-file-and-startup-command/m-p/2150762#M240050</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am facing problems with debugging code using J-link and VSCode extension with iMXRT117x. I am using a custom board without flash - only external RAM is available. With MCUXpresso I was able to establish proper debugging session but with VSCode I have troubles.&amp;nbsp;&lt;/P&gt;&lt;P&gt;First thing that is not working fully correct for me is that J-link settings file is loaded from default location which is in the "build" directory. I can change the settings in the file but my environment work in the way that when I clean project the build directory is deleted so I need to change settings file every time I clean the build. Is it possible to set custom path to the settings J-link file?&lt;/P&gt;&lt;P&gt;Second thing is that to be able properly debug the code I need to add the memory settings. In the MCUXpresso it is done in the way presented below&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Greenhal_0-1754988324796.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/351965iC1DA9A389F0B1A4F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Greenhal_0-1754988324796.png" alt="Greenhal_0-1754988324796.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Greenhal_0-1754988324796.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;How can I add this settings to the VSCode debugger?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
    <pubDate>Tue, 12 Aug 2025 08:51:16 GMT</pubDate>
    <dc:creator>Greenhal</dc:creator>
    <dc:date>2025-08-12T08:51:16Z</dc:date>
    <item>
      <title>VSCode J-link settings file and startup command</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VSCode-J-link-settings-file-and-startup-command/m-p/2150762#M240050</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am facing problems with debugging code using J-link and VSCode extension with iMXRT117x. I am using a custom board without flash - only external RAM is available. With MCUXpresso I was able to establish proper debugging session but with VSCode I have troubles.&amp;nbsp;&lt;/P&gt;&lt;P&gt;First thing that is not working fully correct for me is that J-link settings file is loaded from default location which is in the "build" directory. I can change the settings in the file but my environment work in the way that when I clean project the build directory is deleted so I need to change settings file every time I clean the build. Is it possible to set custom path to the settings J-link file?&lt;/P&gt;&lt;P&gt;Second thing is that to be able properly debug the code I need to add the memory settings. In the MCUXpresso it is done in the way presented below&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Greenhal_0-1754988324796.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/351965iC1DA9A389F0B1A4F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Greenhal_0-1754988324796.png" alt="Greenhal_0-1754988324796.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Greenhal_0-1754988324796.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;How can I add this settings to the VSCode debugger?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Tue, 12 Aug 2025 08:51:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VSCode-J-link-settings-file-and-startup-command/m-p/2150762#M240050</guid>
      <dc:creator>Greenhal</dc:creator>
      <dc:date>2025-08-12T08:51:16Z</dc:date>
    </item>
    <item>
      <title>Re: VSCode J-link settings file and startup command</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VSCode-J-link-settings-file-and-startup-command/m-p/2150820#M240053</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;You're facing two key issues with J-Link and VSCode on your iMXRT117x custom board. First, to avoid losing your J-Link settings file when cleaning the build directory, you can set a custom path in launch.json using the -settingsfile argument, pointing to a stable location like ${workspaceFolder}/jlink_settings.ini. Second, to enable proper debugging with external RAM, replicate MCUXpresso’s memory settings by adding a memoryMap entry in launch.json, specifying the RAM’s start address, size, and access type. This ensures the debugger knows where valid memory is for breakpoints and variable inspection.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Aug 2025 09:52:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VSCode-J-link-settings-file-and-startup-command/m-p/2150820#M240053</guid>
      <dc:creator>Jamie309Perez</dc:creator>
      <dc:date>2025-08-12T09:52:12Z</dc:date>
    </item>
    <item>
      <title>Re: VSCode J-link settings file and startup command</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VSCode-J-link-settings-file-and-startup-command/m-p/2152530#M240123</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210543"&gt;@Greenhal&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Unfortunately, the two features that you are looking for are not available on the current version of VS Code. Please continue using standalone MCUXpresso IDE instead.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Aug 2025 20:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VSCode-J-link-settings-file-and-startup-command/m-p/2152530#M240123</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-08-14T20:47:11Z</dc:date>
    </item>
  </channel>
</rss>