<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Always on PWM Overlay in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Always-on-PWM-Overlay/m-p/2148898#M239965</link>
    <description>&lt;P&gt;Hi folks,&lt;/P&gt;&lt;P&gt;I am working with a Verdin imx8mp som + Dahlia carrier board from Toradex and created a Buildroot configuration to build a Linux image for this hardware.&lt;BR /&gt;The device tree I am using is comprised of the files attached to this post.&lt;BR /&gt;I have successfully created overlays to wake up the Linux from Suspend to RAM when a given GPIO is pressed or to interface with an external LCD.&lt;/P&gt;&lt;P&gt;Now I need an overlay that will make PWM2 keep running even when the system goes into Suspend to RAM mode.&lt;BR /&gt;Can you please help me with that?&lt;BR /&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Fri, 08 Aug 2025 06:05:13 GMT</pubDate>
    <dc:creator>rodG</dc:creator>
    <dc:date>2025-08-08T06:05:13Z</dc:date>
    <item>
      <title>Always on PWM Overlay</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Always-on-PWM-Overlay/m-p/2148898#M239965</link>
      <description>&lt;P&gt;Hi folks,&lt;/P&gt;&lt;P&gt;I am working with a Verdin imx8mp som + Dahlia carrier board from Toradex and created a Buildroot configuration to build a Linux image for this hardware.&lt;BR /&gt;The device tree I am using is comprised of the files attached to this post.&lt;BR /&gt;I have successfully created overlays to wake up the Linux from Suspend to RAM when a given GPIO is pressed or to interface with an external LCD.&lt;/P&gt;&lt;P&gt;Now I need an overlay that will make PWM2 keep running even when the system goes into Suspend to RAM mode.&lt;BR /&gt;Can you please help me with that?&lt;BR /&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Aug 2025 06:05:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Always-on-PWM-Overlay/m-p/2148898#M239965</guid>
      <dc:creator>rodG</dc:creator>
      <dc:date>2025-08-08T06:05:13Z</dc:date>
    </item>
    <item>
      <title>Re: Always on PWM Overlay</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Always-on-PWM-Overlay/m-p/2149263#M239989</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You have to go with&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/5672"&gt;@toradex&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 08 Aug 2025 14:03:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Always-on-PWM-Overlay/m-p/2149263#M239989</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-08-08T14:03:01Z</dc:date>
    </item>
  </channel>
</rss>